Dear all,
I would like to compiler power sgx driver for my card with 3515 processor, unfortunately some errors that I can't fix its. Somebody can help me.
I have used a kernel version 2.6.33.7 with somme driver modify and uImage run.
Thank you for your reponse
Regards,
Francis LE
$ make OMAPES=3.x BUILD=release
building the sgx kernel modules...
make[1]: Entering directory `/home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM'
make -C /home/flehoanglong/OMAP3D/kernel M=`pwd` clean
make[2]: Entering directory `/home/flehoanglong/OMAP3D/kernel'
CLEAN /home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/.tmp_versions
make[2]: Leaving directory `/home/flehoanglong/OMAP3D/kernel'
make[1]: Leaving directory `/home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM'
make[1]: Entering directory `/home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM'
make -C /home/flehoanglong/OMAP3D/kernel M=`pwd`
make[2]: Entering directory `/home/flehoanglong/OMAP3D/kernel'
LD /home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/bufferclass_ti/built-in.o
CC [M] /home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/bufferclass_ti/bc_cat.o
LD [M] /home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/bufferclass_ti/bufferclass_ti.o
LD /home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/dc_omap3430_linux/built-in.o
CC [M] /home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/dc_omap3430_linux/omaplfb_displayclass.o
CC [M] /home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/dc_omap3430_linux/omaplfb_linux.o
/home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/dc_omap3430_linux/omaplfb_linux.c:57:50: error: expected declaration specifiers or '...' before 'IMG_UINT32'
/home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/dc_omap3430_linux/omaplfb_linux.c: In function 'OMAPLFBEnableVSyncInterrupt':
/home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/dc_omap3430_linux/omaplfb_linux.c:104:6: error: 'pOMAPLFBVSyncISRHandle' undeclared (first use in this function)
/home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/dc_omap3430_linux/omaplfb_linux.c:104:6: note: each undeclared identifier is reported only once for each function it appears in
/home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/dc_omap3430_linux/omaplfb_linux.c: In function 'OMAPLFBDisableVSyncInterrupt':
/home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/dc_omap3430_linux/omaplfb_linux.c:110:6: error: 'pOMAPLFBVSyncISRHandle' undeclared (first use in this function)
/home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/dc_omap3430_linux/omaplfb_linux.c: In function 'OMAPLFBFlip':
/home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/dc_omap3430_linux/omaplfb_linux.c:195:2: error: too many arguments to function 'omap_dispc_set_plane_base'
/home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/dc_omap3430_linux/omaplfb_linux.c:57:13: note: declared here
make[4]: *** [/home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/dc_omap3430_linux/omaplfb_linux.o] Error 1
make[3]: *** [/home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM/services4/3rdparty/dc_omap3430_linux] Error 2
make[2]: *** [_module_/home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM] Error 2
make[2]: Leaving directory `/home/flehoanglong/OMAP3D/kernel'
make[1]: *** [all] Error 2
make[1]: Leaving directory `/home/flehoanglong/OMAP3D/graphics/OMAP35x_Graphics_SDK_3_01_00_07/GFX_Linux_KM'
make: *** [buildkernel] Error 2