Hi,
How to run the GPIO-LED example on the K2E EVM ( ARM core ) -or- K2H EVM (ARM core ) ?
Please post the video, so that it will be easy to run.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
How to run the GPIO-LED example on the K2E EVM ( ARM core ) -or- K2H EVM (ARM core ) ?
Please post the video, so that it will be easy to run.
How to run the GPIO-LED example on the K2E EVM ( ARM core ) -or- K2H EVM (ARM core ) ?
Pre-requisite:
Step1:
Generate the PDK examples by following this link:-
For K2E
For K2H
Step2:
For K2E : DIP switch settings of the K2E EVM in "NO BOOT" -- SW1 - 1,2,3,4 -- OFF, OFF, OFF, OFF.
For K2H : DIP switch settings of "NO BOOT" -- SW1 - 1,2,3,4 -- OFF, OFF, OFF, ON.
Step3:
Watch the video, below and follow the steps.
The steps in the video are captured for K2E EVM. However, the same procedure shall be applied for K2H EVM too.
Regards
Shankari G