Other Parts Discussed in Thread: TDA4, TEST
What is the work flow for creating a LDC mesh LUT for fisheye distortion correction on TDA4?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
This FAQ is adapted from another E2E discussion about the same topic here.
This is an example work flow for creating a TDA4 LDC mesh LUT for fisheye distortion correction.
1. This is the "matlab/octave" code for generating a mesh LUT text file to be used with DCC tuning tool for TDA4 ISP.
function [] = gen_lut(spec_file, pitch_in_mm,f_in_mm, W, H, hc, vc,s ,m) f = f_in_mm/pitch_in_mm ; [h_p , v_p] = meshgrid( 0:W, 0:H); [h_d,v_d] = xyz2distorted(h_p,v_p, f/s, hc, vc,spec_file, pitch_in_mm); h_delta = round((h_d-h_p) * 8); v_delta = round((v_d-v_p) * 8); mh = h_delta(1:2^m:end, 1:2^m:end)'; mv = v_delta(1:2^m:end, 1:2^m:end)'; dlmwrite('mesh.txt', [mh(:), mv(:)], 'delimiter', ' '); function [h_d, v_d] = xyz2distorted(x, y, z, hc, vc, spec_file, pitch_in_mm) [phi, r] = cart2pol(x-hc, y-vc); theta = atan2(r, z); lut = read_spec(spec_file, pitch_in_mm); r = interp1(lut(:,1), lut(:,2), theta); [h_d, v_d] = pol2cart(phi, r); h_d = h_d + hc; v_d = v_d + vc; function lut = read_spec(spec_file, pitch_in_mm) lut0 = dlmread(spec_file); theta = lut0(:,1)/180*pi; lut = [theta, lut0(:,2)/pitch_in_mm];
2. Call the above matlab code as below with the given lens distortion spec file in text format.
s = 2; m = 4; pitch_in_mm = 0.0028; f_in_mm = 0.85; W = 1280; H = 944; hc = W/2; vc = H/2; Wmesh = ceil(W / 2^m) * 2^m; Hmesh = ceil(H / 2^m) * 2^m; gen_lut("spec_file.txt", pitch_in_mm, f_in_mm, Wmesh, Hmesh, hc, vc, s, m);
Lens distortion spec file (the first column is in degrees and the second in mm):
0 0 1 0.01484264 2 0.02969027 3 0.04454789 4 0.05942044 5 0.07431283 6 0.08922991 7 0.10417648 8 0.11915721 9 0.13417672 10 0.14923947 11 0.16434983 12 0.179512 13 0.19473004 14 0.21000785 15 0.22534914 16 0.24075744 17 0.25623609 18 0.2717882 19 0.28741673 20 0.30312436 21 0.31891361 22 0.33478678 23 0.35074594 24 0.366793 25 0.38292965 26 0.39915742 27 0.41547767 28 0.43189163 29 0.4484004 30 0.46500498 31 0.48170629 32 0.4985052 33 0.51540257 34 0.53239923 35 0.54949606 36 0.56669399 37 0.58399403 38 0.60139728 39 0.61890497 40 0.63651849 41 0.65423936 42 0.67206928 43 0.69001016 44 0.70806407 45 0.7262333 46 0.74452032 47 0.7629278 48 0.78145862 49 0.80011582 50 0.8189026 51 0.83782233 52 0.85687848 53 0.87607467 54 0.89541455 55 0.91490184 56 0.93454026 57 0.9543335 58 0.97428515 59 0.9943987 60 1.01467742 61 1.03512436 62 1.05574223 63 1.07653335 64 1.09749959 65 1.11864221 66 1.13996187 67 1.16145842 68 1.18313088 69 1.20497727 70 1.22699447 71 1.24917817 72 1.27152265 73 1.29402069 74 1.3166634 75 1.33944009 76 1.36233815 77 1.38534288 78 1.40843739 79 1.43160246 80 1.4548165 81 1.47805542 82 1.50129263 83 1.52449902 84 1.54764298 85 1.57069051 86 1.59360531 87 1.61634901 88 1.63888135 89 1.66116052 90 1.68314347 91 1.7047863 92 1.72604473 93 1.74687449 94 1.76723187 95 1.78707414 96 1.80636008
3. The output file "mesh.txt" from above call is in the right format as input to TDA4 DCC tuning tool.
The first column is for horizontal offsets and the second for vertical offsets.
1818 1341 1729 1308 1641 1274 1555 1240 1471 1205 1388 1170 1308 1134 1229 1098 1152 1062 1077 1025 1004 987 933 949 865 911 799 873 735 834 674 796 616 757 560 718 507 680 456 641 409 603 364 566 323 529 284 492 248 457 215 422 185 389 157 357 133 327 111 298 92 271 75 246 60 223 48 202 37 184 29 168 21 155 15 145 9 138 5 133 0 132 -5 133 -9 138 -15 145 -21 155 -29 168 -37 184 -48 202 -60 223 -75 246 -92 271 -111 298 -133 327 -157 357 -185 389 -215 422 -248 457 -284 492 -323 529 -364 566 -409 603 -456 641 -507 680 -560 718 -616 757 -674 796 -735 834 -799 873 -865 911 -933 949 -1004 987 -1077 1025 -1152 1062 -1229 1098 -1308 1134 -1388 1170 -1471 1205 -1555 1240 -1641 1274 -1729 1308 -1818 1341 1785 1272 1695 1239 1607 1206 1521 1171 1436 1137 1353 1102 1272 1066 1192 1030 1115 993 1039 956 966 918 895 880 827 841 760 802 696 763 635 724 577 685 521 646 468 606 418 567 371 528 327 490 285 452 247 415 212 378 180 343 151 308 126 275 103 244 83 214 65 186 50 160 38 136 28 115 20 96 14 79 9 66 6 55 3 47 2 43 0 41 -2 43 -3 47 -6 55 -9 66 -14 79 -20 96 -28 115 -38 136 -50 160 -65 186 -83 214 -103 244 -126 275 -151 308 -180 343 -212 378 -247 415 -285 452 -327 490 -371 528 -418 567 -468 606 -521 646 -577 685 -635 724 -696 763 -760 802 -827 841 -895 880 -966 918 -1039 956 -1115 993 -1192 1030 -1272 1066 -1353 1102 -1436 1137 -1521 1171 -1607 1206 -1695 1239 -1785 1272 1753 1205 1662 1172 1574 1139 1487 1105 1401 1070 1317 1035 1236 999 1156 963 1078 926 1002 889 928 851 857 812 788 774 721 734 657 695 596 655 537 615 481 575 428 536 378 496 332 456 288 417 247 378 210 340 176 302 145 266 117 230 93 196 71 164 53 133 38 104 25 77 15 52 7 29 2 10 -1 -7 -3 -21 -4 -33 -3 -41 -2 -45 0 -47 2 -45 3 -41 4 -33 3 -21 1 -7 -2 10 -7 29 -15 52 -25 77 -38 104 -53 133 -71 164 -93 196 -117 230 -145 266 -176 302 -210 340 -247 378 -288 417 -332 456 -378 496 -428 536 -481 575 -537 615 -596 655 -657 695 -721 734 -788 774 -857 812 -928 851 -1002 889 -1078 926 -1156 963 -1236 999 -1317 1035 -1401 1070 -1487 1105 -1574 1139 -1662 1172 -1753 1205 1720 1140 1629 1107 1540 1074 1452 1040 1366 1006 1282 971 1199 935 1119 899 1040 862 964 824 890 786 818 748 749 708 682 669 617 629 556 589 497 549 441 508 388 467 338 427 292 387 248 346 208 307 172 267 138 229 108 191 82 155 59 120 39 86 22 54 9 24 -1 -4 -9 -30 -14 -53 -17 -74 -17 -91 -16 -106 -13 -118 -10 -126 -5 -131 0 -133 5 -131 10 -126 13 -118 16 -106 17 -91 17 -74 14 -53 9 -30 1 -4 -9 24 -22 54 -39 86 -59 120 -82 155 -108 191 -138 229 -172 267 -208 307 -248 346 -292 387 -338 427 -388 467 -441 508 -497 549 -556 589 -617 629 -682 669 -749 708 -818 748 -890 786 -964 824 -1040 862 -1119 899 -1199 935 -1282 971 -1366 1006 -1452 1040 -1540 1074 -1629 1107 -1720 1140 1688 1076 1597 1044 1507 1011 1418 977 1332 943 1247 908 1163 873 1082 836 1003 799 926 762 852 724 779 685 709 646 642 606 577 566 515 526 456 485 400 444 347 402 297 361 251 320 208 279 168 239 132 198 100 159 71 120 46 83 24 47 6 12 -9 -21 -21 -53 -29 -82 -34 -109 -36 -133 -36 -154 -34 -173 -30 -188 -24 -200 -16 -209 -8 -214 0 -216 8 -214 16 -209 24 -200 30 -188 34 -173 36 -154 36 -133 34 -109 29 -82 21 -53 9 -21 -6 12 -24 47 -46 83 -71 120 -100 159 -132 198 -168 239 -208 279 -251 320 -297 361 -347 402 -400 444 -456 485 -515 526 -577 566 -642 606 -709 646 -779 685 -852 724 -926 762 -1003 799 -1082 836 -1163 873 -1247 908 -1332 943 -1418 977 -1507 1011 -1597 1044 -1688 1076 1656 1015 1564 983 1474 950 1384 917 1297 883 1211 848 1128 813 1046 776 966 740 888 702 813 664 740 625 670 586 602 546 537 506 474 465 415 424 359 382 306 340 256 299 210 257 167 215 128 174 92 133 60 92 32 53 8 14 -12 -23 -29 -59 -42 -94 -51 -126 -57 -156 -60 -184 -60 -209 -57 -232 -51 -251 -44 -267 -34 -280 -24 -289 -12 -295 0 -296 12 -295 24 -289 34 -280 44 -267 51 -251 57 -232 60 -209 60 -184 57 -156 51 -126 42 -94 29 -59 12 -23 -8 14 -32 53 -60 92 -92 133 -128 174 -167 215 -210 257 -256 299 -306 340 -359 382 -415 424 -474 465 -537 506 -602 546 -670 586 -740 625 -813 664 -888 702 -966 740 -1046 776 -1128 813 -1211 848 -1297 883 -1384 917 -1474 950 -1564 983 -1656 1015 1625 955 1532 923 1441 891 1351 858 1263 824 1176 790 1092 755 1009 719 929 682 851 645 775 607 701 568 630 529 562 489 496 448 433 407 373 366 317 324 264 282 214 239 167 197 125 154 86 112 51 70 20 29 -7 -12 -31 -51 -50 -90 -65 -127 -76 -162 -83 -196 -87 -227 -87 -256 -84 -283 -78 -306 -69 -326 -58 -343 -45 -356 -31 -366 -16 -371 0 -373 16 -371 31 -366 45 -356 58 -343 69 -326 78 -306 84 -283 87 -256 87 -227 83 -196 76 -162 65 -127 50 -90 31 -51 7 -12 -20 29 -51 70 -86 112 -125 154 -167 197 -214 239 -264 282 -317 324 -373 366 -433 407 -496 448 -562 489 -630 529 -701 568 -775 607 -851 645 -929 682 -1009 719 -1092 755 -1176 790 -1263 824 -1351 858 -1441 891 -1532 923 -1625 955 1594 897 1501 866 1408 834 1318 801 1229 768 1142 734 1057 699 973 664 892 627 813 590 736 552 662 514 590 474 521 434 455 394 392 353 332 311 275 269 221 226 171 183 125 140 82 97 43 54 9 12 -22 -31 -48 -72 -70 -113 -88 -152 -102 -191 -111 -227 -116 -262 -118 -295 -115 -325 -110 -352 -100 -376 -88 -397 -74 -415 -57 -429 -39 -439 -20 -445 0 -447 20 -445 39 -439 57 -429 74 -415 88 -397 100 -376 110 -352 115 -325 118 -295 116 -262 111 -227 102 -191 88 -152 70 -113 48 -72 22 -31 -9 12 -43 54 -82 97 -125 140 -171 183 -221 226 -275 269 -332 311 -392 353 -455 394 -521 434 -590 474 -662 514 -736 552 -813 590 -892 627 -973 664 -1057 699 -1142 734 -1229 768 -1318 801 -1408 834 -1501 866 -1594 897 1564 841 1469 810 1376 779 1285 747 1196 714 1108 680 1022 646 938 611 856 575 776 538 698 500 623 462 551 423 481 383 414 342 350 301 290 259 232 217 178 174 128 131 81 88 39 44 0 0 -34 -43 -64 -86 -90 -129 -111 -170 -128 -211 -140 -250 -147 -288 -151 -324 -150 -358 -145 -389 -136 -417 -124 -443 -108 -465 -90 -483 -69 -498 -47 -508 -24 -515 0 -517 24 -515 47 -508 69 -498 90 -483 108 -465 124 -443 136 -417 145 -389 150 -358 151 -324 147 -288 140 -250 128 -211 111 -170 90 -129 64 -86 34 -43 -0 0 -39 44 -81 88 -128 131 -178 174 -232 217 -290 259 -350 301 -414 342 -481 383 -551 423 -623 462 -698 500 -776 538 -856 575 -938 611 -1022 646 -1108 680 -1196 714 -1285 747 -1376 779 -1469 810 -1564 841 1534 786 1439 756 1345 726 1253 694 1163 662 1074 629 987 595 902 560 819 525 739 489 660 451 585 413 511 374 441 335 373 294 309 253 247 211 189 169 135 126 84 82 38 39 -5 -6 -44 -50 -78 -94 -107 -138 -132 -181 -153 -224 -168 -265 -179 -306 -185 -345 -186 -382 -183 -417 -175 -449 -163 -479 -148 -505 -129 -528 -107 -547 -82 -562 -56 -573 -28 -580 0 -582 28 -580 56 -573 82 -562 107 -547 129 -528 148 -505 163 -479 175 -449 183 -417 186 -382 185 -345 179 -306 168 -265 153 -224 132 -181 107 -138 78 -94 44 -50 5 -6 -38 39 -84 82 -135 126 -189 169 -247 211 -309 253 -373 294 -441 335 -511 374 -585 413 -660 451 -739 489 -819 525 -902 560 -987 595 -1074 629 -1163 662 -1253 694 -1345 726 -1439 756 -1534 786 1505 734 1409 704 1314 675 1222 644 1130 612 1041 580 953 547 867 513 784 478 702 442 623 405 546 367 472 329 401 290 333 249 267 208 205 167 147 124 92 81 41 38 -6 -6 -49 -51 -88 -95 -122 -140 -151 -184 -176 -229 -195 -272 -210 -315 -219 -356 -224 -396 -223 -435 -217 -471 -207 -504 -192 -535 -173 -562 -150 -586 -124 -606 -96 -622 -65 -634 -33 -641 0 -643 33 -641 65 -634 96 -622 124 -606 150 -586 173 -562 192 -535 207 -504 217 -471 223 -435 224 -396 219 -356 210 -315 195 -272 176 -229 151 -184 122 -140 88 -95 49 -51 6 -6 -41 38 -92 81 -147 124 -205 167 -267 208 -333 249 -401 290 -472 329 -546 367 -623 405 -702 442 -784 478 -867 513 -953 547 -1041 580 -1130 612 -1222 644 -1314 675 -1409 704 -1505 734 1476 683 1380 655 1285 625 1191 595 1099 565 1008 533 920 500 833 467 749 433 666 398 586 361 509 324 434 286 361 248 292 208 226 167 163 126 104 84 48 41 -3 -3 -51 -47 -94 -92 -133 -137 -167 -182 -196 -227 -220 -271 -239 -316 -252 -359 -261 -402 -263 -443 -261 -482 -253 -519 -240 -554 -222 -586 -199 -615 -173 -640 -143 -661 -110 -677 -75 -689 -38 -697 0 -699 38 -697 75 -689 110 -677 143 -661 173 -640 199 -615 222 -586 240 -554 253 -519 261 -482 263 -443 261 -402 252 -359 239 -316 220 -271 196 -227 167 -182 133 -137 94 -92 51 -47 3 -3 -48 41 -104 84 -163 126 -226 167 -292 208 -361 248 -434 286 -509 324 -586 361 -666 398 -749 433 -833 467 -920 500 -1008 533 -1099 565 -1191 595 -1285 625 -1380 655 -1476 683 1449 634 1351 606 1255 578 1161 549 1068 519 977 488 887 457 800 424 714 391 631 356 550 321 471 284 396 247 322 209 252 170 185 130 122 89 62 47 5 4 -47 -39 -95 -83 -139 -128 -178 -173 -212 -218 -241 -264 -265 -309 -283 -354 -296 -398 -303 -442 -304 -484 -300 -524 -289 -563 -274 -599 -253 -632 -227 -661 -196 -687 -162 -709 -125 -726 -84 -739 -43 -747 0 -749 43 -747 84 -739 125 -726 162 -709 196 -687 227 -661 253 -632 274 -599 289 -563 300 -524 304 -484 303 -442 296 -398 283 -354 265 -309 241 -264 212 -218 178 -173 139 -128 95 -83 47 -39 -5 4 -62 47 -122 89 -185 130 -252 170 -322 209 -396 247 -471 284 -550 321 -631 356 -714 391 -800 424 -887 457 -977 488 -1068 519 -1161 549 -1255 578 -1351 606 -1449 634 1422 587 1324 560 1227 533 1132 505 1038 476 946 446 856 415 767 384 681 351 596 317 515 283 435 248 358 211 284 174 213 135 145 96 81 55 20 14 -38 -28 -91 -71 -140 -115 -184 -160 -223 -205 -258 -250 -287 -296 -310 -341 -328 -387 -340 -432 -346 -476 -346 -519 -340 -560 -327 -600 -309 -637 -285 -671 -255 -702 -221 -728 -182 -751 -140 -769 -95 -782 -48 -790 0 -793 48 -790 95 -782 140 -769 182 -751 221 -728 255 -702 285 -671 309 -637 327 -600 340 -560 346 -519 346 -476 340 -432 328 -387 310 -341 287 -296 258 -250 223 -205 184 -160 140 -115 91 -71 38 -28 -20 14 -81 55 -145 96 -213 135 -284 174 -358 211 -435 248 -515 283 -596 317 -681 351 -767 384 -856 415 -946 446 -1038 476 -1132 505 -1227 533 -1324 560 -1422 587 1397 541 1298 516 1200 489 1104 462 1009 434 916 406 825 376 736 345 648 314 563 281 480 248 400 214 322 178 247 142 174 104 106 65 40 26 -22 -15 -80 -56 -134 -99 -184 -142 -228 -186 -268 -231 -303 -276 -332 -322 -356 -368 -374 -414 -385 -459 -390 -504 -389 -548 -381 -590 -366 -630 -345 -668 -318 -703 -285 -735 -246 -763 -203 -787 -156 -805 -106 -819 -53 -827 0 -830 53 -827 106 -819 156 -805 203 -787 246 -763 285 -735 318 -703 345 -668 366 -630 381 -590 389 -548 390 -504 385 -459 374 -414 356 -368 332 -322 303 -276 268 -231 228 -186 184 -142 134 -99 80 -56 22 -15 -40 26 -106 65 -174 104 -247 142 -322 178 -400 214 -480 248 -563 281 -648 314 -736 345 -825 376 -916 406 -1009 434 -1104 462 -1200 489 -1298 516 -1397 541 1372 497 1272 473 1174 448 1077 422 981 395 888 368 795 339 705 310 617 279 531 248 447 216 365 183 286 148 210 113 137 76 67 39 0 0 -63 -39 -122 -80 -177 -122 -227 -165 -273 -208 -313 -252 -349 -297 -378 -343 -402 -389 -419 -434 -430 -480 -435 -525 -432 -569 -422 -612 -406 -653 -382 -692 -352 -728 -315 -761 -272 -790 -225 -814 -173 -834 -117 -848 -59 -857 0 -860 59 -857 117 -848 173 -834 225 -814 272 -790 315 -761 352 -728 382 -692 406 -653 422 -612 432 -569 435 -525 430 -480 419 -434 402 -389 378 -343 349 -297 313 -252 273 -208 227 -165 177 -122 122 -80 63 -39 -0 0 -67 39 -137 76 -210 113 -286 148 -365 183 -447 216 -531 248 -617 279 -705 310 -795 339 -888 368 -981 395 -1077 422 -1174 448 -1272 473 -1372 497 1349 455 1248 432 1149 408 1051 384 955 358 860 332 767 305 676 276 587 247 499 217 415 187 332 155 252 122 175 87 101 52 29 16 -38 -21 -102 -60 -162 -100 -218 -140 -270 -182 -316 -225 -358 -268 -394 -313 -424 -358 -448 -403 -465 -449 -476 -494 -479 -539 -476 -584 -465 -627 -446 -669 -420 -709 -386 -745 -346 -779 -299 -809 -247 -834 -190 -854 -129 -869 -65 -878 0 -881 65 -878 129 -869 190 -854 247 -834 299 -809 346 -779 386 -745 420 -709 446 -669 465 -627 476 -584 479 -539 476 -494 465 -449 448 -403 424 -358 394 -313 358 -268 316 -225 270 -182 218 -140 162 -100 102 -60 38 -21 -29 16 -101 52 -175 87 -252 122 -332 155 -415 187 -499 217 -587 247 -676 276 -767 305 -860 332 -955 358 -1051 384 -1149 408 -1248 432 -1349 455 1327 415 1225 393 1125 370 1027 347 930 323 834 298 740 272 648 245 558 218 470 189 384 160 300 129 219 98 141 65 65 31 -7 -3 -76 -39 -141 -76 -202 -115 -259 -154 -311 -195 -359 -236 -401 -279 -438 -322 -469 -366 -493 -411 -511 -456 -521 -501 -524 -546 -520 -591 -507 -634 -487 -676 -458 -716 -422 -754 -378 -788 -327 -818 -270 -844 -208 -865 -141 -880 -71 -889 0 -892 71 -889 141 -880 208 -865 270 -844 327 -818 378 -788 422 -754 458 -716 487 -676 507 -634 520 -591 524 -546 521 -501 511 -456 493 -411 469 -366 438 -322 401 -279 359 -236 311 -195 259 -154 202 -115 141 -76 76 -39 7 -3 -65 31 -141 65 -219 98 -300 129 -384 160 -470 189 -558 218 -648 245 -740 272 -834 298 -930 323 -1027 347 -1125 370 -1225 393 -1327 415 1306 375 1204 355 1103 334 1004 312 906 289 809 266 715 242 622 217 531 191 442 164 355 136 270 107 188 77 109 46 32 14 -41 -19 -111 -53 -178 -89 -240 -125 -298 -163 -352 -202 -400 -242 -443 -283 -481 -325 -513 -368 -538 -412 -556 -456 -566 -501 -569 -545 -564 -589 -550 -633 -528 -675 -497 -715 -458 -753 -411 -787 -356 -818 -294 -844 -226 -865 -153 -881 -77 -890 0 -894 77 -890 153 -881 226 -865 294 -844 356 -818 411 -787 458 -753 497 -715 528 -675 550 -633 564 -589 569 -545 566 -501 556 -456 538 -412 513 -368 481 -325 443 -283 400 -242 352 -202 298 -163 240 -125 178 -89 111 -53 41 -19 -32 14 -109 46 -188 77 -270 107 -355 136 -442 164 -531 191 -622 217 -715 242 -809 266 -906 289 -1004 312 -1103 334 -1204 355 -1306 375 1286 338 1184 319 1082 299 982 279 884 258 786 236 691 213 597 190 505 166 415 141 327 114 242 87 158 59 78 30 0 0 -74 -31 -145 -64 -213 -97 -276 -132 -335 -168 -390 -205 -440 -243 -484 -282 -523 -323 -555 -364 -581 -407 -599 -450 -610 -493 -613 -536 -607 -580 -593 -623 -569 -664 -536 -704 -494 -742 -444 -776 -384 -807 -318 -834 -244 -855 -166 -871 -84 -880 0 -884 84 -880 166 -871 244 -855 318 -834 384 -807 444 -776 494 -742 536 -704 569 -664 593 -623 607 -580 613 -536 610 -493 599 -450 581 -407 555 -364 523 -323 484 -282 440 -243 390 -205 335 -168 276 -132 213 -97 145 -64 74 -31 -0 0 -78 30 -158 59 -242 87 -327 114 -415 141 -505 166 -597 190 -691 213 -786 236 -884 258 -982 279 -1082 299 -1184 319 -1286 338 1269 301 1165 284 1063 266 962 247 863 228 765 208 669 187 574 165 481 143 390 120 302 95 215 70 131 44 49 17 -29 -11 -105 -40 -177 -70 -246 -101 -310 -134 -371 -168 -427 -203 -478 -239 -523 -276 -563 -314 -596 -354 -623 -394 -642 -435 -653 -477 -656 -519 -650 -561 -635 -603 -610 -644 -575 -683 -531 -720 -476 -754 -413 -785 -342 -811 -263 -833 -179 -848 -90 -858 0 -861 90 -858 179 -848 263 -833 342 -811 413 -785 476 -754 531 -720 575 -683 610 -644 635 -603 650 -561 656 -519 653 -477 642 -435 623 -394 596 -354 563 -314 523 -276 478 -239 427 -203 371 -168 310 -134 246 -101 177 -70 105 -40 29 -11 -49 17 -131 44 -215 70 -302 95 -390 120 -481 143 -574 165 -669 187 -765 208 -863 228 -962 247 -1063 266 -1165 284 -1269 301 1252 266 1148 250 1046 234 944 217 844 199 746 181 649 162 553 142 459 122 368 101 278 79 190 56 105 32 23 7 -57 -19 -133 -45 -207 -73 -276 -102 -342 -132 -404 -164 -461 -196 -513 -230 -560 -264 -601 -300 -635 -337 -662 -375 -682 -414 -694 -454 -697 -494 -691 -534 -675 -574 -649 -613 -613 -651 -566 -687 -509 -721 -441 -751 -365 -776 -281 -797 -191 -813 -97 -822 0 -825 97 -822 191 -813 281 -797 365 -776 441 -751 509 -721 566 -687 613 -651 649 -613 675 -574 691 -534 697 -494 694 -454 682 -414 662 -375 635 -337 601 -300 560 -264 513 -230 461 -196 404 -164 342 -132 276 -102 207 -73 133 -45 57 -19 -23 7 -105 32 -190 56 -278 79 -368 101 -459 122 -553 142 -649 162 -746 181 -844 199 -944 217 -1046 234 -1148 250 -1252 266 1238 232 1133 218 1030 203 928 188 827 172 728 156 630 139 534 121 440 103 347 84 257 64 168 44 82 22 -1 -0 -82 -24 -159 -48 -234 -73 -305 -99 -372 -127 -434 -155 -493 -185 -546 -215 -594 -247 -636 -280 -671 -315 -699 -350 -720 -386 -733 -423 -736 -460 -730 -498 -714 -535 -687 -572 -649 -609 -600 -643 -540 -675 -469 -703 -388 -728 -299 -748 -203 -763 -103 -772 0 -775 103 -772 203 -763 299 -748 388 -728 469 -703 540 -675 600 -643 649 -609 687 -572 714 -535 730 -498 736 -460 733 -423 720 -386 699 -350 671 -315 636 -280 594 -247 546 -215 493 -185 434 -155 372 -127 305 -99 234 -73 159 -48 82 -24 1 -0 -82 22 -168 44 -257 64 -347 84 -440 103 -534 121 -630 139 -728 156 -827 172 -928 188 -1030 203 -1133 218 -1238 232 1225 199 1120 187 1016 174 913 160 812 147 712 132 614 117 517 102 422 86 329 69 238 51 148 33 62 14 -23 -5 -104 -26 -183 -48 -258 -70 -330 -93 -398 -118 -462 -143 -521 -169 -576 -197 -625 -226 -668 -255 -704 -286 -733 -318 -755 -351 -768 -384 -772 -418 -766 -453 -750 -487 -722 -522 -683 -555 -632 -587 -569 -617 -495 -643 -410 -666 -316 -685 -215 -698 -109 -707 0 -710 109 -707 215 -698 316 -685 410 -666 495 -643 569 -617 632 -587 683 -555 722 -522 750 -487 766 -453 772 -418 768 -384 755 -351 733 -318 704 -286 668 -255 625 -226 576 -197 521 -169 462 -143 398 -118 330 -93 258 -70 183 -48 104 -26 23 -5 -62 14 -148 33 -238 51 -329 69 -422 86 -517 102 -614 117 -712 132 -812 147 -913 160 -1016 174 -1120 187 -1225 199 1213 167 1108 156 1004 145 901 134 799 122 699 110 600 97 502 84 407 70 313 56 221 41 131 25 44 9 -41 -8 -124 -26 -203 -45 -279 -64 -352 -84 -421 -105 -486 -127 -547 -150 -602 -174 -652 -199 -696 -225 -733 -252 -764 -280 -786 -309 -800 -339 -805 -369 -799 -400 -783 -430 -755 -461 -714 -491 -661 -520 -596 -546 -519 -570 -430 -591 -331 -608 -225 -620 -114 -627 0 -630 114 -627 225 -620 331 -608 430 -591 519 -570 596 -546 661 -520 714 -491 755 -461 783 -430 799 -400 805 -369 800 -339 786 -309 764 -280 733 -252 696 -225 652 -199 602 -174 547 -150 486 -127 421 -105 352 -84 279 -64 203 -45 124 -26 41 -8 -44 9 -131 25 -221 41 -313 56 -407 70 -502 84 -600 97 -699 110 -799 122 -901 134 -1004 145 -1108 156 -1213 167 1204 135 1098 127 994 118 890 108 788 99 687 88 588 78 490 67 394 55 299 43 207 31 117 18 28 5 -57 -10 -140 -24 -221 -40 -298 -56 -371 -73 -441 -90 -507 -109 -568 -128 -624 -148 -675 -169 -720 -191 -759 -213 -790 -237 -813 -261 -828 -287 -833 -312 -828 -339 -811 -365 -783 -391 -742 -417 -687 -442 -620 -465 -539 -485 -447 -503 -345 -517 -234 -527 -119 -534 0 -536 119 -534 234 -527 345 -517 447 -503 539 -485 620 -465 687 -442 742 -417 783 -391 811 -365 828 -339 833 -312 828 -287 813 -261 790 -237 759 -213 720 -191 675 -169 624 -148 568 -128 507 -109 441 -90 371 -73 298 -56 221 -40 140 -24 57 -10 -28 5 -117 18 -207 31 -299 43 -394 55 -490 67 -588 78 -687 88 -788 99 -890 108 -994 118 -1098 127 -1204 135 1196 105 1090 98 985 91 882 83 779 76 678 68 578 60 480 51 383 42 289 33 196 23 105 13 16 2 -70 -9 -154 -21 -235 -33 -312 -46 -387 -59 -457 -73 -524 -87 -586 -102 -643 -118 -695 -135 -740 -152 -780 -171 -812 -189 -836 -209 -851 -229 -857 -250 -852 -271 -835 -292 -807 -314 -765 -335 -709 -355 -640 -373 -557 -390 -461 -404 -356 -415 -242 -423 -122 -428 0 -429 122 -428 242 -423 356 -415 461 -404 557 -390 640 -373 709 -355 765 -335 807 -314 835 -292 852 -271 857 -250 851 -229 836 -209 812 -189 780 -171 740 -152 695 -135 643 -118 586 -102 524 -87 457 -73 387 -59 312 -46 235 -33 154 -21 70 -9 -16 2 -105 13 -196 23 -289 33 -383 42 -480 51 -578 60 -678 68 -779 76 -882 83 -985 91 -1090 98 -1196 105 1190 74 1084 70 979 64 875 59 773 54 671 48 571 42 473 36 376 29 280 23 187 16 96 8 7 1 -80 -7 -164 -16 -245 -25 -324 -34 -398 -43 -469 -53 -537 -64 -599 -75 -657 -86 -709 -99 -756 -111 -796 -124 -828 -138 -853 -152 -869 -167 -875 -182 -870 -198 -854 -213 -825 -229 -783 -245 -726 -259 -655 -273 -570 -285 -472 -295 -364 -303 -247 -309 -125 -312 0 -313 125 -312 247 -309 364 -303 472 -295 570 -285 655 -273 726 -259 783 -245 825 -229 854 -213 870 -198 875 -182 869 -167 853 -152 828 -138 796 -124 756 -111 709 -99 657 -86 599 -75 537 -64 469 -53 398 -43 324 -34 245 -25 164 -16 80 -7 -7 1 -96 8 -187 16 -280 23 -376 29 -473 36 -571 42 -671 48 -773 54 -875 59 -979 64 -1084 70 -1190 74 1187 44 1080 42 975 38 871 35 768 32 666 29 566 25 467 21 370 17 275 13 181 9 90 5 0 0 -87 -5 -171 -10 -253 -15 -331 -21 -406 -26 -478 -33 -545 -39 -608 -46 -666 -53 -719 -60 -766 -68 -806 -76 -840 -84 -865 -93 -881 -102 -887 -111 -883 -120 -867 -130 -838 -140 -795 -149 -737 -158 -665 -166 -579 -174 -480 -180 -369 -185 -251 -188 -127 -190 0 -191 127 -190 251 -188 369 -185 480 -180 579 -174 665 -166 737 -158 795 -149 838 -140 867 -130 883 -120 887 -111 881 -102 865 -93 840 -84 806 -76 766 -68 719 -60 666 -53 608 -46 545 -39 478 -33 406 -26 331 -21 253 -15 171 -10 87 -5 -0 0 -90 5 -181 9 -275 13 -370 17 -467 21 -566 25 -666 29 -768 32 -871 35 -975 38 -1080 42 -1187 44 1185 15 1078 14 973 13 869 12 766 11 664 9 564 8 465 7 368 6 272 4 178 3 87 1 -3 -0 -90 -2 -174 -3 -256 -5 -335 -7 -410 -9 -482 -11 -550 -13 -613 -15 -671 -18 -724 -20 -771 -23 -812 -25 -845 -28 -871 -31 -887 -34 -894 -37 -889 -40 -873 -44 -844 -47 -801 -50 -743 -53 -671 -56 -584 -58 -483 -60 -372 -62 -253 -63 -128 -64 0 -64 128 -64 253 -63 372 -62 483 -60 584 -58 671 -56 743 -53 801 -50 844 -47 873 -44 889 -40 894 -37 887 -34 871 -31 845 -28 812 -25 771 -23 724 -20 671 -18 613 -15 550 -13 482 -11 410 -9 335 -7 256 -5 174 -3 90 -2 3 -0 -87 1 -178 3 -272 4 -368 6 -465 7 -564 8 -664 9 -766 11 -869 12 -973 13 -1078 14 -1185 15 1185 -15 1078 -14 973 -13 869 -12 766 -11 664 -9 564 -8 465 -7 368 -6 272 -4 178 -3 87 -1 -3 0 -90 2 -174 3 -256 5 -335 7 -410 9 -482 11 -550 13 -613 15 -671 18 -724 20 -771 23 -812 25 -845 28 -871 31 -887 34 -894 37 -889 40 -873 44 -844 47 -801 50 -743 53 -671 56 -584 58 -483 60 -372 62 -253 63 -128 64 0 64 128 64 253 63 372 62 483 60 584 58 671 56 743 53 801 50 844 47 873 44 889 40 894 37 887 34 871 31 845 28 812 25 771 23 724 20 671 18 613 15 550 13 482 11 410 9 335 7 256 5 174 3 90 2 3 0 -87 -1 -178 -3 -272 -4 -368 -6 -465 -7 -564 -8 -664 -9 -766 -11 -869 -12 -973 -13 -1078 -14 -1185 -15 1187 -44 1080 -42 975 -38 871 -35 768 -32 666 -29 566 -25 467 -21 370 -17 275 -13 181 -9 90 -5 0 -0 -87 5 -171 10 -253 15 -331 21 -406 26 -478 33 -545 39 -608 46 -666 53 -719 60 -766 68 -806 76 -840 84 -865 93 -881 102 -887 111 -883 120 -867 130 -838 140 -795 149 -737 158 -665 166 -579 174 -480 180 -369 185 -251 188 -127 190 0 191 127 190 251 188 369 185 480 180 579 174 665 166 737 158 795 149 838 140 867 130 883 120 887 111 881 102 865 93 840 84 806 76 766 68 719 60 666 53 608 46 545 39 478 33 406 26 331 21 253 15 171 10 87 5 -0 -0 -90 -5 -181 -9 -275 -13 -370 -17 -467 -21 -566 -25 -666 -29 -768 -32 -871 -35 -975 -38 -1080 -42 -1187 -44 1190 -74 1084 -70 979 -64 875 -59 773 -54 671 -48 571 -42 473 -36 376 -29 280 -23 187 -16 96 -8 7 -1 -80 7 -164 16 -245 25 -324 34 -398 43 -469 53 -537 64 -599 75 -657 86 -709 99 -756 111 -796 124 -828 138 -853 152 -869 167 -875 182 -870 198 -854 213 -825 229 -783 245 -726 259 -655 273 -570 285 -472 295 -364 303 -247 309 -125 312 0 313 125 312 247 309 364 303 472 295 570 285 655 273 726 259 783 245 825 229 854 213 870 198 875 182 869 167 853 152 828 138 796 124 756 111 709 99 657 86 599 75 537 64 469 53 398 43 324 34 245 25 164 16 80 7 -7 -1 -96 -8 -187 -16 -280 -23 -376 -29 -473 -36 -571 -42 -671 -48 -773 -54 -875 -59 -979 -64 -1084 -70 -1190 -74 1196 -105 1090 -98 985 -91 882 -83 779 -76 678 -68 578 -60 480 -51 383 -42 289 -33 196 -23 105 -13 16 -2 -70 9 -154 21 -235 33 -312 46 -387 59 -457 73 -524 87 -586 102 -643 118 -695 135 -740 152 -780 171 -812 189 -836 209 -851 229 -857 250 -852 271 -835 292 -807 314 -765 335 -709 355 -640 373 -557 390 -461 404 -356 415 -242 423 -122 428 0 429 122 428 242 423 356 415 461 404 557 390 640 373 709 355 765 335 807 314 835 292 852 271 857 250 851 229 836 209 812 189 780 171 740 152 695 135 643 118 586 102 524 87 457 73 387 59 312 46 235 33 154 21 70 9 -16 -2 -105 -13 -196 -23 -289 -33 -383 -42 -480 -51 -578 -60 -678 -68 -779 -76 -882 -83 -985 -91 -1090 -98 -1196 -105 1204 -135 1098 -127 994 -118 890 -108 788 -99 687 -88 588 -78 490 -67 394 -55 299 -43 207 -31 117 -18 28 -5 -57 10 -140 24 -221 40 -298 56 -371 73 -441 90 -507 109 -568 128 -624 148 -675 169 -720 191 -759 213 -790 237 -813 261 -828 287 -833 312 -828 339 -811 365 -783 391 -742 417 -687 442 -620 465 -539 485 -447 503 -345 517 -234 527 -119 534 0 536 119 534 234 527 345 517 447 503 539 485 620 465 687 442 742 417 783 391 811 365 828 339 833 312 828 287 813 261 790 237 759 213 720 191 675 169 624 148 568 128 507 109 441 90 371 73 298 56 221 40 140 24 57 10 -28 -5 -117 -18 -207 -31 -299 -43 -394 -55 -490 -67 -588 -78 -687 -88 -788 -99 -890 -108 -994 -118 -1098 -127 -1204 -135 1213 -167 1108 -156 1004 -145 901 -134 799 -122 699 -110 600 -97 502 -84 407 -70 313 -56 221 -41 131 -25 44 -9 -41 8 -124 26 -203 45 -279 64 -352 84 -421 105 -486 127 -547 150 -602 174 -652 199 -696 225 -733 252 -764 280 -786 309 -800 339 -805 369 -799 400 -783 430 -755 461 -714 491 -661 520 -596 546 -519 570 -430 591 -331 608 -225 620 -114 627 0 630 114 627 225 620 331 608 430 591 519 570 596 546 661 520 714 491 755 461 783 430 799 400 805 369 800 339 786 309 764 280 733 252 696 225 652 199 602 174 547 150 486 127 421 105 352 84 279 64 203 45 124 26 41 8 -44 -9 -131 -25 -221 -41 -313 -56 -407 -70 -502 -84 -600 -97 -699 -110 -799 -122 -901 -134 -1004 -145 -1108 -156 -1213 -167 1225 -199 1120 -187 1016 -174 913 -160 812 -147 712 -132 614 -117 517 -102 422 -86 329 -69 238 -51 148 -33 62 -14 -23 5 -104 26 -183 48 -258 70 -330 93 -398 118 -462 143 -521 169 -576 197 -625 226 -668 255 -704 286 -733 318 -755 351 -768 384 -772 418 -766 453 -750 487 -722 522 -683 555 -632 587 -569 617 -495 643 -410 666 -316 685 -215 698 -109 707 0 710 109 707 215 698 316 685 410 666 495 643 569 617 632 587 683 555 722 522 750 487 766 453 772 418 768 384 755 351 733 318 704 286 668 255 625 226 576 197 521 169 462 143 398 118 330 93 258 70 183 48 104 26 23 5 -62 -14 -148 -33 -238 -51 -329 -69 -422 -86 -517 -102 -614 -117 -712 -132 -812 -147 -913 -160 -1016 -174 -1120 -187 -1225 -199 1238 -232 1133 -218 1030 -203 928 -188 827 -172 728 -156 630 -139 534 -121 440 -103 347 -84 257 -64 168 -44 82 -22 -1 0 -82 24 -159 48 -234 73 -305 99 -372 127 -434 155 -493 185 -546 215 -594 247 -636 280 -671 315 -699 350 -720 386 -733 423 -736 460 -730 498 -714 535 -687 572 -649 609 -600 643 -540 675 -469 703 -388 728 -299 748 -203 763 -103 772 0 775 103 772 203 763 299 748 388 728 469 703 540 675 600 643 649 609 687 572 714 535 730 498 736 460 733 423 720 386 699 350 671 315 636 280 594 247 546 215 493 185 434 155 372 127 305 99 234 73 159 48 82 24 1 0 -82 -22 -168 -44 -257 -64 -347 -84 -440 -103 -534 -121 -630 -139 -728 -156 -827 -172 -928 -188 -1030 -203 -1133 -218 -1238 -232 1252 -266 1148 -250 1046 -234 944 -217 844 -199 746 -181 649 -162 553 -142 459 -122 368 -101 278 -79 190 -56 105 -32 23 -7 -57 19 -133 45 -207 73 -276 102 -342 132 -404 164 -461 196 -513 230 -560 264 -601 300 -635 337 -662 375 -682 414 -694 454 -697 494 -691 534 -675 574 -649 613 -613 651 -566 687 -509 721 -441 751 -365 776 -281 797 -191 813 -97 822 0 825 97 822 191 813 281 797 365 776 441 751 509 721 566 687 613 651 649 613 675 574 691 534 697 494 694 454 682 414 662 375 635 337 601 300 560 264 513 230 461 196 404 164 342 132 276 102 207 73 133 45 57 19 -23 -7 -105 -32 -190 -56 -278 -79 -368 -101 -459 -122 -553 -142 -649 -162 -746 -181 -844 -199 -944 -217 -1046 -234 -1148 -250 -1252 -266 1269 -301 1165 -284 1063 -266 962 -247 863 -228 765 -208 669 -187 574 -165 481 -143 390 -120 302 -95 215 -70 131 -44 49 -17 -29 11 -105 40 -177 70 -246 101 -310 134 -371 168 -427 203 -478 239 -523 276 -563 314 -596 354 -623 394 -642 435 -653 477 -656 519 -650 561 -635 603 -610 644 -575 683 -531 720 -476 754 -413 785 -342 811 -263 833 -179 848 -90 858 0 861 90 858 179 848 263 833 342 811 413 785 476 754 531 720 575 683 610 644 635 603 650 561 656 519 653 477 642 435 623 394 596 354 563 314 523 276 478 239 427 203 371 168 310 134 246 101 177 70 105 40 29 11 -49 -17 -131 -44 -215 -70 -302 -95 -390 -120 -481 -143 -574 -165 -669 -187 -765 -208 -863 -228 -962 -247 -1063 -266 -1165 -284 -1269 -301 1286 -338 1184 -319 1082 -299 982 -279 884 -258 786 -236 691 -213 597 -190 505 -166 415 -141 327 -114 242 -87 158 -59 78 -30 0 -0 -74 31 -145 64 -213 97 -276 132 -335 168 -390 205 -440 243 -484 282 -523 323 -555 364 -581 407 -599 450 -610 493 -613 536 -607 580 -593 623 -569 664 -536 704 -494 742 -444 776 -384 807 -318 834 -244 855 -166 871 -84 880 0 884 84 880 166 871 244 855 318 834 384 807 444 776 494 742 536 704 569 664 593 623 607 580 613 536 610 493 599 450 581 407 555 364 523 323 484 282 440 243 390 205 335 168 276 132 213 97 145 64 74 31 -0 -0 -78 -30 -158 -59 -242 -87 -327 -114 -415 -141 -505 -166 -597 -190 -691 -213 -786 -236 -884 -258 -982 -279 -1082 -299 -1184 -319 -1286 -338 1306 -375 1204 -355 1103 -334 1004 -312 906 -289 809 -266 715 -242 622 -217 531 -191 442 -164 355 -136 270 -107 188 -77 109 -46 32 -14 -41 19 -111 53 -178 89 -240 125 -298 163 -352 202 -400 242 -443 283 -481 325 -513 368 -538 412 -556 456 -566 501 -569 545 -564 589 -550 633 -528 675 -497 715 -458 753 -411 787 -356 818 -294 844 -226 865 -153 881 -77 890 0 894 77 890 153 881 226 865 294 844 356 818 411 787 458 753 497 715 528 675 550 633 564 589 569 545 566 501 556 456 538 412 513 368 481 325 443 283 400 242 352 202 298 163 240 125 178 89 111 53 41 19 -32 -14 -109 -46 -188 -77 -270 -107 -355 -136 -442 -164 -531 -191 -622 -217 -715 -242 -809 -266 -906 -289 -1004 -312 -1103 -334 -1204 -355 -1306 -375 1327 -415 1225 -393 1125 -370 1027 -347 930 -323 834 -298 740 -272 648 -245 558 -218 470 -189 384 -160 300 -129 219 -98 141 -65 65 -31 -7 3 -76 39 -141 76 -202 115 -259 154 -311 195 -359 236 -401 279 -438 322 -469 366 -493 411 -511 456 -521 501 -524 546 -520 591 -507 634 -487 676 -458 716 -422 754 -378 788 -327 818 -270 844 -208 865 -141 880 -71 889 0 892 71 889 141 880 208 865 270 844 327 818 378 788 422 754 458 716 487 676 507 634 520 591 524 546 521 501 511 456 493 411 469 366 438 322 401 279 359 236 311 195 259 154 202 115 141 76 76 39 7 3 -65 -31 -141 -65 -219 -98 -300 -129 -384 -160 -470 -189 -558 -218 -648 -245 -740 -272 -834 -298 -930 -323 -1027 -347 -1125 -370 -1225 -393 -1327 -415 1349 -455 1248 -432 1149 -408 1051 -384 955 -358 860 -332 767 -305 676 -276 587 -247 499 -217 415 -187 332 -155 252 -122 175 -87 101 -52 29 -16 -38 21 -102 60 -162 100 -218 140 -270 182 -316 225 -358 268 -394 313 -424 358 -448 403 -465 449 -476 494 -479 539 -476 584 -465 627 -446 669 -420 709 -386 745 -346 779 -299 809 -247 834 -190 854 -129 869 -65 878 0 881 65 878 129 869 190 854 247 834 299 809 346 779 386 745 420 709 446 669 465 627 476 584 479 539 476 494 465 449 448 403 424 358 394 313 358 268 316 225 270 182 218 140 162 100 102 60 38 21 -29 -16 -101 -52 -175 -87 -252 -122 -332 -155 -415 -187 -499 -217 -587 -247 -676 -276 -767 -305 -860 -332 -955 -358 -1051 -384 -1149 -408 -1248 -432 -1349 -455 1372 -497 1272 -473 1174 -448 1077 -422 981 -395 888 -368 795 -339 705 -310 617 -279 531 -248 447 -216 365 -183 286 -148 210 -113 137 -76 67 -39 0 -0 -63 39 -122 80 -177 122 -227 165 -273 208 -313 252 -349 297 -378 343 -402 389 -419 434 -430 480 -435 525 -432 569 -422 612 -406 653 -382 692 -352 728 -315 761 -272 790 -225 814 -173 834 -117 848 -59 857 0 860 59 857 117 848 173 834 225 814 272 790 315 761 352 728 382 692 406 653 422 612 432 569 435 525 430 480 419 434 402 389 378 343 349 297 313 252 273 208 227 165 177 122 122 80 63 39 -0 -0 -67 -39 -137 -76 -210 -113 -286 -148 -365 -183 -447 -216 -531 -248 -617 -279 -705 -310 -795 -339 -888 -368 -981 -395 -1077 -422 -1174 -448 -1272 -473 -1372 -497 1397 -541 1298 -516 1200 -489 1104 -462 1009 -434 916 -406 825 -376 736 -345 648 -314 563 -281 480 -248 400 -214 322 -178 247 -142 174 -104 106 -65 40 -26 -22 15 -80 56 -134 99 -184 142 -228 186 -268 231 -303 276 -332 322 -356 368 -374 414 -385 459 -390 504 -389 548 -381 590 -366 630 -345 668 -318 703 -285 735 -246 763 -203 787 -156 805 -106 819 -53 827 0 830 53 827 106 819 156 805 203 787 246 763 285 735 318 703 345 668 366 630 381 590 389 548 390 504 385 459 374 414 356 368 332 322 303 276 268 231 228 186 184 142 134 99 80 56 22 15 -40 -26 -106 -65 -174 -104 -247 -142 -322 -178 -400 -214 -480 -248 -563 -281 -648 -314 -736 -345 -825 -376 -916 -406 -1009 -434 -1104 -462 -1200 -489 -1298 -516 -1397 -541 1422 -587 1324 -560 1227 -533 1132 -505 1038 -476 946 -446 856 -415 767 -384 681 -351 596 -317 515 -283 435 -248 358 -211 284 -174 213 -135 145 -96 81 -55 20 -14 -38 28 -91 71 -140 115 -184 160 -223 205 -258 250 -287 296 -310 341 -328 387 -340 432 -346 476 -346 519 -340 560 -327 600 -309 637 -285 671 -255 702 -221 728 -182 751 -140 769 -95 782 -48 790 0 793 48 790 95 782 140 769 182 751 221 728 255 702 285 671 309 637 327 600 340 560 346 519 346 476 340 432 328 387 310 341 287 296 258 250 223 205 184 160 140 115 91 71 38 28 -20 -14 -81 -55 -145 -96 -213 -135 -284 -174 -358 -211 -435 -248 -515 -283 -596 -317 -681 -351 -767 -384 -856 -415 -946 -446 -1038 -476 -1132 -505 -1227 -533 -1324 -560 -1422 -587 1449 -634 1351 -606 1255 -578 1161 -549 1068 -519 977 -488 887 -457 800 -424 714 -391 631 -356 550 -321 471 -284 396 -247 322 -209 252 -170 185 -130 122 -89 62 -47 5 -4 -47 39 -95 83 -139 128 -178 173 -212 218 -241 264 -265 309 -283 354 -296 398 -303 442 -304 484 -300 524 -289 563 -274 599 -253 632 -227 661 -196 687 -162 709 -125 726 -84 739 -43 747 0 749 43 747 84 739 125 726 162 709 196 687 227 661 253 632 274 599 289 563 300 524 304 484 303 442 296 398 283 354 265 309 241 264 212 218 178 173 139 128 95 83 47 39 -5 -4 -62 -47 -122 -89 -185 -130 -252 -170 -322 -209 -396 -247 -471 -284 -550 -321 -631 -356 -714 -391 -800 -424 -887 -457 -977 -488 -1068 -519 -1161 -549 -1255 -578 -1351 -606 -1449 -634 1476 -683 1380 -655 1285 -625 1191 -595 1099 -565 1008 -533 920 -500 833 -467 749 -433 666 -398 586 -361 509 -324 434 -286 361 -248 292 -208 226 -167 163 -126 104 -84 48 -41 -3 3 -51 47 -94 92 -133 137 -167 182 -196 227 -220 271 -239 316 -252 359 -261 402 -263 443 -261 482 -253 519 -240 554 -222 586 -199 615 -173 640 -143 661 -110 677 -75 689 -38 697 0 699 38 697 75 689 110 677 143 661 173 640 199 615 222 586 240 554 253 519 261 482 263 443 261 402 252 359 239 316 220 271 196 227 167 182 133 137 94 92 51 47 3 3 -48 -41 -104 -84 -163 -126 -226 -167 -292 -208 -361 -248 -434 -286 -509 -324 -586 -361 -666 -398 -749 -433 -833 -467 -920 -500 -1008 -533 -1099 -565 -1191 -595 -1285 -625 -1380 -655 -1476 -683 1505 -734 1409 -704 1314 -675 1222 -644 1130 -612 1041 -580 953 -547 867 -513 784 -478 702 -442 623 -405 546 -367 472 -329 401 -290 333 -249 267 -208 205 -167 147 -124 92 -81 41 -38 -6 6 -49 51 -88 95 -122 140 -151 184 -176 229 -195 272 -210 315 -219 356 -224 396 -223 435 -217 471 -207 504 -192 535 -173 562 -150 586 -124 606 -96 622 -65 634 -33 641 0 643 33 641 65 634 96 622 124 606 150 586 173 562 192 535 207 504 217 471 223 435 224 396 219 356 210 315 195 272 176 229 151 184 122 140 88 95 49 51 6 6 -41 -38 -92 -81 -147 -124 -205 -167 -267 -208 -333 -249 -401 -290 -472 -329 -546 -367 -623 -405 -702 -442 -784 -478 -867 -513 -953 -547 -1041 -580 -1130 -612 -1222 -644 -1314 -675 -1409 -704 -1505 -734 1534 -786 1439 -756 1345 -726 1253 -694 1163 -662 1074 -629 987 -595 902 -560 819 -525 739 -489 660 -451 585 -413 511 -374 441 -335 373 -294 309 -253 247 -211 189 -169 135 -126 84 -82 38 -39 -5 6 -44 50 -78 94 -107 138 -132 181 -153 224 -168 265 -179 306 -185 345 -186 382 -183 417 -175 449 -163 479 -148 505 -129 528 -107 547 -82 562 -56 573 -28 580 0 582 28 580 56 573 82 562 107 547 129 528 148 505 163 479 175 449 183 417 186 382 185 345 179 306 168 265 153 224 132 181 107 138 78 94 44 50 5 6 -38 -39 -84 -82 -135 -126 -189 -169 -247 -211 -309 -253 -373 -294 -441 -335 -511 -374 -585 -413 -660 -451 -739 -489 -819 -525 -902 -560 -987 -595 -1074 -629 -1163 -662 -1253 -694 -1345 -726 -1439 -756 -1534 -786 1564 -841 1469 -810 1376 -779 1285 -747 1196 -714 1108 -680 1022 -646 938 -611 856 -575 776 -538 698 -500 623 -462 551 -423 481 -383 414 -342 350 -301 290 -259 232 -217 178 -174 128 -131 81 -88 39 -44 0 -0 -34 43 -64 86 -90 129 -111 170 -128 211 -140 250 -147 288 -151 324 -150 358 -145 389 -136 417 -124 443 -108 465 -90 483 -69 498 -47 508 -24 515 0 517 24 515 47 508 69 498 90 483 108 465 124 443 136 417 145 389 150 358 151 324 147 288 140 250 128 211 111 170 90 129 64 86 34 43 -0 -0 -39 -44 -81 -88 -128 -131 -178 -174 -232 -217 -290 -259 -350 -301 -414 -342 -481 -383 -551 -423 -623 -462 -698 -500 -776 -538 -856 -575 -938 -611 -1022 -646 -1108 -680 -1196 -714 -1285 -747 -1376 -779 -1469 -810 -1564 -841 1594 -897 1501 -866 1408 -834 1318 -801 1229 -768 1142 -734 1057 -699 973 -664 892 -627 813 -590 736 -552 662 -514 590 -474 521 -434 455 -394 392 -353 332 -311 275 -269 221 -226 171 -183 125 -140 82 -97 43 -54 9 -12 -22 31 -48 72 -70 113 -88 152 -102 191 -111 227 -116 262 -118 295 -115 325 -110 352 -100 376 -88 397 -74 415 -57 429 -39 439 -20 445 0 447 20 445 39 439 57 429 74 415 88 397 100 376 110 352 115 325 118 295 116 262 111 227 102 191 88 152 70 113 48 72 22 31 -9 -12 -43 -54 -82 -97 -125 -140 -171 -183 -221 -226 -275 -269 -332 -311 -392 -353 -455 -394 -521 -434 -590 -474 -662 -514 -736 -552 -813 -590 -892 -627 -973 -664 -1057 -699 -1142 -734 -1229 -768 -1318 -801 -1408 -834 -1501 -866 -1594 -897 1625 -955 1532 -923 1441 -891 1351 -858 1263 -824 1176 -790 1092 -755 1009 -719 929 -682 851 -645 775 -607 701 -568 630 -529 562 -489 496 -448 433 -407 373 -366 317 -324 264 -282 214 -239 167 -197 125 -154 86 -112 51 -70 20 -29 -7 12 -31 51 -50 90 -65 127 -76 162 -83 196 -87 227 -87 256 -84 283 -78 306 -69 326 -58 343 -45 356 -31 366 -16 371 0 373 16 371 31 366 45 356 58 343 69 326 78 306 84 283 87 256 87 227 83 196 76 162 65 127 50 90 31 51 7 12 -20 -29 -51 -70 -86 -112 -125 -154 -167 -197 -214 -239 -264 -282 -317 -324 -373 -366 -433 -407 -496 -448 -562 -489 -630 -529 -701 -568 -775 -607 -851 -645 -929 -682 -1009 -719 -1092 -755 -1176 -790 -1263 -824 -1351 -858 -1441 -891 -1532 -923 -1625 -955 1656 -1015 1564 -983 1474 -950 1384 -917 1297 -883 1211 -848 1128 -813 1046 -776 966 -740 888 -702 813 -664 740 -625 670 -586 602 -546 537 -506 474 -465 415 -424 359 -382 306 -340 256 -299 210 -257 167 -215 128 -174 92 -133 60 -92 32 -53 8 -14 -12 23 -29 59 -42 94 -51 126 -57 156 -60 184 -60 209 -57 232 -51 251 -44 267 -34 280 -24 289 -12 295 0 296 12 295 24 289 34 280 44 267 51 251 57 232 60 209 60 184 57 156 51 126 42 94 29 59 12 23 -8 -14 -32 -53 -60 -92 -92 -133 -128 -174 -167 -215 -210 -257 -256 -299 -306 -340 -359 -382 -415 -424 -474 -465 -537 -506 -602 -546 -670 -586 -740 -625 -813 -664 -888 -702 -966 -740 -1046 -776 -1128 -813 -1211 -848 -1297 -883 -1384 -917 -1474 -950 -1564 -983 -1656 -1015 1688 -1076 1597 -1044 1507 -1011 1418 -977 1332 -943 1247 -908 1163 -873 1082 -836 1003 -799 926 -762 852 -724 779 -685 709 -646 642 -606 577 -566 515 -526 456 -485 400 -444 347 -402 297 -361 251 -320 208 -279 168 -239 132 -198 100 -159 71 -120 46 -83 24 -47 6 -12 -9 21 -21 53 -29 82 -34 109 -36 133 -36 154 -34 173 -30 188 -24 200 -16 209 -8 214 0 216 8 214 16 209 24 200 30 188 34 173 36 154 36 133 34 109 29 82 21 53 9 21 -6 -12 -24 -47 -46 -83 -71 -120 -100 -159 -132 -198 -168 -239 -208 -279 -251 -320 -297 -361 -347 -402 -400 -444 -456 -485 -515 -526 -577 -566 -642 -606 -709 -646 -779 -685 -852 -724 -926 -762 -1003 -799 -1082 -836 -1163 -873 -1247 -908 -1332 -943 -1418 -977 -1507 -1011 -1597 -1044 -1688 -1076 1720 -1140 1629 -1107 1540 -1074 1452 -1040 1366 -1006 1282 -971 1199 -935 1119 -899 1040 -862 964 -824 890 -786 818 -748 749 -708 682 -669 617 -629 556 -589 497 -549 441 -508 388 -467 338 -427 292 -387 248 -346 208 -307 172 -267 138 -229 108 -191 82 -155 59 -120 39 -86 22 -54 9 -24 -1 4 -9 30 -14 53 -17 74 -17 91 -16 106 -13 118 -10 126 -5 131 0 133 5 131 10 126 13 118 16 106 17 91 17 74 14 53 9 30 1 4 -9 -24 -22 -54 -39 -86 -59 -120 -82 -155 -108 -191 -138 -229 -172 -267 -208 -307 -248 -346 -292 -387 -338 -427 -388 -467 -441 -508 -497 -549 -556 -589 -617 -629 -682 -669 -749 -708 -818 -748 -890 -786 -964 -824 -1040 -862 -1119 -899 -1199 -935 -1282 -971 -1366 -1006 -1452 -1040 -1540 -1074 -1629 -1107 -1720 -1140 1753 -1205 1662 -1172 1574 -1139 1487 -1105 1401 -1070 1317 -1035 1236 -999 1156 -963 1078 -926 1002 -889 928 -851 857 -812 788 -774 721 -734 657 -695 596 -655 537 -615 481 -575 428 -536 378 -496 332 -456 288 -417 247 -378 210 -340 176 -302 145 -266 117 -230 93 -196 71 -164 53 -133 38 -104 25 -77 15 -52 7 -29 2 -10 -1 7 -3 21 -4 33 -3 41 -2 45 0 47 2 45 3 41 4 33 3 21 1 7 -2 -10 -7 -29 -15 -52 -25 -77 -38 -104 -53 -133 -71 -164 -93 -196 -117 -230 -145 -266 -176 -302 -210 -340 -247 -378 -288 -417 -332 -456 -378 -496 -428 -536 -481 -575 -537 -615 -596 -655 -657 -695 -721 -734 -788 -774 -857 -812 -928 -851 -1002 -889 -1078 -926 -1156 -963 -1236 -999 -1317 -1035 -1401 -1070 -1487 -1105 -1574 -1139 -1662 -1172 -1753 -1205 1785 -1272 1695 -1239 1607 -1206 1521 -1171 1436 -1137 1353 -1102 1272 -1066 1192 -1030 1115 -993 1039 -956 966 -918 895 -880 827 -841 760 -802 696 -763 635 -724 577 -685 521 -646 468 -606 418 -567 371 -528 327 -490 285 -452 247 -415 212 -378 180 -343 151 -308 126 -275 103 -244 83 -214 65 -186 50 -160 38 -136 28 -115 20 -96 14 -79 9 -66 6 -55 3 -47 2 -43 0 -41 -2 -43 -3 -47 -6 -55 -9 -66 -14 -79 -20 -96 -28 -115 -38 -136 -50 -160 -65 -186 -83 -214 -103 -244 -126 -275 -151 -308 -180 -343 -212 -378 -247 -415 -285 -452 -327 -490 -371 -528 -418 -567 -468 -606 -521 -646 -577 -685 -635 -724 -696 -763 -760 -802 -827 -841 -895 -880 -966 -918 -1039 -956 -1115 -993 -1192 -1030 -1272 -1066 -1353 -1102 -1436 -1137 -1521 -1171 -1607 -1206 -1695 -1239 -1785 -1272 1818 -1341 1729 -1308 1641 -1274 1555 -1240 1471 -1205 1388 -1170 1308 -1134 1229 -1098 1152 -1062 1077 -1025 1004 -987 933 -949 865 -911 799 -873 735 -834 674 -796 616 -757 560 -718 507 -680 456 -641 409 -603 364 -566 323 -529 284 -492 248 -457 215 -422 185 -389 157 -357 133 -327 111 -298 92 -271 75 -246 60 -223 48 -202 37 -184 29 -168 21 -155 15 -145 9 -138 5 -133 0 -132 -5 -133 -9 -138 -15 -145 -21 -155 -29 -168 -37 -184 -48 -202 -60 -223 -75 -246 -92 -271 -111 -298 -133 -327 -157 -357 -185 -389 -215 -422 -248 -457 -284 -492 -323 -529 -364 -566 -409 -603 -456 -641 -507 -680 -560 -718 -616 -757 -674 -796 -735 -834 -799 -873 -865 -911 -933 -949 -1004 -987 -1077 -1025 -1152 -1062 -1229 -1098 -1308 -1134 -1388 -1170 -1471 -1205 -1555 -1240 -1641 -1274 -1729 -1308 -1818 -1341
4. Load "mesh.txt" above along with the LDC input YUV image from the camera into DCC tuning tool to generate a LDC preview and the DCC xml file for LDC.
Tuning tool can take care of the block size and H/W padding details (please follow the LDC plugin guide from the help menu).
LDC input image with fisheye distortion:
original image_1280x944_uyvy.yuv
LDC output preview from DCC tuning tool:
DCC xml file and its included LUT in H/W format exported by DCC tuning tool.
<?xml version="1.0" encoding="utf-8"?> <cfg_ldc_xml xmlns:xsi="http://www.w3.org/2001/xmlschema-instance" xmlns:xsd="http://www.w3.org/2001/xmlschema"> <!--this is a comment--> <dcc_name>cfg_ldc</dcc_name> <dcc_header> <camera_module_id> 42 </camera_module_id> <dcc_descriptor_id> 5 </dcc_descriptor_id> <algorithm_vendor_id> 1 </algorithm_vendor_id> <tunning_tool_version> 0 </tunning_tool_version> </dcc_header> <!--=======================================================================--> <typedef> <cfg_ldc_vars type="struct"> <ldc_en type="uint16"> </ldc_en> <ldc_ldmapen type="uint16"> </ldc_ldmapen> <ldc_datamode type="uint16"> </ldc_datamode> <ldc_opdatamode type="uint16"> </ldc_opdatamode> <ldc_ip_dfmt type="uint16"> </ldc_ip_dfmt> <ldc_pwarpen type="uint16"> </ldc_pwarpen> <ldc_yint_typ type="uint16"> </ldc_yint_typ> <ldc_regmode_en type="uint16"> </ldc_regmode_en> <ldc_meshtable_m type="uint16"> </ldc_meshtable_m> <ldc_mesh_frsz_w type="uint16"> </ldc_mesh_frsz_w> <ldc_mesh_frsz_h type="uint16"> </ldc_mesh_frsz_h> <ldc_compute_frsz_w type="uint16"> </ldc_compute_frsz_w> <ldc_compute_frsz_h type="uint16"> </ldc_compute_frsz_h> <ldc_initx type="uint16"> </ldc_initx> <ldc_inity type="uint16"> </ldc_inity> <ldc_input_frsz_w type="uint16"> </ldc_input_frsz_w> <ldc_input_frsz_h type="uint16"> </ldc_input_frsz_h> <ldc_obw type="uint16"> </ldc_obw> <ldc_obh type="uint16"> </ldc_obh> <ldc_pixpad type="uint16"> </ldc_pixpad> <ldc_a type="int16"> </ldc_a> <ldc_b type="int16"> </ldc_b> <ldc_c type="int16"> </ldc_c> <ldc_d type="int16"> </ldc_d> <ldc_e type="int16"> </ldc_e> <ldc_f type="int16"> </ldc_f> <ldc_g type="int16"> </ldc_g> <ldc_h type="int16"> </ldc_h> <ldc_sf_width type="uint16[3]"> </ldc_sf_width> <ldc_sf_height type="uint16[3]"> </ldc_sf_height> <ldc_sf_en type="uint16[3][3]"> </ldc_sf_en> <ldc_sf_obw type="uint16[3][3]"> </ldc_sf_obw> <ldc_sf_obh type="uint16[3][3]"> </ldc_sf_obh> <ldc_sf_pad type="uint16[3][3]"> </ldc_sf_pad> <ldc_ylut_en type="uint16"> </ldc_ylut_en> <ldc_yin_bitdpth type="uint16"> </ldc_yin_bitdpth> <ldc_yout_bitdpth type="uint16"> </ldc_yout_bitdpth> <ldc_clut_en type="uint16"> </ldc_clut_en> <ldc_cin_bitdpth type="uint16"> </ldc_cin_bitdpth> <ldc_cout_bitdpth type="uint16"> </ldc_cout_bitdpth> <ldc_y_lut type="uint16[513]"> </ldc_y_lut> <ldc_c_lut type="uint16[513]"> </ldc_c_lut> <mesh_table_pitch_in_bytes type="uint32"> </mesh_table_pitch_in_bytes> <mesh_table_size type="uint32"> </mesh_table_size> <mesh_lut type="uint16*"> </mesh_lut> </cfg_ldc_vars> </typedef> <!--=======================================================================--> <use_case val="65535"> <n-space> <region0 class="0"> <exposure val="1" min="0" max="2000000"> </exposure> <gain val="0" min="0" max="100000"> </gain> </region0> </n-space> <parameter_package> <ldc_dcc type="cfg_ldc_vars"> { 1 // LDC_CTRL LDC_EN(0) LDC Enable, 0: Disable, 1: Enable 1 // LDC_CTRL LDMAPEN(1) LD Mapping enable, 0: disable, 1: enable 0 // LDC_CTRL DATAMODE(4:3) Input data mode, 0: YUV422, 1: Y only, 2: YUV420, 3: YUV420 UV 0 // LDC_CTRL OP_DATAMODE Output data mode, 0: keep UYVY; 1: convert to 420 0 // LDC_CTRL IP_DFMT(6:5) Input pixel format, 0: 8b, 1: 12b packed, 2: 12b unpacked 1 // LDC_CTRL PWARPEN(7) 0: Disable perspective warp. 1: Enable perspective warp 1 // LDC_CFG YINT_TYP(6) Interpolation type for Y data. 0: Bicubic, 1: Bilinear 0 // LDC_CFG REGMODE_EN Region mode, 0: disable, 1: enable 4 // LDC_MESHTABLE_CFG M(2:0) Mesh table subsampling factor (0-7) 1280 // LDC_MESH_FRSZ W(13:0) Mesh frame width (0-8192) 944 // LDC_MESH_FRSZ H(29:16) Mesh frame height (0-8192) 1280 // LDC_COMPUTE_FRSZ W(13:0) Compute width (0-8192) 944 // LDC_COMPUTE_FRSZ H(29:16) Compute height (0-8192) 0 // LDC_INITXY INITX(13:0) Output starting horizontal coordinate (0-8192) 0 // LDC_INITXY INITY(29:16) Output starting vertical coordinate (0-8192) 1280 // LDC_INPUT_FRSZ W(29:16) Input frame width 944 // LDC_INPUT_FRSZ H(13:0) Input frame height 80 // LDC_BLOCK_SIZE OBW(7:0) Output block width (0-255) 48 // LDC_BLOCK_SIZE OBH(15:8) Output block height (0-255) 1 // LDC_BLOCK_SIZE PIXPAD(19:16) Pixel pad (0-15) 4096 // LDC_AB A(15:0) Affine Transform warp, A S16Q12 0 // LDC_AB B(31:16) Affine Transform warp, B S16Q12 0 // LDC_CD C(15:0) Affine Transform warp, C S16Q3 0 // LDC_CD D(31:16) Affine Transform warp, D S16Q12 4096 // LDC_EF E(15:0) Affine Transform warp, E S16Q12 0 // LDC_EF F(31:16) Affine Transform warp, F S16Q3 0 // LDC_GH G(15:0) Affine Transform warp, G S16Q23 0 // LDC_GH H(31:16) Affine Transform warp, H S16Q23 {0, 0, 0} //ldc_sf_width [3] {0, 0, 0} //ldc_sf_height[3] {{0, 0, 0}, {0, 0, 0}, {0, 0, 0}} //ldc_sf_en [3][3] {{0, 0, 0}, {0, 0, 0}, {0, 0, 0}} //ldc_sf_obw[3][3] {{0, 0, 0}, {0, 0, 0}, {0, 0, 0}} //ldc_sf_obh[3][3] {{0, 0, 0}, {0, 0, 0}, {0, 0, 0}} //ldc_sf_pad[3][3] 0 // LDC_DUALOUT_CFG YLUT_EN Luma LUT enable (0-1) 8 // LDC_DUALOUT_CFG YIN_BITDPTH Luma input bit depth (8-12) 8 // LDC_DUALOUT_CFG YOUT_BITDPTH Luma output bit depth (8-12) 0 // LDC_DUALOUT_CFG CLUT_EN Chroma LUT enable (0-1) 8 // LDC_DUALOUT_CFG CIN_BITDPTH Chroma input bit depth (8-12) 8 // LDC_DUALOUT_CFG COUT_BITDPTH Chroma output bit depth (8-12) { //y_lut 0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0 } { //c_lut 0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0 } 336, //mesh_table_pitch_in_bytes 10080, //mesh_table_size { //mesh_lut #include "asamplesensor_mesh_lut.txt" } } </ldc_dcc> </parameter_package> </use_case> <!--=====================================================================--> </cfg_ldc_xml>
This H/W version of the mesh table "test_mesht_lut.txt" is in 32-bit words with little endian encoding and each row of the mesh table must be 16-byte aligned.
For example, the first row in "mesh.txt" above is "1818 (0x71a), 1341 (0x53d)", and the corresponding 32-bit binary word is "0x53d, 0x71a" in "test_mesh_lut.txt".
At the end of each row in "test_mesh_lut.txt", you can find the padding of six "0x0000" so that each row is 336 bytes (336=16x21).
5. Copy the above xml file and its included LUT text file to the "imaging/sensor_drv/src/sensor_name/dcc_xmls/" folder in PSDK for your sensor.
Then, you may need to run the "generate_dcc.sh" under the folder and recompile PSDK.
PSDK sample apps such as "vx_app_single_cam" will pick up the new DCC settings for LDC.