Hi there, a customer is looking for recommendations on replacements for the following devices since they are Obsolete:
TMS320C6747BZKBA3 |
TMS320C6747BZKBT3 |
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there, a customer is looking for recommendations on replacements for the following devices since they are Obsolete:
TMS320C6747BZKBA3 |
TMS320C6747BZKBT3 |
The replacement part would be TMS320C6747DZKBA3.
This is the current version of the part that your customer is looking for.
This part can be purchased directly from the TI store here: https://www.ti.com/store/ti/en/p/product/?p=TMS320C6747DZKBA3
Regards,
Kyle
Thanks Kyle. Two follow-ups:
1. Is that the replacement for BOTH orderables I had?
2. What changed between the old and the replacement?
Thanks,
Kannan
Kannan,
The replacement parts are aligned as follows:
Original Part New Part
1. TMS320C6747BZKBA3 ===> TMS320C6747DZKBA3
2. TMS320C6747BZKBT3 ===> TMS320C6747DZKBT3
You will notice that the "B" letter that immediately follows the C6747 part of the orderable has been changed from "B" to "D". From the datasheet, this change indicates an update to the silicon version that is used. This is fairly common practice across all TI device to have revisions to silicon through the life of the device. Unless otherwise noted in the errata or datasheet, there should be no functional differences in these new part numbers.
Regards,
Kyle