-
Hi
We have CCS 10 project with bios base on TMS320C6745.
Without using the edma3 the project pass building.
We add edma3 to the project and update main.c with:
#include "C:\ti\edma3_lld_02_12_00_20\packages\ti\sdo\edma3\drv\edma3_drv.h"The project build pass.The problem:When we add any function of edma3 like:EDMA3_DRV_delete (0,NULL);The project fail to build with message:undefined first referencedsymbol in file--------- ----------------EDMA3_DRV_delete ./main.objerror #10234-D: unresolved symbols remainerror #10010: errors encountered during linkinglooks like there is problem with lib....
Please advice what need to do for integrating EDMA3 and pass the build?
Shaul