Other Parts Discussed in Thread: TMDXIDK5718, TLK105L, DP83848C
Hi,
I'm using SDK-LINUX-AM57X 06_03_00_106 on our custom board.
Our board has 3 ethernet ports .
It is similer to TMDXIDK5718. But it doesn't have 2 Gigabit (1000Mb) Ethernet Ports.
All 3 ports are 100Mb Ethernet Ports on PRU-ICSS.
The PHY deviceis DP83848MSQ/NOPB instead of TLK105L.
Mdio found PHY devices.
davinci_mdio 4b232400.mdio: phy[1]: device 4b232400.mdio:01, driver NS DP83848C 10/100 Mbps PHY <- pruss1_emac1
davinci_mdio 4b2b2400.mdio: phy[1]: device 4b2b2400.mdio:01, driver NS DP83848C 10/100 Mbps PHY <- pruss2_emac0
davinci_mdio 4b2b2400.mdio: phy[3]: device 4b2b2400.mdio:03, driver NS DP83848C 10/100 Mbps PHY <- pruss2_emac1
pruss1_eth driver is initialized.I set IPv4 address to pruss1_eth1.ARP packets are sent.
On "ping" command, packets are sent,but recived packets are not recognised.
RXD0, 1, 2, 3 signals are shown in PHY→MAC.
But system did not recognized any packets.
Tx works, but Rx does not.
Can you think of any reasons ?
Regards,
Toshio Masuchi