This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How to connect each of the unused warm reset inputs (MCU_RESETz and RESET_REQz)?
The schematic review checklist (SPRACU5B) describes that they must be held low during power sequencing.
Should the unused warm reset inputs (MCU_RESETz and RESET_REQz) be tied to the reset output along with the cold reset input (MCU_PORz)?
Best regards,
Daisuke
Hi,
Can each of the unused warm reset inputs (MCU_RESETz and RESET_REQz) only be pulled up to their supply voltage and not connected anywhere else?
Please give me an answer as soon as possible. Your prompt reply would be appreciated.
Best regards,
Daisuke
Each of these balls must be connected to the corresponding power supply through separate external pull resistors to ensure these balls are held to a valid logic high level if a PCB signal trace is connected and not actively driven by an attached device. The internal pull-up may be used to hold a valid logic high level if no PCB signal trace is connected to the ball
Regards,
James
Hi James-san,
Thank you for your reply.
The schematic review checklist (SPRACU5B) describes that the reset signals into MCU_PORz, MCU_RESETz and RESET_REQz must be held low during power sequencing.
Do not the unused warm reset inputs (MCU_RESETz and RESET_REQz) need to be held low during power sequencing?
Best regards,
Daisuke