Part Number: SK-TDA4VM
Hi ,
One SK-TDA4VM has ethernet issue as below shown. Is there any test tool for it to check if PHY or else HW is OK? Thanks.
root@j7-evm:/opt/edge_ai_apps# ifconfig
eth0: flags=4099<UP,BROADCAST,MULTICAST> mtu 1500 metric 1
ether 24:76:25:96:22:1b txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
lo: flags=73<UP,LOOPBACK,RUNNING> mtu 65536 metric 1
inet 127.0.0.1 netmask 255.0.0.0
inet6 ::1 prefixlen 128 scopeid 0x10<host>
loop txqueuelen 1000 (Local Loopback)
RX packets 82 bytes 6220 (6.0 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 82 bytes 6220 (6.0 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
root@j7-evm:/opt/edge_ai_apps# dhcp
-sh: dhcp: command not found
root@j7-evm:/opt/edge_ai_apps# ifconfig eth0 up
root@j7-evm:/opt/edge_ai_apps# ifconfig eth0 down
root@j7-evm:/opt/edge_ai_apps# ifconfig eth0 up
[ 67.355954] TI DP83867 46000f00.mdio:00: attached PHY driver [TI DP83867] (mi i_bus:phy_addr=46000f00.mdio:00, irq=POLL)
root@j7-evm:/opt/edge_ai_apps# [ 67.370567] am65-cpsw-nuss 46000000.ethernet e th0: Link is Down