Other Parts Discussed in Thread: LMK03318
Hello,
I originally posted this question on the Clock & Timing forum and was asked by Hao to re-post the question on this forum.
I am using the LMK03318 in Hardmode with ROM Option 45 to provide 3 LVPECL clocks to the TMS320C6678 (LJCB/CML inputs). My question is regarding the best input voltage level for the TMS320C6678. Currently the only circuitry between these two ICs is a 0.1uF capacitor. Please see the attached Word document for a discussion. Also please see the attached spreadsheet, which has 3 tabs showing the voltages from the Hyperlynx simulation of my present design.
As described on pages 4 and 5 of SCAA059C, should I add Ra series resistors?
What resistor value for Ra should I use?
Regards,
Larry
LVPECL to LJCB voltage adjustment.docxDAR6 Hyperlynx Simulations 4-20-2022.xlsx