This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In our application, we will have eMMC in MMC2 and NOR flash in QSPI. The boot can be either from eMMC or NOR flash. We need to interface FPGA to GPMC and it is seen that sysboot is multiplexed with the GPMC AD[0:15] pins. Is there any problem with such a design so that after booting GPMC interface is free to use for FPGA communication.
We also require DSP core in our application whereas the DSP clock3 again has a dependency on sysboot pin. In conjunction with the above requirements, how can we configure the sysboot pins?
Thank you
Hello. This is a long pending thread (sorry for the inconvenience). Please confirm whether this thread is still relevant.