Part Number: AM5718
Hi,
We are in the design stage of an ARM+DSP based Processor module. We have chosen the SItara Processor AM5718 for our application. It is planned to use parallel NOR as boot flash in non-multiplexed mode configuration. So CS0 of Processor will be used by NOR Flash. In addition to NOR Flash interface to GPMC, we are planning to use a NAND Flash & FPGA using CS1 & CS2 respectively. Using eMMC NAND is restricting to use multiplexed mode NOR boot Flash configuration (as per TRM, if correctly understood). So in multiplexed mode configuration an extra address / data latch IC is required, but we are having module size constraints. So it is planned to interface NAND Flash to GPMC.
GPMC Interface:
CS0 --> Parallel NOR Flash (Boot)
CS1 --> NAND Flash (Storage)
CS2 --> FPGA
Please confirm whether GPMC interface can be used in the above configuration.
Regards
Hafiz