The Linux based SRV application on TDA4VM takes 20-25 Seconds to launch based on the boot media and the media hosting the rootfs.
How to optimize this to 2-3 seconds?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The Linux based SRV application on TDA4VM takes 20-25 Seconds to launch based on the boot media and the media hosting the rootfs.
How to optimize this to 2-3 seconds?
Hi,
The exercise is done on top of 8.2 SDK for TDA4VM.
A detailed procedure on optimizing the SRV use case to 2.2 Seconds to first frame to display is here:
SRV Optimizations SDK 8.2-v20-20220620_061317.pdf
The corresponding patches zip folder for each step in the above pdf is attached here:
SRV-8.2-Attachments.zip
Best Regards,
Keerthy