This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
My customer is looking to have more than three (edit: XGA) overlays. I see that the DSS provides two overlays.
Best regards,
Mari
Hi Bin,
Thanks for your reply. Looking forward to responses from the graphics experts.
-Mari
Hi Bin,
Do you have any updates from the graphics expert?
Sorry for the urgency, but being able to overlay at least three layers is key for this customer. If we can answer these questions for them, it would be very helpful for device selection.
Best regards,
Mari
Hi Mari,
Sorry for the delay, our graphics expert will be back to office next week. Please allow him a few days to catch up the work since he has been out for a few weeks.
Hi Mari,
In general, there isn't any limit on how many input images the GPU can read. However, your performance will vary based on the number of images read and their resolution/format. For example, reading a single 1080p image will be faster than multiple 1080p images. In your case, the GPU should be able to read 3 images and composite them into one output image. The GPU on AM625 is OpenGLES3.1 compliant and the customer can use standard Khronos API for composition.
Regards,
Krunal
Hi Krunal,
Thanks for your response.
Best,
Mari
Hi Mari,
1. Yes and just to clarify, it's OpenGL ES 3.1.
2. The DSS IP supports alpha blending and composition. Please refer to the TRM for all the available feature set.
3. Based on my discussion with developer, we don't have any DSS examples yet and I will file for an internal ticket. With regards to the GPU, the customer could just refer to online examples on Khronos website.
Regards,
Krunal
Hi Krunal,
Thanks for your response. Would you be able to provide more documentation on the libdrm module with regards to AM625x?
Best,
Mari
Hi Mari,
The libdrm module comes from the community and if you are interested in examples, please refer to the following:
1. https://github.com/tomba/kmsxx
2. https://github.com/freedesktop/mesa-kmscube
Regards,
Krunal