This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello there , hello Misael Lopez,
Would please confirm TDA4VM SDK Ver8.4 supported
1) gPTP on CPSW9G : ready and tested with TDA4VM-EVM board ? if yes, what's the gPTP version
2) linuxptp4l on Linux A72 : ready and tested with TDA4VM-EVM board ?
Hi,
linuxptp4l on Linux A72 : ready and tested with TDA4VM-EVM board ?
This is present from SDK 8.4 onwards on native ethernet driver on Linux. Note that linuxptp is not used with ethfw or enet applications.
gPTP on CPSW9G : ready and tested with TDA4VM-EVM board ? if yes, what's the gPTP version
On Ethfw and Enet applications, we have ptp API using which we can configure a ptp slave only. This is also verified on EVM.
Regards,
Tanmay