This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
I'm using AM2634 CAN but some issues may need your help:
1. CAN bus has some error frame appear randomly.
I want to know how to use the parameter like recErrCnt,canErrLogCnt in MCAN_ErrCntStatus
How these counters work? Which conditions will the counter reset?
2. I need to change sample point from 70% to 80%
I have modify the parameters to meet the requirement.
But I found there's more error frame occur after modification.
bitTimes->nomRatePrescalar = 0xFU;
bitTimes->nomTimeSeg1 = 0x5U;
bitTimes->nomTimeSeg2 = 0x2U;
bitTimes->nomSynchJumpWidth = 0x0U;
bitTimes->dataRatePrescalar = 0x3U;
bitTimes->dataTimeSeg1 = 0x5U;
bitTimes->dataTimeSeg2 = 0x2U;
bitTimes->dataSynchJumpWidth = 0x0U;
bitTimes->nomRatePrescalar = 0xFU;
bitTimes->nomTimeSeg1 = 0x6U;
bitTimes->nomTimeSeg2 = 0x1U;
bitTimes->nomSynchJumpWidth = 0x0U;
bitTimes->dataRatePrescalar = 0x3U;
bitTimes->dataTimeSeg1 = 0x6U;
bitTimes->dataTimeSeg2 = 0x1U;
bitTimes->dataSynchJumpWidth = 0x0U;
Is there more parameters I need to modify or something else to do?
Thanks for your help.
Best Regards
Hi Jay,
I'll take a look at get back with you soon.
Thanks,
Frank
Frank,
Customer report issue that canErrLogCnt always reports "zero" when recErrCnt is increasing.
typedef struct
{
uint32_t transErrLogCnt;
/**< Transmit Error Counter */
uint32_t recErrCnt;
/**< Receive Error Counter */
uint32_t rpStatus;
/**< Receive Error Passive
* 0 = The Receive Error Counter is below the error passive level(128)
* 1 = The Receive Error Counter has reached the error passive level(128)
*/
uint32_t canErrLogCnt;
/**< CAN Error Logging */
}MCAN_ErrCntStatus;
The API MCAN_getErrCounters() use to access ECR register to get error count:
/* Checking for Rx Errors */
MCAN_getErrCounters(gMcanBaseAddr, &errCounter);
According to MCAN manual which can be downloaded from here : https://www.bosch-semiconductors.com/ip-modules/can-ip-modules/m-can/
Byte access: Reading byte 2 will reset CEL to zero, reading bytes 3/1/0 has no impact.
However in SDK8.03 driver source code:
void MCAN_getErrCounters(uint32_t baseAddr,
MCAN_ErrCntStatus *errCounter)
{
errCounter->transErrLogCnt = HW_RD_FIELD32(MCAN_CfgAddr(baseAddr) + MCAN_ECR,
MCAN_ECR_TEC);
errCounter->recErrCnt = HW_RD_FIELD32(MCAN_CfgAddr(baseAddr) + MCAN_ECR,
MCAN_ECR_REC);
errCounter->rpStatus = HW_RD_FIELD32(MCAN_CfgAddr(baseAddr) + MCAN_ECR,
MCAN_ECR_RP);
errCounter->canErrLogCnt = HW_RD_FIELD32(MCAN_CfgAddr(baseAddr) + MCAN_ECR,
MCAN_ECR_CEL);
}
The first 3x 32bits access will reset CEL field so the last call will always read "zero" into canErrLogCnt.
SDK driverlib needs to be modified and change counter read order to get correct result.
void MCAN_getErrCounters(uint32_t baseAddr,
MCAN_ErrCntStatus *errCounter)
{
errCounter->canErrLogCnt = HW_RD_FIELD32(MCAN_CfgAddr(baseAddr) + MCAN_ECR,
MCAN_ECR_CEL);
errCounter->transErrLogCnt = HW_RD_FIELD32(MCAN_CfgAddr(baseAddr) + MCAN_ECR,
MCAN_ECR_TEC);
errCounter->recErrCnt = HW_RD_FIELD32(MCAN_CfgAddr(baseAddr) + MCAN_ECR,
MCAN_ECR_REC);
errCounter->rpStatus = HW_RD_FIELD32(MCAN_CfgAddr(baseAddr) + MCAN_ECR,
MCAN_ECR_RP);
// Issue: 2022/10. 17
// CEL always read as "zero" when access struct MCAN_ErrCntStatus;
// Change the access the order to ECR register since CEL will be reset after it is read
// errCounter->canErrLogCnt = HW_RD_FIELD32(MCAN_CfgAddr(baseAddr) + MCAN_ECR,
// MCAN_ECR_CEL);
// TEC, REC, and RP will not be impact by read access to ECR register
}
Please double confirm and fix this issue in next version of SDK.
Regards
Andre
Hi,
Thanks for your help about Q1. The canErrLogCnt data can be changed after modify.
And is there any suggesting about Q2? I have a customer request about CAN sample point from 70% to 80%.
http://www.bittiming.can-wiki.info/
Now after I set up parameter like below and connect with Vector OE,there's error frame occur and than bus off.
bitTimes->nomRatePrescalar = 0xFU;
bitTimes->nomTimeSeg1 = 0x6U;
bitTimes->nomTimeSeg2 = 0x1U;
bitTimes->nomSynchJumpWidth = 0x0U;
bitTimes->dataRatePrescalar = 0x3U;
bitTimes->dataTimeSeg1 = 0x6U;
bitTimes->dataTimeSeg2 = 0x1U;
bitTimes->dataSynchJumpWidth = 0x0U;
How to solve this problem?
Thanks for your help.
Best Regards
Jay,
May you try to increase bitTimes->nomSynchJumpWidth = bitTimes->dataSynchJumpWidth = 0x01U?
Increasing SJW to improve tolerance. As long as SJW <= min(TSeg1, TSeg2) the setting should be OK.
Regards
Andre
I have try change the parameter(dataSynchJumpWidth )to 0x01U but useless.
Now I already modify a set of parameters without error frame.
I will open new question if there's any response from my customer testing.
Thanks for your help.
Best Regards
Hi Andre,
Please double confirm and fix this issue in next version of SDK.
Will you file an SDK bug for this?
Regards,
Frank
Frank,
I don’t know if FAE has access right to file SDK bug. I don’t have Jira access neither. So can you please help to file SDK bug?
Thanks for your help.
Regards
Andre
Hi Andre,
No problem, I'll file a bug. Thanks for your help on this issue!
Regards,
Frank