Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA750: The Samsung HS200 eMMC doesn't work well

Part Number: DRA750

Hi, Expert

SoC: DRA750

SDK VERSION: 3.2

Kernel version: Linux-4.4.84

Our customer encountered eMMC issue on their system based on DRA750. When they used Micron eMMC NAND Flash, it worked well. But when they replaced the Micron eMMC NAND flash by Samsung eMMC NAND flash(KLM8G1GEUF-B04P-EMMC-8GB-Ver5.1-3.3V-8). After  running a period of time, a little of them can't start up successfully, the system halt in loading application because some lib can't be loaded successfully.

Can you help to review the eMMC schematic diagram?

DRA750 eMMC schematic.pdf

Best Regards

Tony