This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
To do this, run python uart_uniflash.py -p COM10 --cfg=sbl_prebuilt/am62x-sk/default_sbl_null.cfg
The following error occurs when the command is executed. The sdk used for viewing the figure is am62 /mcu_plus_sdk_am62x_08_04_00_16,How to solve it?
Hi,
Line 20 is a command to flash stage 2 bootloader. For that, you need to build the Stage 2 bootloader appimage. You can run the following command from the root directory of mcu_plus_sdk_am62x_08_04_00_16 to build the required appimage.
$(MAKE) -s -C examples\drivers\boot\sbl_uart_uniflash_multistage\sbl_uart_uniflash_stage2\am62x-sk\r5fss0-0_nortos\ti-arm-clang all
where $(MAKE)
is the command to executable make build system.
Regards,
Prashant
Following your advice, I closed the transfer of this file, but the next file that followed could not be transferred either. I tried to restart the development board and found that the corresponding directory did contain this tiimage, but the transfer failed
Hi,
Could you please try flashing to eMMC instead of OSPI to narrow down the issue. Change the operation type to flash-emmc as shown:
Do power cycle the board before flashing. Please follow the steps to power cycle at below link and confirm the C characters getting printed before flashing.
Regards,
Prashant
I now all the operations are based on software-dl.ti.com/.../EVM_SETUP_PAGE.html M_SOC_INIT this step comes from (which is the user guide you provided) every time you execute python uart_uniflash.py -p COM10 --cfg=sbl_prebuilt/am62x-sk/default_sbl_null.cfg
I always make sure to close the serial port after printing c on the serial port. I can confirm that this step is OK. The development board I am using now has been used by other colleagues before, which is normal, but his startup mode is sd card. I changed the corresponding position in default_sbl_null.cfg to emmc, but it still doesn't work, and the transmission still cannot be done. I don't know if you mean to change the mode to emmc
Hi,
It seems you have solved this problem. Can you please tell us how did you solve the problem which will benefit others also.
Regards,
Prashant
I did not solve this problem. I just changed the way to initialize the flash memory and did not start it in this way. In addition, I would like to know the reason why xds110 could not be connected when I tried to debug m4 kernel
I just changed the way to initialize the flash memory and did not start it in this way.
Can you please elaborate more on this.
About the other issue, we can take it on that other thread.
Regards,
Prashant
The purpose of sending these files is to normally start the whole chip and debug it. I replaced it with an sd card to initialize the chip as normal. The m4 kernel can be started normally through the sd card and can be seen in the command line
Hi,
My understanding says that you are following https://software-dl.ti.com/mcu-plus-sdk/esd/AM62X/latest/exports/docs/api_guide_am62x/EVM_SETUP_PAGE.html#EVM_SOC_INIT
You have a SD card flashed with default linux image. You then set bootmode pins to boot mode from SD card. Then, when the board is powered up, ROM boots from SD card and binaries on SD card sets up the board.
Is that correct?
Regards,
Prashant