This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Can't use CSITX TX1

Genius 13655 points

Part Number: TDA4VM
Other Parts Discussed in Thread: TDA4VH

Hello Champs,

HW: customer own board

SW: Rtos 08_05_00_11 SDK

There are two CSITX: TX0 and TX1. Customer met errors when using TX1. TX0 can work successfully.

He configured it as below

printf("csitx instId %d\n",csitxObj->inst_id);
if(VX_SUCCESS == status)
{
memset(&csitxObj->csitx_params, 0, sizeof(tivx_csitx_params_t));

tivx_csitx_params_init(&csitxObj->csitx_params);
csitxObj->csitx_params.numInst = 1U;
csitxObj->csitx_params.numCh = 1;
csitxObj->csitx_params.instId[0U] = csitxObj->inst_id;
csitxObj->csitx_params.instCfg[0U].rxCompEnable = (uint32_t)vx_true_e;
csitxObj->csitx_params.instCfg[0U].rxv1p3MapEnable = (uint32_t)vx_true_e;
csitxObj->csitx_params.instCfg[0U].laneBandSpeed = TIVX_CSITX_LANE_BAND_SPEED_450_TO_510_MBPS;
csitxObj->csitx_params.instCfg[0U].laneSpeedMbps = 400;
csitxObj->csitx_params.instCfg[0U].numDataLanes = 4U;
csitxObj->csitx_params.instCfg[0U].vBlank = 22U;
csitxObj->csitx_params.instCfg[0U].hBlank = 40U;
csitxObj->csitx_params.instCfg[0U].startDelayPeriod = 40U;

for (loopCnt = 0U ;
loopCnt < csitxObj->csitx_params.instCfg[0U].numDataLanes ;
loopCnt++)
{
csitxObj->csitx_params.instCfg[0U].lanePolarityCtrl[loopCnt] = 0u;
}
for (loopCnt = 0U; loopCnt < csitxObj->csitx_params.numCh; loopCnt++)
{
csitxObj->csitx_params.chVcNum[loopCnt] = loopCnt;
csitxObj->csitx_params.chInstMap[loopCnt] = csitxObj->csitx_params.instId[0U];
}


csitxObj->csitx_params_obj = vxCreateUserDataObject(context, "tivx_csitx_params_t", sizeof(tivx_csitx_params_t), &csitxObj->csitx_params);
status = vxGetStatus((vx_reference)csitxObj->csitx_params_obj);

if(VX_SUCCESS == status)
{
vxSetReferenceName((vx_reference)csitxObj->csitx_params_obj, "csitx_node_csitx_params_obj");
}
}

It prompted below error

In the function CsitxDrv_dphytxLaneReady, when setting wait register to 1, it times out.


Thanks
Regards,
Shine