hello , am working on custom am3358 board.
and its similar to beagle bone black
we are using ti-rtos.
and using all peripherals like uart,i2c,spi . but when i enable all peripherals processor hang
and when i disable any two peripherals like either two uart or one i2c and one spi, or like any two combinations , it works fine.
here we are using all 6 uarts , 2 spi and 3 i2c given by am3358 in this by default UART-0 is for debug and rest all are assigned to different peripherals.
so total of 11 we have with 6-uart, 2-spi and 3-i2c ,if we enable 9 means its working fine and if we enable all 11 means processor halts.
can anyone tell what could be the issue here.