Hi, helping a customer out on this.
1. Please see image below for compile errors in the standard build. This is urgent.
2. Can you put freertos on C6678?
3. Can you port lightweight protocol stack on the C6678?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, helping a customer out on this.
1. Please see image below for compile errors in the standard build. This is urgent.
2. Can you put freertos on C6678?
3. Can you port lightweight protocol stack on the C6678?
Kannan,
Please see image below for compile errors in the standard build. This is urgent.
Have they tried the SDK ( Software development kit - Processor SDK 6.3 ) of C6678? Tried building the examples and RTOS without any errors?
If no, please ask them to try, at a first hand. Follow this FAQ: [FAQ] TMS320C6678: Quick set up Guide C6678 and C6678-EVM - Processors forum - Processors - TI E2E support forums
Can you put freertos on C6678?
C6678 already has RTOS. The processor SDK 6.3 has RTOS in it. Download link for PROCESSOR-SDK-RTOS-C667x 06_03_00_106 : https://software-dl.ti.com/processor-sdk-rtos/esd/C667x/latest/index_FDS.html
C6678 was already successfully running the RTOS.
All the examples given in the below link runs on top of the RTOS.
3. Can you port lightweight protocol stack on the C6678?
Yes. Possible. It already runs NIMU emac client successfully.
Regards
Shankari G