This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Where we can get more sample about VISONAPP except for C7x Kernel Application SAMPLE?
Hi :We want the C7 DSP to be used for general purpose computing samples, not based on TIDL(deep learning)
Hi Jiawei,
Thanks for reaching out.
There are some C7X DSP demos in 06.01.01.12 (19 Dec 2019) TDA4VM SDK version.
https://www.ti.com/tool/download/PROCESSOR-SDK-RTOS-J721E/06.01.01.12
You can find them from the following zip files
Kind Regards,
Weilun
Customer is using RTOS SDK8.02, which released with C7x CGT V2.1.1 LTS, the 06.01.01.12 released with C7x CGT 1.2.0.STS, can the 7X DSP demos in 06.01.01.12 build with C7x CGT 2.x?
Tony,
You might see some incompatibilities in the APIs between the two versions of compiler (You can refer to the compiler release notes between the two versions to identify them)
Regards,
Varun