Hi Ti,
On AM6548, we tried to read/write ASIX AX58100 by SPI.
From the waveform capture as attached, I can see some data output from AX58100.
In below pic, C2 is MOSI, and C4 is MISO.
And the "RED" square is the data from AX58100.
However, from my Linux test program, I cannot read any data from output.
root@AX-564EB0MB1T:/home# ./spiTest
spi mode: 0x3
bits per word: 8
max speed: 400000 Hz (400 KHz)
TX | 00 06 08 FF FF __ __ __ |.....|
RX | 00 00 00 00 00 00 00 00 |........|
I'm trying to find some registers in AM65 spec, and I doubt if this is cause.
If it is, how can I set it from Linux?
Could you help to check the program as attached and see if any config lost?
// SPDX-License-Identifier: GPL-2.0-only /* * SPI testing utility (using spidev driver) * * Copyright (c) 2007 MontaVista Software, Inc. * Copyright (c) 2007 Anton Vorontsov <avorontsov@ru.mvista.com> * * Cross-compile with cross-gcc -I/path/to/cross-kernel/include */ #include <stdint.h> #include <unistd.h> #include <stdio.h> #include <stdlib.h> #include <string.h> #include <getopt.h> #include <fcntl.h> #include <time.h> #include <sys/ioctl.h> #include <linux/ioctl.h> #include <sys/stat.h> #include <linux/types.h> #include <linux/spi/spidev.h> #include <stdbool.h> #include <errno.h> #define ARRAY_SIZE(a) (sizeof(a) / sizeof((a)[0])) static void pabort(const char *s) { perror(s); abort(); } static const char *device = "/dev/spidev9.0"; static uint32_t mode; static uint8_t bits = 8; static char *input_file; static char *output_file; static uint32_t speed = 400000; static uint16_t delay; static int verbose; static int transfer_size; static int iterations; static int interval = 5; /* interval in seconds for showing transfer rate */ uint8_t default_tx[10] = {0}; uint8_t default_rx[ARRAY_SIZE(default_tx)] = {0, }; char *input_tx; static void hex_dump(const void *src, size_t length, size_t line_size, char *prefix) { int i = 0; const unsigned char *address = src; const unsigned char *line = address; unsigned char c; printf("%s | ", prefix); while (length-- > 0) { printf("%02X ", *address++); if (!(++i % line_size) || (length == 0 && i % line_size)) { if (length == 0) { while (i++ % line_size) printf("__ "); } printf(" |"); while (line < address) { c = *line++; printf("%c", (c < 32 || c > 126) ? '.' : c); } printf("|\n"); if (length > 0) printf("%s | ", prefix); } } } static void transfer(int fd, uint8_t const *tx, uint8_t const *rx, size_t len) { int ret; int out_fd; struct spi_ioc_transfer tr = { .tx_buf = (unsigned long)tx, .rx_buf = (unsigned long)rx, .len = len, .delay_usecs = delay, .speed_hz = speed, .bits_per_word = bits, }; if (mode & SPI_TX_QUAD) tr.tx_nbits = 4; else if (mode & SPI_TX_DUAL) tr.tx_nbits = 2; if (mode & SPI_RX_QUAD) tr.rx_nbits = 4; else if (mode & SPI_RX_DUAL) tr.rx_nbits = 2; if (!(mode & SPI_LOOP)) { if (mode & (SPI_TX_QUAD | SPI_TX_DUAL)) tr.rx_buf = 0; else if (mode & (SPI_RX_QUAD | SPI_RX_DUAL)) tr.tx_buf = 0; } ret = ioctl(fd, SPI_IOC_MESSAGE(1), &tr); if (ret < 1) pabort("can't send spi message"); //if (verbose) hex_dump(tx, len, 8, "TX"); //if (verbose) hex_dump(rx, len+3, 8, "RX"); } static void print_usage(const char *prog) { printf("Usage: %s [-DsbdlHOLC3vpNR24SI]\n", prog); puts(" -D --device device to use (default /dev/spidev1.1)\n" " -s --speed max speed (Hz)\n" " -d --delay delay (usec)\n" " -b --bpw bits per word\n" " -i --input input data from a file (e.g. \"test.bin\")\n" " -o --output output data to a file (e.g. \"results.bin\")\n" " -l --loop loopback\n" " -H --cpha clock phase\n" " -O --cpol clock polarity\n" " -L --lsb least significant bit first\n" " -C --cs-high chip select active high\n" " -3 --3wire SI/SO signals shared\n" " -v --verbose Verbose (show tx buffer)\n" " -p Send data (e.g. \"1234\\xde\\xad\")\n" " -N --no-cs no chip select\n" " -R --ready slave pulls low to pause\n" " -2 --dual dual transfer\n" " -4 --quad quad transfer\n" " -S --size transfer size\n" " -I --iter iterations\n"); exit(1); } static void parse_opts(int argc, char *argv[]) { while (1) { static const struct option lopts[] = { { "device", 1, 0, 'D' }, { "speed", 1, 0, 's' }, { "delay", 1, 0, 'd' }, { "bpw", 1, 0, 'b' }, { "input", 1, 0, 'i' }, { "output", 1, 0, 'o' }, { "loop", 0, 0, 'l' }, { "cpha", 0, 0, 'H' }, { "cpol", 0, 0, 'O' }, { "lsb", 0, 0, 'L' }, { "cs-high", 0, 0, 'C' }, { "3wire", 0, 0, '3' }, { "no-cs", 0, 0, 'N' }, { "ready", 0, 0, 'R' }, { "dual", 0, 0, '2' }, { "verbose", 0, 0, 'v' }, { "quad", 0, 0, '4' }, { "size", 1, 0, 'S' }, { "iter", 1, 0, 'I' }, { NULL, 0, 0, 0 }, }; int c; c = getopt_long(argc, argv, "D:s:d:b:i:o:lHOLC3NR24p:vS:I:", lopts, NULL); if (c == -1) break; switch (c) { case 'D': device = optarg; break; case 's': speed = atoi(optarg); break; case 'd': delay = atoi(optarg); break; case 'b': bits = atoi(optarg); break; case 'i': input_file = optarg; break; case 'o': output_file = optarg; break; case 'l': mode |= SPI_LOOP; break; case 'H': mode |= SPI_CPHA; break; case 'O': mode |= SPI_CPOL; break; case 'L': mode |= SPI_LSB_FIRST; break; case 'C': mode |= SPI_CS_HIGH; break; case '3': mode |= SPI_3WIRE; break; case 'N': mode |= SPI_NO_CS; break; case 'v': verbose = 1; break; case 'R': mode |= SPI_READY; break; case 'p': input_tx = optarg; break; case '2': mode |= SPI_TX_DUAL; break; case '4': mode |= SPI_TX_QUAD; break; case 'S': transfer_size = atoi(optarg); break; case 'I': iterations = atoi(optarg); break; default: print_usage(argv[0]); break; } } if (mode & SPI_LOOP) { if (mode & SPI_TX_DUAL) mode |= SPI_RX_DUAL; if (mode & SPI_TX_QUAD) mode |= SPI_RX_QUAD; } } static uint64_t _read_count; static uint64_t _write_count; /* SPI command definition */ #define HW_SPI_NOP_CMD 0x00 #define HW_SPI_READ_CMD 0x02 #define HW_SPI_READ_WITH_WAIT_CMD 0x03 #define HW_SPI_WRITE_CMD 0x04 #define HW_SPI_ADDR_EXT_CMD 0x06 #define HW_SPI_CMD_MASK 0x07 int main(int argc, char *argv[]) { int ret = 0; int fd; parse_opts(argc, argv); fd = open(device, O_RDWR); if (fd < 0) pabort("can't open device"); /* * spi mode */ mode = SPI_CPOL | SPI_CPHA; ret = ioctl(fd, SPI_IOC_WR_MODE32, &mode); if (ret == -1) pabort("can't set spi mode"); //ret = ioctl(fd, SPI_IOC_RD_MODE32, &mode); //if (ret == -1) // pabort("can't get spi mode"); /* * bits per word */ ret = ioctl(fd, SPI_IOC_WR_BITS_PER_WORD, &bits); if (ret == -1) pabort("can't set bits per word"); //ret = ioctl(fd, SPI_IOC_RD_BITS_PER_WORD, &bits); //if (ret == -1) // pabort("can't get bits per word"); /* * max speed hz */ ret = ioctl(fd, SPI_IOC_WR_MAX_SPEED_HZ, &speed); if (ret == -1) pabort("can't set max speed hz"); //ret = ioctl(fd, SPI_IOC_RD_MAX_SPEED_HZ, &speed); //if (ret == -1) // pabort("can't get max speed hz"); printf("spi mode: 0x%x\n", mode); printf("bits per word: %d\n", bits); printf("max speed: %d Hz (%d KHz)\n", speed, speed/1000); //addr=0x0000 type memset(default_tx, 0, sizeof(default_tx)); default_tx[0] = 0x00; default_tx[1] = 0x00 | HW_SPI_ADDR_EXT_CMD; default_tx[2] = (0x00 & 0xe0) | (HW_SPI_READ_CMD << 2); default_tx[3] = 0xFF;//dummy default_tx[3+1] = 0x0;//data default_tx[3+1] = 0xFF;//data //default_tx[5] = 0xFF; transfer(fd, default_tx, default_rx, 5);//sizeof(default_tx)); //addr=0x0001 version memset(default_tx, 0, sizeof(default_tx)); default_tx[0] = 0x01; default_tx[1] = 0x00 | HW_SPI_ADDR_EXT_CMD; default_tx[2] = (0x01 & 0xe0) | (HW_SPI_READ_CMD << 2); default_tx[3] = 0xFF;//dummy default_tx[3+1] = 0x0;//data default_tx[3+1] = 0xFF;//data //default_tx[5] = 0xFF; transfer(fd, default_tx, default_rx, 5);//sizeof(default_tx)); close(fd); return ret; }
Btw, I also tried to set SPI mode with dual mode, but it cannot set the device as well.
root@AX-564EB0MB1T:/home# ./spiTest
spi mode: 0x103
bits per word: 8
max speed: 400000 Hz (400 KHz)
can't send spi message: Invalid argument
Aborted
Thanks.
Eric