Other Parts Discussed in Thread: DRA821
I am trying to build a recipe in the TI-SDK 08_04_00_06, what I am trying to build is sysbench application.
I downloaded and install the gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu cross compiler
When I try to build I get the following error, what should the MACHINE= be ? I have tried aarch64 and j7-evm but it does not seem to work correctly with either, but id does seem to go further with aarch64
nbdev@nbdev:~/ti-processor-sdk-linux-j7200-evm-08_04_00_06/yocto-build/build$ TOOLCHAIN_BASE=/home/nbdev MACHINE=aarch64 bitbake sysbench
WARNING: Layer meta-psdkla should set LAYERSERIES_COMPAT_meta-psdkla in its conf/layer.conf file to list the core layer names it is compatible with.
NOTE: Started PRServer with DBfile: /home/nbdev/ti-processor-sdk-linux-j7200-evm-08_04_00_06/yocto-build/build/cache/prserv.sqlite3, IP: 127.0.0.1, PORT: 44345, PID: 20533
WARNING: Layer meta-psdkla should set LAYERSERIES_COMPAT_meta-psdkla in its conf/layer.conf file to list the core layer names it is compatible with.
ERROR: OE-core's config sanity checker detected a potential misconfiguration.
Either fix the cause of this error or at your own risk disable the checker (see sanity.conf).
Following is the list of potential problems / advisories:
MACHINE=aarch64 is invalid. Please set a valid MACHINE in your local.conf, environment or other configuration file.