This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Questions about LDC output image in DCC of TDA4

Part Number: TDA4VM

Hi TI experts,

The mesh lut files was generated follow the step of the case [FAQ] TDA4VM: How to create a LDC mesh LUT for fisheye distortion correction on TDA4?, however, I found that the output image of LDC has one problem, the last line of the image is messy green, as shown in figure below:

   

do you know what cause this?

another question is that the YUV image saved by DCC is not processed by LDC, is that normal?

The xml file  is attached here for check:

6761.OVX3C-MAX9295_MARS_mesh_ldc_dcc.xml
Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
<?xml version="1.0" encoding="utf-8"?>
<cfg_ldc_xml xmlns:xsi="http://www.w3.org/2001/xmlschema-instance" xmlns:xsd="http://www.w3.org/2001/xmlschema">
<!--this is a comment-->
<dcc_name>cfg_ldc</dcc_name>
<dcc_header>
<camera_module_id> 233 </camera_module_id>
<dcc_descriptor_id> 5 </dcc_descriptor_id>
<algorithm_vendor_id> 1 </algorithm_vendor_id>
<tunning_tool_version> 0 </tunning_tool_version>
</dcc_header>
<!--=======================================================================-->
<typedef>
<cfg_ldc_vars type="struct">
<ldc_en type="uint16"> </ldc_en>
<ldc_ldmapen type="uint16"> </ldc_ldmapen>
<ldc_datamode type="uint16"> </ldc_datamode>
<ldc_opdatamode type="uint16"> </ldc_opdatamode>
<ldc_ip_dfmt type="uint16"> </ldc_ip_dfmt>
<ldc_pwarpen type="uint16"> </ldc_pwarpen>
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX
   

4578.OVX3C-MAX9295_MARS_mesh_lut.txt