Part Number: LP-AM263
Hi,
I'm working on a project to interface with a third party sensor array. The HAL test provided by the vendor involves using a GPIO pin that is polled as well as being connected to an ISR.
I am starting from the gpio_input_interrupt example in SDK version 08.05.00.24. When I change the syscfg file so that gpio1.GPIO_gpioPin.$assign = "EPWM0_A" and connect a wire to J2.11 on my launchpad, the interrupt is never triggered when I connect that pin between GND and 3.3V. Is there another step that I'm missing to connect that pin to an interrupt?
Also, when using the original pin connected to SW4, I added the line "DebugP_log("Current key value: %d\r\n", GPIO_pinRead(bankNum, pinNum)" to get the current value of the interrupt pin, but it always reads as 0, even when I am holding the button. Is there another function that should be used to read interrupt pins?
Thanks,
Mike