Dear all,
I am facing an issue with loading the CCS compiled executable using mpmcl load command.
But, using CCS it is loading and executing well.
Observing the following error on loading.
root@k2hk-evm:~# mpmcl load dsp4 exe.out
can't send data to /var/run/mpm/mpm_daemon (error: Connection refused)
load failed (error: 0)
what could be the issue? Any additional compilation flags to be set in CCS for loading with mpmcl?