Other Parts Discussed in Thread: OPA362, TPD12S015
Hello,
I am trying to implement a dts file for a half duplex communication with modbus devices via rs485. I have a custom beaglebone based in beaglebone black with a rs485 input. I want to create a dts file to control properly the rts signal. The rts signal its responsible to control if my device gonna read or write in the channel (both functions in the same time dont work due too half duplex communication). For now i have created a dts file, a script to send a command via the port and i have a logic analyzer to see what happens. The problem i have its that the rts signal its way off. It should be low and when i am sending the command(tx) become high, until the command send and become low again to read the response(no response for now as i am connected with the logic analyzer). Can you provide any dts file for this usage or explain what i should do?
I am providing a link with the dts and script files and a screenshot from logic analyzer (https://we.tl/t-OxwD2nOlnq).
Thank you in advance,
Panos.