Hi,
when compiling some code for the PRU of the AM3358, the compiler crashes:
INTERNAL ERROR: optpru experienced a segmentation fault while processing function main file /tmp/TI0LRs1EyhN This is caused by a defect in the TI C/C++ Optimizer. TI Customer Support may be able to suggest a workaround to avoid this.
The funny thing here: when I add the option "--preproc_with_comment" to the compiler call, the issue is gone and the crash does not happen any more.
What I have added last to my code and which seem to be related to that issue is the following macro:
#define SEND_LOGIC1_CELL \ { \ uint32_t reg; \ if (*state1==0) \ { \ reg=SL1_BIT; \ } \ else \ { \ reg=0; \ } \ if (*state2==0) \ { \ reg|=SL2_BIT; \ } \ else \ { \ __delay_cycles(1); \ } \ __R30=reg; \ if (*state1==1) \ { \ reg=SL1_BIT; \ } \ else \ { \ reg=0; \ } \ if (*state2==1) \ { \ reg|=SL2_BIT; \ } \ *pCtr1=*pCtr1+1; \ *pCtr2=*pCtr2+1; \ __delay_cycles(P0_CLOCK_CYCLES+2); \ __R30=reg; \ }
So that works for me right now, but may be this is an issue somebody at TI is interested in...