This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA829V: Connection between DRA829 and PCIe SW(PI7C9X3G1632GP)

Part Number: DRA829V
Other Parts Discussed in Thread: DRA829

Hi experts,

We want to connect a DRA829 with a PCIe SW(PI7C9X3G1632GP), but we cannot see the downstream of the PCIe SW and an error occurs.
Also tried to connect DRA829 with another PCIe SW, but result is similarly.

Q1:Is there something I need to configure in the device-tree of the DRA829? If you have any example settings, please let us know.

[Add 2023/5/8]

Q2:Could you please tell me which PCIe SWs TI have tested the connection with the DRA829EVM and their configurations?

We have tested connections between the DRA829EVM and several different PCIe SWs, but we get errors in the downstream port configuration on all PCIe SWs.
we are wondering if it is possible to connect PCIe SW to DRA829.

Best regards,
O.H