Part Number: DRA829V
Other Parts Discussed in Thread: DRA829, , TDA4VM, DRA821, AM69A
Hi experts,
*This is a re-post as the original thread is completely unresponsive.
We want to connect a DRA829 with a PCIe SW(PI7C9X3G1632GP), but we cannot see the downstream of the PCIe SW and an error occurs.
Also tried to connect DRA829 with another PCIe SW, but result is similarly.
Q1:Is there something I need to configure in the device-tree of the DRA829? If you have any example settings, please let us know.
Q2:Could you please tell me which PCIe SWs TI have tested the connection with the DRA829EVM and their configurations?
We have tested connections between the DRA829EVM and several different PCIe SWs, but we get errors in the downstream port configuration on all PCIe SWs.
we are wondering if it is possible to connect PCIe SW to DRA829.
Best regards,
O.H