Hi,.
We have a question from one of our clients.
They are looking at the value they are setting in each register to be on the safe side.
They have confirmed that the system is writing 1 to b[0] (AUTOIDLE) in UART's UART_SYSC.
However, the write of 1 is Reserved and cannot be determined.
Is there any problem with this write?
They are using Processor SDK Linux Ver. 07.03.00.005.
Best Regards,
Kouji Nishigata