This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI experts,
I follow "[FAQ] TDA4VM: How to create a LDC mesh LUT for fisheye distortion correction on TDA4?" to generate mesh table. While setting s=2; m=4, it has some many NaN in mesh table.
May I know how to decide suitable value for s and m?
0 0.000 0.1 0.005 0.2 0.010 0.3 0.015 0.4 0.020 0.5 0.025 0.6 0.030 0.7 0.036 0.8 0.041 0.9 0.046 1 0.051 1.1 0.056 1.2 0.061 1.3 0.066 1.4 0.071 1.5 0.076 1.6 0.081 1.7 0.086 1.8 0.091 1.9 0.097 2 0.102 2.1 0.107 2.2 0.112 2.3 0.117 2.4 0.122 2.5 0.127 2.6 0.132 2.7 0.137 2.8 0.142 2.9 0.147 3 0.152 3.1 0.157 3.2 0.163 3.3 0.168 3.4 0.173 3.5 0.178 3.6 0.183 3.7 0.188 3.8 0.193 3.9 0.198 4 0.203 4.1 0.208 4.2 0.213 4.3 0.218 4.4 0.223 4.5 0.229 4.6 0.234 4.7 0.239 4.8 0.244 4.9 0.249 5 0.254 5.1 0.259 5.2 0.264 5.3 0.269 5.4 0.274 5.5 0.279 5.6 0.284 5.7 0.289 5.8 0.295 5.9 0.300 6 0.305 6.1 0.310 6.2 0.315 6.3 0.320 6.4 0.325 6.5 0.330 6.6 0.335 6.7 0.340 6.8 0.345 6.9 0.350 7 0.355 7.1 0.360 7.2 0.366 7.3 0.371 7.4 0.376 7.5 0.381 7.6 0.386 7.7 0.391 7.8 0.396 7.9 0.401 8 0.406 8.1 0.411 8.2 0.416 8.3 0.421 8.4 0.426 8.5 0.431 8.6 0.436 8.7 0.442 8.8 0.447 8.9 0.452 9 0.457 9.1 0.462 9.2 0.467 9.3 0.472 9.4 0.477 9.5 0.482 9.6 0.487 9.7 0.492 9.8 0.497 9.9 0.502 10 0.507 10.1 0.512 10.2 0.517 10.3 0.522 10.4 0.528 10.5 0.533 10.6 0.538 10.7 0.543 10.8 0.548 10.9 0.553 11 0.558 11.1 0.563 11.2 0.568 11.3 0.573 11.4 0.578 11.5 0.583 11.6 0.588 11.7 0.593 11.8 0.598 11.9 0.603 12 0.608 12.1 0.613 12.2 0.618 12.3 0.624 12.4 0.629 12.5 0.634 12.6 0.639 12.7 0.644 12.8 0.649 12.9 0.654 13 0.659 13.1 0.664 13.2 0.669 13.3 0.674 13.4 0.679 13.5 0.684 13.6 0.689 13.7 0.694 13.8 0.699 13.9 0.704 14 0.709 14.1 0.714 14.2 0.719 14.3 0.724 14.4 0.729 14.5 0.734 14.6 0.739 14.7 0.744 14.8 0.749 14.9 0.754 15 0.760 15.1 0.765 15.2 0.770 15.3 0.775 15.4 0.780 15.5 0.785 15.6 0.790 15.7 0.795 15.8 0.800 15.9 0.805 16 0.810 16.1 0.815 16.2 0.820 16.3 0.825 16.4 0.830 16.5 0.835 16.6 0.840 16.7 0.845 16.8 0.850 16.9 0.855 17 0.860 17.1 0.865 17.2 0.870 17.3 0.875 17.4 0.880 17.5 0.885 17.6 0.890 17.7 0.895 17.8 0.900 17.9 0.905 18 0.910 18.1 0.915 18.2 0.920 18.3 0.925 18.4 0.930 18.5 0.935 18.6 0.940 18.7 0.945 18.8 0.950 18.9 0.955 19 0.960 19.1 0.965 19.2 0.970 19.3 0.975 19.4 0.980 19.5 0.985 19.6 0.990 19.7 0.995 19.8 1.000 19.9 1.005 20 1.010 20.1 1.015 20.2 1.020 20.3 1.025 20.4 1.030 20.5 1.035 20.6 1.040 20.7 1.045 20.8 1.050 20.9 1.055 21 1.060 21.1 1.065 21.2 1.070 21.3 1.075 21.4 1.080 21.5 1.085 21.6 1.090 21.7 1.094 21.8 1.099 21.9 1.104 22 1.109 22.1 1.114 22.2 1.119 22.3 1.124 22.4 1.129 22.5 1.134 22.6 1.139 22.7 1.144 22.8 1.149 22.9 1.154 23 1.159 23.1 1.164 23.2 1.169 23.3 1.174 23.4 1.179 23.5 1.184 23.6 1.189 23.7 1.194 23.8 1.199 23.9 1.204 24 1.208 24.1 1.213 24.2 1.218 24.3 1.223 24.4 1.228 24.5 1.233 24.6 1.238 24.7 1.243 24.8 1.248 24.9 1.253 25 1.258 25.1 1.263 25.2 1.268 25.3 1.273 25.4 1.277 25.5 1.282 25.6 1.287 25.7 1.292 25.8 1.297 25.9 1.302 26 1.307 26.1 1.312 26.2 1.317 26.3 1.322 26.4 1.327 26.5 1.332 26.6 1.336 26.7 1.341 26.8 1.346 26.9 1.351 27 1.356 27.1 1.361 27.2 1.366 27.3 1.371 27.4 1.376 27.5 1.381 27.6 1.385 27.7 1.390 27.8 1.395 27.9 1.400 28 1.405 28.1 1.410 28.2 1.415 28.3 1.420 28.4 1.425 28.5 1.429 28.6 1.434 28.7 1.439 28.8 1.444 28.9 1.449 29 1.454 29.1 1.459 29.2 1.464 29.3 1.468 29.4 1.473 29.5 1.478 29.6 1.483 29.7 1.488 29.8 1.493 29.9 1.498 30 1.503 30.1 1.507 30.2 1.512 30.3 1.517 30.4 1.522 30.5 1.527 30.6 1.532 30.7 1.537 30.8 1.541 30.9 1.546 31 1.551 31.1 1.556 31.2 1.561 31.3 1.566 31.4 1.570 31.5 1.575 31.6 1.580 31.7 1.585 31.8 1.590 31.9 1.595 32 1.599 32.1 1.604 32.2 1.609 32.3 1.614 32.4 1.619 32.5 1.624 32.6 1.628 32.7 1.633 32.8 1.638 32.9 1.643 33 1.648 33.1 1.652 33.2 1.657 33.3 1.662 33.4 1.667 33.5 1.672 33.6 1.676 33.7 1.681 33.8 1.686 33.9 1.691 34 1.696 34.1 1.700 34.2 1.705 34.3 1.710 34.4 1.715 34.5 1.720 34.6 1.724 34.7 1.729 34.8 1.734 34.9 1.739 35 1.743 35.1 1.748 35.2 1.753 35.3 1.758 35.4 1.763 35.5 1.767 35.6 1.772 35.7 1.777 35.8 1.782 35.9 1.786 36 1.791 36.1 1.796 36.2 1.801 36.3 1.805 36.4 1.810 36.5 1.815 36.6 1.820 36.7 1.824 36.8 1.829 36.9 1.834 37 1.839 37.1 1.843 37.2 1.848 37.3 1.853 37.4 1.858 37.5 1.862 37.6 1.867 37.7 1.872 37.8 1.876 37.9 1.881 38 1.886 38.1 1.891 38.2 1.895 38.3 1.900 38.4 1.905 38.5 1.909 38.6 1.914 38.7 1.919 38.8 1.924 38.9 1.928 39 1.933 39.1 1.938 39.2 1.942 39.3 1.947 39.4 1.952 39.5 1.956 39.6 1.961 39.7 1.966 39.8 1.971 39.9 1.975 40 1.980 40.1 1.985 40.2 1.989 40.3 1.994 40.4 1.999 40.5 2.003 40.6 2.008 40.7 2.013 40.8 2.017 40.9 2.022 41 2.027 41.1 2.031 41.2 2.036 41.3 2.041 41.4 2.045 41.5 2.050 41.6 2.055 41.7 2.059 41.8 2.064 41.9 2.068 42 2.073 42.1 2.078 42.2 2.082 42.3 2.087 42.4 2.092 42.5 2.096 42.6 2.101 42.7 2.106 42.8 2.110 42.9 2.115 43 2.119 43.1 2.124 43.2 2.129 43.3 2.133 43.4 2.138 43.5 2.142 43.6 2.147 43.7 2.152 43.8 2.156 43.9 2.161 44 2.165 44.1 2.170 44.2 2.175 44.3 2.179 44.4 2.184 44.5 2.188 44.6 2.193 44.7 2.198 44.8 2.202 44.9 2.207 45 2.211 45.1 2.216 45.2 2.220 45.3 2.225 45.4 2.230 45.5 2.234 45.6 2.239 45.7 2.243 45.8 2.248 45.9 2.252 46 2.257 46.1 2.261 46.2 2.266 46.3 2.271 46.4 2.275 46.5 2.280 46.6 2.284 46.7 2.289 46.8 2.293 46.9 2.298 47 2.302 47.1 2.307 47.2 2.311 47.3 2.316 47.4 2.320 47.5 2.325 47.6 2.329 47.7 2.334 47.8 2.338 47.9 2.343 48 2.347 48.1 2.352 48.2 2.356 48.3 2.361 48.4 2.365 48.5 2.370 48.6 2.374 48.7 2.379 48.8 2.383 48.9 2.388 49 2.392 49.1 2.397 49.2 2.401 49.3 2.406 49.4 2.410 49.5 2.415 49.6 2.419 49.7 2.424 49.8 2.428 49.9 2.432 50 2.437 50.1 2.441 50.2 2.446 50.3 2.450 50.4 2.455 50.5 2.459 50.6 2.464 50.7 2.468 50.8 2.472 50.9 2.477 51 2.481 51.1 2.486 51.2 2.490 51.3 2.495 51.4 2.499 51.5 2.503 51.6 2.508 51.7 2.512 51.8 2.517 51.9 2.521 52 2.525 52.1 2.530 52.2 2.534 52.3 2.539 52.4 2.543 52.5 2.547 52.6 2.552 52.7 2.556 52.8 2.560 52.9 2.565 53 2.569 53.1 2.574 53.2 2.578 53.3 2.582 53.4 2.587 53.5 2.591 53.6 2.595 53.7 2.600 53.8 2.604 53.9 2.608 54 2.613 54.1 2.617 54.2 2.621 54.3 2.626 54.4 2.630 54.5 2.634 54.6 2.639 54.7 2.643 54.8 2.647 54.9 2.652 55 2.656 55.1 2.660 55.2 2.664 55.3 2.669 55.4 2.673 55.5 2.677 55.6 2.682 55.7 2.686 55.8 2.690 55.9 2.694 56 2.699 56.1 2.703 56.2 2.707 56.3 2.711 56.4 2.716 56.5 2.720 56.6 2.724 56.7 2.728 56.8 2.733 56.9 2.737 57 2.741 57.1 2.745 57.2 2.750 57.3 2.754 57.4 2.758 57.5 2.762 57.6 2.766 57.7 2.771 57.8 2.775 57.9 2.779 58 2.783 58.1 2.787 58.2 2.792 58.3 2.796 58.4 2.800 58.5 2.804 58.6 2.808 58.7 2.813 58.8 2.817 58.9 2.821 59 2.825 59.1 2.829 59.2 2.833 59.3 2.838 59.4 2.842 59.5 2.846 59.6 2.850 59.7 2.854 59.8 2.858 59.9 2.862 60 2.866 60.1 2.871 60.2 2.875 60.3 2.879 60.4 2.883 60.5 2.887 60.6 2.891 60.7 2.895 60.8 2.899 60.9 2.903 61 2.907 61.1 2.911 61.2 2.916 61.3 2.920 61.4 2.924 61.5 2.928 61.6 2.932 61.7 2.936 61.8 2.940 61.9 2.944 62 2.948 62.1 2.952 62.2 2.956 62.3 2.960 62.4 2.964 62.5 2.968 62.6 2.972 62.7 2.976 62.8 2.980 62.9 2.984 63 2.988 63.1 2.992 63.2 2.996 63.3 3.000 63.4 3.004 63.5 3.008 63.6 3.012 63.7 3.016 63.8 3.020 63.9 3.024 64 3.028 64.1 3.032 64.2 3.035 64.3 3.039 64.4 3.043 64.5 3.047 64.6 3.051 64.7 3.055 64.8 3.059 64.9 3.063 65 3.067 65.1 3.071 65.2 3.074 65.3 3.078 65.4 3.082 65.5 3.086 65.6 3.090 65.7 3.094 65.8 3.098 65.9 3.101 66 3.105 66.1 3.109 66.2 3.113 66.3 3.117 66.4 3.120 66.5 3.124 66.6 3.128 66.7 3.132 66.8 3.136 66.9 3.139 67 3.143 67.1 3.147 67.2 3.151 67.3 3.154 67.4 3.158 67.5 3.162 67.6 3.166 67.7 3.169 67.8 3.173 67.9 3.177 68 3.181 68.1 3.184 68.2 3.188 68.3 3.192 68.4 3.195 68.5 3.199 68.6 3.203 68.7 3.206 68.8 3.210 68.9 3.214 69 3.217 69.1 3.221 69.2 3.225 69.3 3.228 69.4 3.232 69.5 3.235 69.6 3.239 69.7 3.243 69.8 3.246 69.9 3.250 70 3.253 70.1 3.257 70.2 3.261 70.3 3.264 70.4 3.268 70.5 3.271 70.6 3.275 70.7 3.278 70.8 3.282 70.9 3.285 71 3.289 71.1 3.292 71.2 3.296 71.3 3.299 71.4 3.303 71.5 3.306 71.6 3.310 71.7 3.313 71.8 3.317 71.9 3.320 72 3.324 72.1 3.327 72.2 3.330 72.3 3.334 72.4 3.337 72.5 3.341 72.6 3.344 72.7 3.347 72.8 3.351 72.9 3.354 73 3.357 73.1 3.361 73.2 3.364 73.3 3.367 73.4 3.371 73.5 3.374 73.6 3.377 73.7 3.381 73.8 3.384 73.9 3.387 74 3.391 74.1 3.394 74.2 3.397 74.3 3.400 74.4 3.404 74.5 3.407 74.6 3.410 74.7 3.413 74.8 3.417 74.9 3.420 75 3.423 75.1 3.426 75.2 3.429 75.3 3.433 75.4 3.436 75.5 3.439 75.6 3.442
Dear TI experts,
I upload spec_file.txt and mesh.txt that I use and generate. Could you help to check if there is anything wrong?
Thanks
Hi Gang Hua,
After adding 90 3.442 at the end of spec_file.txt, we can get mesh.txt as attachment. Coud you help to check if it is reasonable?
Thank you
Dear TI
I used cam_single.sh to capture two image
img_msc_0000_1904x1072.YUV and img_viss_0000_1934x1096.YUV
I have converted distortion table "spec_file.txt" to mesh.txt and my setting is W = 1904; H = 1072
Request to get YUV image from Target : Enter IP Address...
Loaded communication DLL:itCommun.dll
Request to get YUV image from Target : Enter IP Address...
Loaded communication DLL:itCommun.dll
Do I set any wrong?
img_msc_0000_1904x1072.rar6557.mesh.txt
0 0.000 0.1 0.005 0.2 0.010 0.3 0.015 0.4 0.020 0.5 0.025 0.6 0.030 0.7 0.036 0.8 0.041 0.9 0.046 1 0.051 1.1 0.056 1.2 0.061 1.3 0.066 1.4 0.071 1.5 0.076 1.6 0.081 1.7 0.086 1.8 0.091 1.9 0.097 2 0.102 2.1 0.107 2.2 0.112 2.3 0.117 2.4 0.122 2.5 0.127 2.6 0.132 2.7 0.137 2.8 0.142 2.9 0.147 3 0.152 3.1 0.157 3.2 0.163 3.3 0.168 3.4 0.173 3.5 0.178 3.6 0.183 3.7 0.188 3.8 0.193 3.9 0.198 4 0.203 4.1 0.208 4.2 0.213 4.3 0.218 4.4 0.223 4.5 0.229 4.6 0.234 4.7 0.239 4.8 0.244 4.9 0.249 5 0.254 5.1 0.259 5.2 0.264 5.3 0.269 5.4 0.274 5.5 0.279 5.6 0.284 5.7 0.289 5.8 0.295 5.9 0.300 6 0.305 6.1 0.310 6.2 0.315 6.3 0.320 6.4 0.325 6.5 0.330 6.6 0.335 6.7 0.340 6.8 0.345 6.9 0.350 7 0.355 7.1 0.360 7.2 0.366 7.3 0.371 7.4 0.376 7.5 0.381 7.6 0.386 7.7 0.391 7.8 0.396 7.9 0.401 8 0.406 8.1 0.411 8.2 0.416 8.3 0.421 8.4 0.426 8.5 0.431 8.6 0.436 8.7 0.442 8.8 0.447 8.9 0.452 9 0.457 9.1 0.462 9.2 0.467 9.3 0.472 9.4 0.477 9.5 0.482 9.6 0.487 9.7 0.492 9.8 0.497 9.9 0.502 10 0.507 10.1 0.512 10.2 0.517 10.3 0.522 10.4 0.528 10.5 0.533 10.6 0.538 10.7 0.543 10.8 0.548 10.9 0.553 11 0.558 11.1 0.563 11.2 0.568 11.3 0.573 11.4 0.578 11.5 0.583 11.6 0.588 11.7 0.593 11.8 0.598 11.9 0.603 12 0.608 12.1 0.613 12.2 0.618 12.3 0.624 12.4 0.629 12.5 0.634 12.6 0.639 12.7 0.644 12.8 0.649 12.9 0.654 13 0.659 13.1 0.664 13.2 0.669 13.3 0.674 13.4 0.679 13.5 0.684 13.6 0.689 13.7 0.694 13.8 0.699 13.9 0.704 14 0.709 14.1 0.714 14.2 0.719 14.3 0.724 14.4 0.729 14.5 0.734 14.6 0.739 14.7 0.744 14.8 0.749 14.9 0.754 15 0.760 15.1 0.765 15.2 0.770 15.3 0.775 15.4 0.780 15.5 0.785 15.6 0.790 15.7 0.795 15.8 0.800 15.9 0.805 16 0.810 16.1 0.815 16.2 0.820 16.3 0.825 16.4 0.830 16.5 0.835 16.6 0.840 16.7 0.845 16.8 0.850 16.9 0.855 17 0.860 17.1 0.865 17.2 0.870 17.3 0.875 17.4 0.880 17.5 0.885 17.6 0.890 17.7 0.895 17.8 0.900 17.9 0.905 18 0.910 18.1 0.915 18.2 0.920 18.3 0.925 18.4 0.930 18.5 0.935 18.6 0.940 18.7 0.945 18.8 0.950 18.9 0.955 19 0.960 19.1 0.965 19.2 0.970 19.3 0.975 19.4 0.980 19.5 0.985 19.6 0.990 19.7 0.995 19.8 1.000 19.9 1.005 20 1.010 20.1 1.015 20.2 1.020 20.3 1.025 20.4 1.030 20.5 1.035 20.6 1.040 20.7 1.045 20.8 1.050 20.9 1.055 21 1.060 21.1 1.065 21.2 1.070 21.3 1.075 21.4 1.080 21.5 1.085 21.6 1.090 21.7 1.094 21.8 1.099 21.9 1.104 22 1.109 22.1 1.114 22.2 1.119 22.3 1.124 22.4 1.129 22.5 1.134 22.6 1.139 22.7 1.144 22.8 1.149 22.9 1.154 23 1.159 23.1 1.164 23.2 1.169 23.3 1.174 23.4 1.179 23.5 1.184 23.6 1.189 23.7 1.194 23.8 1.199 23.9 1.204 24 1.208 24.1 1.213 24.2 1.218 24.3 1.223 24.4 1.228 24.5 1.233 24.6 1.238 24.7 1.243 24.8 1.248 24.9 1.253 25 1.258 25.1 1.263 25.2 1.268 25.3 1.273 25.4 1.277 25.5 1.282 25.6 1.287 25.7 1.292 25.8 1.297 25.9 1.302 26 1.307 26.1 1.312 26.2 1.317 26.3 1.322 26.4 1.327 26.5 1.332 26.6 1.336 26.7 1.341 26.8 1.346 26.9 1.351 27 1.356 27.1 1.361 27.2 1.366 27.3 1.371 27.4 1.376 27.5 1.381 27.6 1.385 27.7 1.390 27.8 1.395 27.9 1.400 28 1.405 28.1 1.410 28.2 1.415 28.3 1.420 28.4 1.425 28.5 1.429 28.6 1.434 28.7 1.439 28.8 1.444 28.9 1.449 29 1.454 29.1 1.459 29.2 1.464 29.3 1.468 29.4 1.473 29.5 1.478 29.6 1.483 29.7 1.488 29.8 1.493 29.9 1.498 30 1.503 30.1 1.507 30.2 1.512 30.3 1.517 30.4 1.522 30.5 1.527 30.6 1.532 30.7 1.537 30.8 1.541 30.9 1.546 31 1.551 31.1 1.556 31.2 1.561 31.3 1.566 31.4 1.570 31.5 1.575 31.6 1.580 31.7 1.585 31.8 1.590 31.9 1.595 32 1.599 32.1 1.604 32.2 1.609 32.3 1.614 32.4 1.619 32.5 1.624 32.6 1.628 32.7 1.633 32.8 1.638 32.9 1.643 33 1.648 33.1 1.652 33.2 1.657 33.3 1.662 33.4 1.667 33.5 1.672 33.6 1.676 33.7 1.681 33.8 1.686 33.9 1.691 34 1.696 34.1 1.700 34.2 1.705 34.3 1.710 34.4 1.715 34.5 1.720 34.6 1.724 34.7 1.729 34.8 1.734 34.9 1.739 35 1.743 35.1 1.748 35.2 1.753 35.3 1.758 35.4 1.763 35.5 1.767 35.6 1.772 35.7 1.777 35.8 1.782 35.9 1.786 36 1.791 36.1 1.796 36.2 1.801 36.3 1.805 36.4 1.810 36.5 1.815 36.6 1.820 36.7 1.824 36.8 1.829 36.9 1.834 37 1.839 37.1 1.843 37.2 1.848 37.3 1.853 37.4 1.858 37.5 1.862 37.6 1.867 37.7 1.872 37.8 1.876 37.9 1.881 38 1.886 38.1 1.891 38.2 1.895 38.3 1.900 38.4 1.905 38.5 1.909 38.6 1.914 38.7 1.919 38.8 1.924 38.9 1.928 39 1.933 39.1 1.938 39.2 1.942 39.3 1.947 39.4 1.952 39.5 1.956 39.6 1.961 39.7 1.966 39.8 1.971 39.9 1.975 40 1.980 40.1 1.985 40.2 1.989 40.3 1.994 40.4 1.999 40.5 2.003 40.6 2.008 40.7 2.013 40.8 2.017 40.9 2.022 41 2.027 41.1 2.031 41.2 2.036 41.3 2.041 41.4 2.045 41.5 2.050 41.6 2.055 41.7 2.059 41.8 2.064 41.9 2.068 42 2.073 42.1 2.078 42.2 2.082 42.3 2.087 42.4 2.092 42.5 2.096 42.6 2.101 42.7 2.106 42.8 2.110 42.9 2.115 43 2.119 43.1 2.124 43.2 2.129 43.3 2.133 43.4 2.138 43.5 2.142 43.6 2.147 43.7 2.152 43.8 2.156 43.9 2.161 44 2.165 44.1 2.170 44.2 2.175 44.3 2.179 44.4 2.184 44.5 2.188 44.6 2.193 44.7 2.198 44.8 2.202 44.9 2.207 45 2.211 45.1 2.216 45.2 2.220 45.3 2.225 45.4 2.230 45.5 2.234 45.6 2.239 45.7 2.243 45.8 2.248 45.9 2.252 46 2.257 46.1 2.261 46.2 2.266 46.3 2.271 46.4 2.275 46.5 2.280 46.6 2.284 46.7 2.289 46.8 2.293 46.9 2.298 47 2.302 47.1 2.307 47.2 2.311 47.3 2.316 47.4 2.320 47.5 2.325 47.6 2.329 47.7 2.334 47.8 2.338 47.9 2.343 48 2.347 48.1 2.352 48.2 2.356 48.3 2.361 48.4 2.365 48.5 2.370 48.6 2.374 48.7 2.379 48.8 2.383 48.9 2.388 49 2.392 49.1 2.397 49.2 2.401 49.3 2.406 49.4 2.410 49.5 2.415 49.6 2.419 49.7 2.424 49.8 2.428 49.9 2.432 50 2.437 50.1 2.441 50.2 2.446 50.3 2.450 50.4 2.455 50.5 2.459 50.6 2.464 50.7 2.468 50.8 2.472 50.9 2.477 51 2.481 51.1 2.486 51.2 2.490 51.3 2.495 51.4 2.499 51.5 2.503 51.6 2.508 51.7 2.512 51.8 2.517 51.9 2.521 52 2.525 52.1 2.530 52.2 2.534 52.3 2.539 52.4 2.543 52.5 2.547 52.6 2.552 52.7 2.556 52.8 2.560 52.9 2.565 53 2.569 53.1 2.574 53.2 2.578 53.3 2.582 53.4 2.587 53.5 2.591 53.6 2.595 53.7 2.600 53.8 2.604 53.9 2.608 54 2.613 54.1 2.617 54.2 2.621 54.3 2.626 54.4 2.630 54.5 2.634 54.6 2.639 54.7 2.643 54.8 2.647 54.9 2.652 55 2.656 55.1 2.660 55.2 2.664 55.3 2.669 55.4 2.673 55.5 2.677 55.6 2.682 55.7 2.686 55.8 2.690 55.9 2.694 56 2.699 56.1 2.703 56.2 2.707 56.3 2.711 56.4 2.716 56.5 2.720 56.6 2.724 56.7 2.728 56.8 2.733 56.9 2.737 57 2.741 57.1 2.745 57.2 2.750 57.3 2.754 57.4 2.758 57.5 2.762 57.6 2.766 57.7 2.771 57.8 2.775 57.9 2.779 58 2.783 58.1 2.787 58.2 2.792 58.3 2.796 58.4 2.800 58.5 2.804 58.6 2.808 58.7 2.813 58.8 2.817 58.9 2.821 59 2.825 59.1 2.829 59.2 2.833 59.3 2.838 59.4 2.842 59.5 2.846 59.6 2.850 59.7 2.854 59.8 2.858 59.9 2.862 60 2.866 60.1 2.871 60.2 2.875 60.3 2.879 60.4 2.883 60.5 2.887 60.6 2.891 60.7 2.895 60.8 2.899 60.9 2.903 61 2.907 61.1 2.911 61.2 2.916 61.3 2.920 61.4 2.924 61.5 2.928 61.6 2.932 61.7 2.936 61.8 2.940 61.9 2.944 62 2.948 62.1 2.952 62.2 2.956 62.3 2.960 62.4 2.964 62.5 2.968 62.6 2.972 62.7 2.976 62.8 2.980 62.9 2.984 63 2.988 63.1 2.992 63.2 2.996 63.3 3.000 63.4 3.004 63.5 3.008 63.6 3.012 63.7 3.016 63.8 3.020 63.9 3.024 64 3.028 64.1 3.032 64.2 3.035 64.3 3.039 64.4 3.043 64.5 3.047 64.6 3.051 64.7 3.055 64.8 3.059 64.9 3.063 65 3.067 65.1 3.071 65.2 3.074 65.3 3.078 65.4 3.082 65.5 3.086 65.6 3.090 65.7 3.094 65.8 3.098 65.9 3.101 66 3.105 66.1 3.109 66.2 3.113 66.3 3.117 66.4 3.120 66.5 3.124 66.6 3.128 66.7 3.132 66.8 3.136 66.9 3.139 67 3.143 67.1 3.147 67.2 3.151 67.3 3.154 67.4 3.158 67.5 3.162 67.6 3.166 67.7 3.169 67.8 3.173 67.9 3.177 68 3.181 68.1 3.184 68.2 3.188 68.3 3.192 68.4 3.195 68.5 3.199 68.6 3.203 68.7 3.206 68.8 3.210 68.9 3.214 69 3.217 69.1 3.221 69.2 3.225 69.3 3.228 69.4 3.232 69.5 3.235 69.6 3.239 69.7 3.243 69.8 3.246 69.9 3.250 70 3.253 70.1 3.257 70.2 3.261 70.3 3.264 70.4 3.268 70.5 3.271 70.6 3.275 70.7 3.278 70.8 3.282 70.9 3.285 71 3.289 71.1 3.292 71.2 3.296 71.3 3.299 71.4 3.303 71.5 3.306 71.6 3.310 71.7 3.313 71.8 3.317 71.9 3.320 72 3.324 72.1 3.327 72.2 3.330 72.3 3.334 72.4 3.337 72.5 3.341 72.6 3.344 72.7 3.347 72.8 3.351 72.9 3.354 73 3.357 73.1 3.361 73.2 3.364 73.3 3.367 73.4 3.371 73.5 3.374 73.6 3.377 73.7 3.381 73.8 3.384 73.9 3.387 74 3.391 74.1 3.394 74.2 3.397 74.3 3.400 74.4 3.404 74.5 3.407 74.6 3.410 74.7 3.413 74.8 3.417 74.9 3.420 75 3.423 75.1 3.426 75.2 3.429 75.3 3.433 75.4 3.436 75.5 3.439 75.6 3.442 75.7 3.445 75.8 3.448 75.9 3.451 76 3.455 76.1 3.458 76.2 3.461 76.3 3.464 76.4 3.467 76.5 3.470 76.6 3.473 76.7 3.476 76.8 3.479 76.9 3.482 77 3.485 77.1 3.488 77.2 3.491 77.3 3.494 77.4 3.497 77.5 3.500 77.6 3.503 77.7 3.506 77.8 3.509 77.9 3.512 78 3.515 78.1 3.518 78.2 3.521 78.3 3.524 78.4 3.527 78.5 3.530 78.6 3.532 78.7 3.535 78.8 3.538 78.9 3.541 79 3.544 79.1 3.547 79.2 3.550 79.3 3.552 79.4 3.555 79.5 3.558 79.6 3.561 79.7 3.564 79.8 3.566 79.9 3.569 80 3.572 80.1 3.575 80.2 3.577 80.3 3.580 80.4 3.583 80.5 3.585 80.6 3.588 80.7 3.591 80.8 3.593 80.9 3.596 81 3.599 81.1 3.601 81.2 3.604 81.3 3.607 81.4 3.609 81.5 3.612 81.6 3.614 81.7 3.617 81.8 3.620 81.9 3.622 82 3.625 82.1 3.627 82.2 3.630 82.3 3.632 82.4 3.635 82.5 3.637 82.6 3.640 82.7 3.642 82.8 3.645 82.9 3.647 83 3.650 83.1 3.652 83.2 3.655 83.3 3.657 83.4 3.659 83.5 3.662 83.6 3.664 83.7 3.666 83.8 3.669 83.9 3.671 84 3.674 84.1 3.676 84.2 3.678 84.3 3.680 84.4 3.683 84.5 3.685 84.6 3.687 84.7 3.690 84.8 3.692 84.9 3.694 85 3.696 85.1 3.699 85.2 3.701 85.3 3.703 85.4 3.705 85.5 3.707 85.6 3.709 85.7 3.712 85.8 3.714 85.9 3.716 86 3.718 86.1 3.720 86.2 3.722 86.3 3.724 86.4 3.726 86.5 3.728 86.6 3.730 86.7 3.733 86.8 3.735 86.9 3.737 87 3.739 87.1 3.741 87.2 3.743 87.3 3.745 87.4 3.746 87.5 3.748 87.6 3.750 87.7 3.752 87.8 3.754 87.9 3.756 88 3.758 88.1 3.760 88.2 3.762 88.3 3.764 88.4 3.765 88.5 3.767 88.6 3.769 88.7 3.771 88.8 3.773 88.9 3.774 89 3.776 89.1 3.778 89.2 3.780 89.3 3.781 89.4 3.783 89.5 3.785 89.6 3.787 89.7 3.788 89.8 3.790 89.9 3.792 90 3.793
Do I set any wrong?
Not really wrong, but your output view goes out of your input view by too much.
You may use smaller "s" values for smaller output view and try again.
seems OK but the top area have some dislocation, can you give me suggestion to modify it?
Same problem as above
You output view on the top is going out of your input image boundary.
LDC H/W repeats input image border pixels when it is getting out of boundary.
You will need to plan your output view properly according to your lens distortion geometry.
Hi Gang
OK, I will try smaller "s" values
How could I build the new bin to camera module
I copy xml to imaging\sensor_drv\src\imx390 and run the "generate_dcc.sh"
Then, It generated some new bin, but i don't know how to use it.
I built imaging and sdk and copy .out to sdk, but It still not work
Thanks
Dear Gang
Could you give me more detail.
I have downloaded pre-build RTOS and source code RTOS
I copied pre-build RTOS and It's workful.
Now, I modified imaging\sensor_drv\src\imx390 in source code RTOS and run the "generate_dcc.sh" and got new bin
Could I just copied bin to sdcard? If yes, where is the path?
Or what is the procedure I need to do?
I made vision_app, sdk, and imaging, then copied all .out to sdcard, but nothing changed.
Or I don't need to make anything, just after modifying then make linux_fs_install_sd?
Thanks
Hi Gang
We are successful to modify parameters.
But I have some questions.
1. I used vision_app script single_cam to take picture, then I only can get img_msc_0000_1904x1072.YUV and img_viss_0000_1934x1096.YUV
But the imx390 config defines IMX390_1920x1080 to preview
2. I used img_msc_0000_1904x1072.YUV to do LDC, DCC simulation is OK, but I push to SD card that the preview is not right, so I need to use 1920x1080 to preduce parameters
How could I take 1920x1080 YUV or RAW?
I need it to simulate LDC on DCC tool
Thanks
Hi Will,
I am not sure about these questions.
IMX390 sensor output raw image and VISS output YUV should be both 1936x1096 if you have not changed the IMX390 sensor driver.
LDC output in PSDK is configured to 1920x1080 in the single-cam app.
Hi Gang
I understand IMX390 sensor output raw image and VISS output YUV should be both 1936x1096
And LDC output in PSDK is configured to 1920x1080
But I need to re-correction LDC, because the LDC is wrong now
So, I need to take 1920x1080 YUV, then I can use DCC tool to re-gen LDC table like this "ldc_xml_IMX390_1920x1080_2.txt"
If I use YUV 1936x1096 to gen 1920x1080 LDC table on DCC tool, the DCC output is wrong
Thanks
Hi Gang
Let me explain my problem
First of all, there is a sample code in TDA4VH-Q1 source code
imaging\sensor_drv\src\imx390\dcc_xmls\wdr\ldc_xml_IMX390_1920x1080_3.txt
I took a YUV image img_viss_0000_1934x1096 to simulate LDC parameter
I set input image size 1934x1096, and output image size 1280x720, then the DCC preview like that.
But If i put the parameter code to code base, modify IMX390_ldc.xml and ldc_xml_IMX390_1934x1096_1.txt
The real preview is like this
So the real resolution is not fitting 1934x1096.
Then I ignored the input size 1934x1096, I used sample resolution 1920x1080 to simulate LDC, now the DCC preview is wrong but output parameter is right for code base.
So, I suspect that I only can use 1920x1080 to simulate. So, I need to take 1920x1080 YUV, but I don't know how to take it
Thanks
First of all, there is a sample code in TDA4VH-Q1 source code
Do you use "app_single_cam" under "vision_apps"?
The sensor output RAW and VISS output YUV should be both 1936x1096.
I am not sure why you have 1934 instead.
When I press "s" key at "app_single_cam", it saves the raw and yuv images with the size below.
RAW file name .//img_0000.raw YUV file name .//img_viss_0000.yuv imgaddr_width = 1936 imgaddr_height = 1096 imgaddr_stride = 1936 width = 1936 height = 1096 YUV file name .//img_ldc_0000.yuv imgaddr_width = 1920 imgaddr_height = 1080 imgaddr_stride = 1920 width = 1920 height = 1080
I suppose LDC output size is decided by "app_single_cam" while creating the LDC openvx node.
If you need to modify LDC output size, you may have to change the LDC node settings.
Hi Gang
That's my mistake.
RAW file name .//img_0000.raw
YUV file name .//img_viss_0000.yuv
imgaddr_width = 1936
imgaddr_height = 1096
imgaddr_stride = 1936
width = 1936
height = 1096
This is what i got.
Then, I need to get 1920x1080 YUV to simulate LDC,
Because, as i mentioned before, I can't use 1936x1096 YUV to simulate LDC on DCC tool
because If I use the output XML code base, I only can get wrong preview.
Can you give me more specific infornation about where i need to modify.
1. How to get 1920x1080 YUV?
2. If i need to modify LDC output, I only need to get new XML or i need to modify source code
Thanks
Then, I need to get 1920x1080 YUV to simulate LDC,
Because, as i mentioned before, I can't use 1936x1096 YUV to simulate LDC on DCC tool
Your LDC input is from VISS output and it should be 1936x1096.
You should use 1936x1096 for LDC input in tuning tool as well.
because If I use the output XML code base, I only can get wrong preview.
I suppose you should be able set LDC output size to 1936x1096 in tuning tool.
2. If i need to modify LDC output, I only need to get new XML or i need to modify source code
If you use the single-cam app, please refer to "app_create_ldc(...)" in "app_single_cam_common.c".
I believe "obj->ldc_out" is the LDC output image.
Hi Gang
We saw some DCC XML parameters were written app_single_cam_common.h
#define LDC_TABLE_WIDTH (1920)
#define LDC_TABLE_HEIGHT (1080)
#define LDC_DS_FACTOR (2)
#define LDC_BLOCK_WIDTH (64)
#define LDC_BLOCK_HEIGHT (32)
#define LDC_PIXEL_PAD (1)
I am confused, if i want use DCC XML config, which app i need to use?
Thanks