Dear Mr. /Mrs.
I would like to know the Juntion Temperature of the TMS320C6203B DSP. In the datasheet is only available the operating case temperature:
Thanks in advance,
Best regards.
Carlos Antón.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Mr. /Mrs.
I would like to know the Juntion Temperature of the TMS320C6203B DSP. In the datasheet is only available the operating case temperature:
Thanks in advance,
Best regards.
Carlos Antón.
The only temperature related information available is detailed in the datasheet. Can you details why Tc is not sufficient?
--Paul
Hello Paul, we need the maximun junction temperature in order to do some thermal stress analisys. We have to ensure that the Tj<Tjmax of the component. Should we regard Tc as Tjmax?
Carlos
Thanks for the detail. I'm checking to see if it is possible to obtain the Tj information you need. However, as noted earlier, there may be no additional information available other than what is already in the datasheet.
--Paul
Carlos
Please refer to the following thread: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/985642/tms320vc5510a-max-junction-temperature/3642354?tisearch=e2e-sitesearch&keymatch=Tcase%20mukul#3642354
From the thread:
Case to Junction calculations/estimations guidance provided in the following application note
http://www.ti.com/lit/an/sprabi3b/sprabi3b.pdf
--Paul