Hi,
On CCS 12.2 : After target conf > Launch > M3 init OK > R5_0_0 Connect > Script DDR init OK.
I tried & failed to any binary (hello world, empty ...) from the SDK mcu_plus_sdk_am64x_08_05_00_24.
The error :
MAIN_Cortex_R5_0_0: Trouble Writing Memory Block at 0x0 on Page 0 of Length 0x40: (Error -1065 @ 0x40) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.10.0.00080)
MAIN_Cortex_R5_0_0: File Loader: Verification failed: Target failed to write 0x00000000
MAIN_Cortex_R5_0_0: GEL: File: C:\Users\a0489623\Documents\workspaceTrixell\hello_world_am64x-evm_r5fss0-0_freertos_ti-arm-clang\Debug\hello_world_am64x-evm_r5fss0-0_freertos_ti-arm-clang.out: Load failed.
What is the problem ?
Regards
Geoffrey