Other Parts Discussed in Thread: SYSCONFIG
Hi TI,
We are trying to bring up the debug UART Interface(MAIN_UART0) on our Custom Board. We don't have SD Card Slot to load the Images. We try to Load the Images
using UART/USB DFU Method. The steps we followed to test UART Boot mode is listed below:
1. Boot Mode Pins are configured to UART Boot.
2. Connected a TTL Converter to connect the UART (RX,TX) to the Host System.
3. After turning ON the Board, I can able to see some Data on the Debug Terminal(/dev/ttyUSB0), but when i try to transfer
tiboot3.bin image using x-modem, I receive an NACK and Transfer Incomplete as response.
I have tried this on the Am62x-SK Board(E2 Version), it was successfully Booted.
I have also attached the Image for your reference. Kindly let us know how to proceed on this.
Regards,
Murali Chikkanna