This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7: BOOTMODE Using VCC1V8_SYS PU

Part Number: AM62A7

Hi 

Because I need to set the VDDSHV3 to 1.8V power rails to use 1.8V level GPIO or I2C in GPMC0.

 I change the VDDSHV3 power source from SoC_DVDD3V3 to SOC_DVDD1V8, 

and the bootmode pull-up power is changed to VCC1V8_SYS;

Could please help me to check if any issues about boot or others .

and because the output level of  VSEL_SD_SOC will be 1.8V, so I need to find a 3.3V GPIO instead the origional port.

Thanks