This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
We are using crystal input of 32.768KHz to the wake-up osc pins of AM625x. However, when we are trying to measure the clock frequency, we are not seeing any waveform.
We have enabled those pins in the sysconfig which are related to wakeup clock. Please let us know why we are not able to see any clk signal when we measure.
Schematics:
sysconfig:
Hi Premalatha,
Thank you for your query.
I have taken your inputs and working on it. Please allow some time to revert back.
Regards,
Tushar
Hi Premalatha,
Can you please confirm how you are checking the crystal oscillator waveform?
Typically, the output of a crystal oscillator should be a sine wave with low amplitude, and low capacitance probes should be needed when you want to measure it.
My suggestion is that instead of checking at the input side, you can check at the output side, like this crystal input is going to the different modules as timers, UART,I2C and other peripherals. Simply toggle a pin in Tmer IRQ and see exactly whether the timer is Running at your initialized frequency or not.
This is one of the approaches, and I need to check if any other pins are there to monitor the CPU clocks.
Regards,
S.Anil.
Hi Anil,
We verified this wake up clock of 32.768khz in the evaluation board and observed the below ,
However, in our design we are not able to see any clock. There isn't any issue with the crystal as the same part number crystal is used in another circuit in our design where it is working.
Hello Premalatha,
I am routing your question to HW expert to comment on the above issue.
Regards,
S.Anil.
I would like to confirm the waveform you show in the oscilloscope capture represents the oscillation of the 32.768kHz crystal circuit. If so, it appears software has enabled the oscillator and it is working as expected.
The next thing to check is the path through the device. I recommend using the clock tree tool to understand the various clock path options and make sure you have selected the appropriate path.
Regards,
Paul