This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are using custom board based on AM62A7 CPU with emmc boot mode(0x1001) for booting
When board is powered on board boots properly from emmc but when we do a warm reset in Uboot/ kernel
board hangs and doesnot reboot
We referred below link and programmed eMMC HW reset enable OTP in 1 board and checked SW reboot worked
Also we tested other boot modes in our board like USB host, USB DFU, eMMC UDA File system mode, In other boot modes board is rebooting properly during SW reboot.
we wanted to know why programming this OTP is required for SW reboot in emmc boot mode?
Hi Vinay,
I have assigned your query to our expert. As he is currently on a customer visit, the response would be delayed.
Best Regards,
Suren
Hello Vinay,
Please refer to eMMC device specification as quoted below
e2e.ti.com/.../4395412
>>>>
Micron eMMC datasheet [https://www.mouser.com/datasheet/2/671/micron_technology_mict-s-a0006806196-1-1759129.pdf]
• RST_n: The RST_n signal is used by the host for resetting the device, moving the device to the pre-idle state.
• By default, the RST_n signal is temporarily disabled in the device.
• The host must set ECSD register byte 162, bits[1:0] to 0x1 to enable this functionality before the host can use it.
<<<<
Best,
-Hong
Hi,
If RST_n signal is required then our doubt is why SW reset is working when testing with eMMC UDA file system mode.
and issue is seen only in eMMC boot mode.
Hello Vinay,
From eMMC spec, "The RST_n signal is used by the host for resetting the device."
My understanding this would apply to booting from eMMC boot partition as well as UDA.
Best,
-Hong
Hi Hong,
Currently if EMMC HW reset enable is not programmed we are facing below issues in eMMC boot
1. SW reboot is not working
2. after pressing HW reset button board hangs and does not reboot
We dont want to program the ECSD register byte 162 in eMMC since it is OTP.
Is there any other way/workaround to resolve the above mentioned issues?
• By default, the RST_n signal is temporarily disabled in the device.
• The host must set ECSD register byte 162, bits[1:0] to 0x1 to enable this functionality before the host can use it.
Once ECSD register byte 162 is set, on AM62A-SK, eMMC boot works as expected from either pressing HW RESET button or issuing SW WarmReset, for example, via "reset" from u-boot or "reboot" from kernel.
Best,
-Hong