This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi expert,
I have these 4 questions on AM623 for HMI using:
1. Whether it supports RGB 24-bit display, similar to the controller with 24-bit RGB output like AM335x?
2. Whether it supports resistor 4-wire touch
3. Whether support RTC
4. Can AM623 connect to DDR3L?
Many thanks,
Joyce
Hello Jpyce,
Thank you for the query.
1. Whether it supports RGB 24-bit display, similar to the controller with 24-bit RGB output like AM335x?
24-bit is supported. The connections will change compared to AM335x.
2. Whether it supports resistor 4-wire touch
Support similar to AM335x is not available internal to the device.
3. Whether support RTC
There is an RTC module but does not provide RTC power pins similar to AM335x.
4. Can AM623 connect to DDR3L?
DDR3L is not supported.
Regards,
Sreenivasa