This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6655: TIMI/TIMO - GPIO unused pins

Part Number: TMS320C6655

Hello,

Could you please let me know if I can leave these GPIOs pins floated if I'm not using them?

I didn't find any direct answer for this question at HW design guide for Keystone devices document

  • These signals have internal pulls as defined here:

    From a reliability perspective (assuming no other pulls that conflict) the pins will be held at a valid logic level with the internal pull.   

    If you're ok with the resulting functionality, then no need to pull them externally.

    E.g., GPIO16 functions as a bootmode pin, and configures PCIE as enabled (pull high) or disabled (IPD pulls low by default).  

    Regards,

    Kyle