This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5718: low singnal on PORZ can't restart the linux in am5718 plat

Part Number: AM5718
Other Parts Discussed in Thread: SYSCONFIG

HI,

I designed the circuit using AM5718 and expect to reset the system using the reset button,the system is linux4.9 which is from the givened SDK: ti-processor-sdk-linux-am57xx-evm-04.03.00.05-Linux-x86-Install.bin;

After the system was running normally, I gave the PORZ pin a low level of approximately 300ms, but the system crashed and did not restart u boot and start Linux.

I would like to ask where the problem lies? How to solve this problem? Kindly help me out on this issue.

Thanks and Best Regards