This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
I designed the circuit using AM5718 and expect to reset the system using the reset button,the system is linux4.9 which is from the givened SDK: ti-processor-sdk-linux-am57xx-evm-04.03.00.05-Linux-x86-Install.bin;
After the system was running normally, I gave the PORZ pin a low level of approximately 300ms, but the system crashed and did not restart u boot and start Linux.
and When I press the reset button, there is no printout, the board crashes, and I need to power off and restart to work again。
I am currently booting from an SD card.
The SYSCONFIG signal will be used as a GPMC part pin after startup.
My board does not have JTAG function.
Isn't it possible to directly reset the reset pin by introducing a low level for a period of time, lasting for 300ms long enough?
I would like to ask where the problem lies? How to solve this problem? Kindly help me out on this issue.
Thanks and Best Regards
Hi,
The assigned engineer is OoO for Thanksgiving holidays, please expect delay in response.
Apologies for the inconvenience and thank you for your patience.
Regards,
Parth
Hello Jiablin,
I believe this is a continuation from this thread: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1278293/am5718-low-singnal-on-porz-can-t-restart-the-linux-in-am5718-plat
Can you confirm?
-Josue
Hi Josue Zamitiz-Ayala,
thank you for your reply.
It's the same one. After asking the question earlier, due to a period of closure, I couldn't reply in a timely manner. When I came back, I found that I couldn't reply anymore. So, I start a new one.
Ok, I can unlock that thread and lets continue the conversation there.
Closing this one.
-Josue