Other Parts Discussed in Thread: SYSBIOS,
Hi everyone,
I am facing a problem in debugging basic bare-metal example on Cortex-R5F core (MCU1_0) of AM65xx IDK board. My environment setup consists of:
- Code Composer Studio v12.40
- AM65xx IDK board
- pdk_am65xx_08_02_00_21 installed on Windows 11
- Compiler TI v20.2.7.LTS
Following the ARM Cortex-R5 bare metal example guide (section 9.9.6. "ARM Cortex-R5"), these compiling warnings are produced:
Launching debugger with AM65xx IDK target configuration and loading .out file as described by the guide, it happens this:
It seems that the program loading into memory fails, maybe because of a linking error. Analyzing the linker script "linker_r5.lds" provided in "PDK INSTALL PATH)/packages/ti/build/am65xx/" folder, I see that MCU_ARMSS0_CORE0_ATCM memory start address is 0x00, while on chapter 2.2 of Technical Reference Manual it is 0x0041000000. Which is the correct one? How it is possible to fix this debug issue?
Thank you in advance for your help.