This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI Support !
We wanted to build a remote device environment and power the SK-TDA4VM through a programmable power supply(Keysight E3648A, Setting to 5V=3A), but we found that the development board could not start and kept restarting. The log and hardware connections are as follows: How should we set up this HW environment?
U-Boot SPL 2023.04-gbd74e615a6 (Sep 06 2023 - 10:09:25 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Loading Environment from nowhere... OK Starting ATF on ARM64 core... NOTICE: BL31: v2.9(release):v2.9.0-dirty NOTICE: BL31: Built : 14:12:59, May 22 2023 I/TC: I/TC: OP-TEE version: 3.20.0 (gcc version 11.3.0 (GCC)) #1 Fri Jan 20 15:42:54 UTC 2023 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html I/TC: Primary CPU initializing I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') I/TC: HUK Initialized U-Boot SPL 2023.04-gbd74e615a6 (Sep 06 2023 - 10:09:25 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Loading Environment from nowhere... OK Starting ATF on ARM64 core... NOTICE: BL31: v2.9(release):v2.9.0-dirty NOTICE: BL31: Built : 14:12:59, May 22 2023 I/TC: I/TC: OP-TEE version: 3.20.0 (gcc version 11.3.0 (GCC)) #1 Fri Jan 20 15:42:54 UTC 2023 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html I/TC: Primary CPU initializing I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Fixing SA2UL firewall owner for GP device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot U-Boot SPL 2023.04-gbd74e615a6 (Sep 06 2023 - 10:09:25 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d U-Boot 2023.04-gbd74e615a6 (Sep 06 2023 - 10:09:25 +0000) SoC: J721E SR1.1 GP Model: Texas Instruments J721E SK A72 Board: J721EX-EAIK rev A1 DRAM: 4 GiB Core: 120 devices, 33 uclasses, devicetree: separate Flash: 0 Bytes MMC: mmc@4fb0000: 1 Loading Environment from nowhere... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000 Net: eth0: ethernet@46000000port@1 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 Failed to load 'boot.scr' 1440 bytes read in 25 ms (55.7 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... 1 bytes read in 24 ms (0 Bytes/s) Already setup. k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work k3_r5f_rproc r5f@41400000: Core 2 is already in use. No rproc commands work 490924 bytes read in 38 ms (12.3 MiB/s) Load Remote Processor 2 with data@addr=0x82000000 490924 bytes: Success! 371772 bytes read in 36 ms (9.8 MiB/s) Load Remote Processor 3 with data@addr=0x82000000 371772 bytes: Success! Failed to load '/lib/firmware/j7-main-r5f1_0-fw' Failed to load '/lib/firmware/j7-main-r5f1_1-fw' 994096 bytes read in 49 ms (19.3 MiB/s) U-Boot SPL 2023.04-gbd74e615a6 (Sep 06 2023 - 10:09:25 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Loading Environment from nowhere... OK Starting ATF on ARM64 core... NOTICE: BL31: v2.9(release):v2.9.0-dirty NOTICE: BL31: Built : 14:12:59, May 22 2023 I/TC: I/TC: OP-TEE version: 3.20.0 (gcc version 11.3.0 (GCC)) #1 Fri Jan 20 15:42:54 UTC 2023 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html I/TC: Primary CPU initializing I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Fixing SA2UL firewall owner for GP device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot U-Boot SPL 2023.04-gbd74e615a6 (Sep 06 2023 - 10:09:25 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d U-Boot SPL 2023.04-gbd74e615a6 (Sep 06 2023 - 10:09:25 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Loading Environment from nowhere... OK Starting ATF on ARM64 core... NOTICE: BL31: v2.9(release):v2.9.0-dirty NOTICE: BL31: Built : 14:12:59, May 22 2023 I/TC: I/TC: OP-TEE version: 3.20.0 (gcc version 11.3.0 (GCC)) #1 Fri Jan 20 15:42:54 UTC 2023 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html I/TC: Primary CPU initializing I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Fixing SA2UL firewall owner for GP device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot U-Boot SPL 2023.04-gbd74e615a6 (Sep 06 2023 - 10:09:25 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d U-Boot 2023.04-gbd74e615a6 (Sep 06 2023 - 10:09:25 +0000) SoC: J721E SR1.1 GP Model: Texas Instruments J721E SK A72 Board: J721EX-EAIK rev A1 DRAM: 4 GiB Core: 120 devices, 33 uclasses, devicetree: separate Flash: 0 Bytes MMC: mmc@4fb0000: 1 Loading Environment from nowhere... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000 Net: eth0: ethernet@46000000port@1 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 Failed to load 'boot.scr' 1440 bytes read in 26 ms (53.7 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... 1 bytes read in 24 ms (0 Bytes/s) Already setup. k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work k3_r5f_rproc r5f@41400000: Core 2 is already in use. No rproc commands work 490924 bytes read in 38 ms (12.3 MiB/s) Load Remote Processor 2 with data@addr=0x82000000 490924 bytes: Success! 371772 bytes read in 36 ms (9.8 MiB/s) Load Remote Processor 3 with data@addr=0x82000000 371772 bytes: Success! Failed to load '/lib/firmware/j7-main-r5f1_0-fw' Failed to load '/lib/firmware/j7-main-r5f1_1-fw' 994096 bytes read in 49 ms (19.3 MiB/s) U-Boot SPL 2023.04-gbd74e615a6 (Sep 06 2023 - 10:09:25 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image d Loading Environment from nowhere... OK Starting ATF on ARM64 core... NOTICE: BL31: v2.9(release):v2.9.0-dirty NOTICE: BL31: Built : 14:12:59, May 22 2023 I/TC: I/TC: OP-TEE version: 3.20.0 (gcc version 11.3.0 (GCC)) #1 Fri Jan 20 15:42:54 UTC 2023 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html I/TC: Primary CPU initializing I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Fixing SA2UL firewall owner for GP device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot
What is the total "Watts" power you supplied ?
Because, the tda4VM-SK board requires "60W of power (20VDC at 3A)". The minimum supply required is 15W supply (5VDC at 3A). However, a 5 V supply may limit available processing with TDA4VM as well as limit some of the available peripherals
---
I understand that you are planning for a remote environment.
But however for other users, we can order the power supply adaptors from the recommended manufacturers given below:
--
Please refer this user guide:- page no: 5 - https://www.ti.com/lit/ug/spruj21c/spruj21c.pdf
Regards
Shankari G
Yes, we have purchased the QADC-65-20-08CB and it does boot. But we still want to use a programmable power supply to build a remote environment, and we tried 5VDC==3A/5VDC==5A/20VDC==3A/20VDC==5A but it couldn't start normally. Is there any way to solve this problem?
Daiwang,
Your query will get notified to hardware engineers.
Thanks for your patience.
Regards
Shankari G
Yes, we have purchased the QADC-65-20-08CB and it does boot.
You said, it boots with " QADC-65-20-08CB"....
Meanwhile, would you post your successful boot logs when you used " QADC-65-20-08CB", power supply adaptor.
Regards
Shankari G
The board did not boot with 20V/3A supply connected? The board is designed to work with a USB-C supply. You are providing voltage, but may not be sufficient for the USB controller to enable the on-board supplies. Can you measure on-board supplies to see if USB controller is enabling power? Maybe measure power net VMAIN - it should have the same voltage (or near same) as the supplied VBUS. Or you can measure any of the other on-board regulators.
Yes, Normal boot log (use QADC-65-20-08CB) as follow:
U-Boot SPL 2023.04-gbd74e615a6 (Sep 06 2023 - 10:09:25 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Loading Environment from nowhere... OK Starting ATF on ARM64 core... NOTICE: BL31: v2.9(release):v2.9.0-dirty NOTICE: BL31: Built : 14:12:59, May 22 2023 I/TC: I/TC: OP-TEE version: 3.20.0 (gcc version 11.3.0 (GCC)) #1 Fri Jan 20 15:42:54 UTC 2023 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html I/TC: Primary CPU initializing I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Fixing SA2UL firewall owner for GP device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot U-Boot SPL 2023.04-gbd74e615a6 (Sep 06 2023 - 10:09:25 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if th e image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if th e image was also encrypted U-Boot 2023.04-gbd74e615a6 (Sep 06 2023 - 10:09:25 +0000) SoC: J721E SR1.1 GP Model: Texas Instruments J721E SK A72 Board: J721EX-EAIK rev A1 DRAM: 4 GiB Core: 120 devices, 33 uclasses, devicetree: separate Flash: 0 Bytes MMC: mmc@4fb0000: 1 Loading Environment from nowhere... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1 000000 Net: eth0: ethernet@46000000port@1 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 Failed to load 'boot.scr' 1520 bytes read in 25 ms (58.6 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... 1 bytes read in 25 ms (0 Bytes/s) Already setup. k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work k3_r5f_rproc r5f@41400000: Core 2 is already in use. No rproc commands work 490924 bytes read in 38 ms (12.3 MiB/s) Load Remote Processor 2 with data@addr=0x82000000 490924 bytes: Success! 371772 bytes read in 36 ms (9.8 MiB/s) Load Remote Processor 3 with data@addr=0x82000000 371772 bytes: Success! Failed to load '/lib/firmware/j7-main-r5f1_0-fw' Failed to load '/lib/firmware/j7-main-r5f1_1-fw' 994096 bytes read in 48 ms (19.8 MiB/s) Load Remote Processor 6 with data@addr=0x82000000 994096 bytes: Success! 994096 bytes read in 49 ms (19.3 MiB/s) Load Remote Processor 7 with data@addr=0x82000000 994096 bytes: Success! 12968080 bytes read in 124 ms (99.7 MiB/s) Load Remote Processor 8 with data@addr=0x82000000 12968080 bytes: Success! 20920832 bytes read in 446 ms (44.7 MiB/s) 102536 bytes read in 30 ms (3.3 MiB/s) Working FDT set to 88000000 10434 bytes read in 28 ms (363.3 KiB/s) 4216 bytes read in 28 ms (146.5 KiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Working FDT set to 88000000 ERROR: reserving fdt memory region failed (addr=880000000 size=27000000 flags=4) Loading Device Tree to 000000008fee3000, end 000000008fffffff ... OK Working FDT set to 8fee3000 Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080] [ 0.000000] Linux version 6.1.46-gf8110d9ce8 (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 11.3.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Mon Sep 4 04:45:34 UTC 2023 [ 0.000000] Machine model: Texas Instruments J721E SK [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created CMA memory pool at 0x00000008e0000000, size 512 MiB [ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a0000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a0100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a1000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a1100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a2000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 31 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a2100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a4000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 31 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a4100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a6000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a6100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a7000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a7100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-c66-dma-memory@a8000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-c66-memory@a8100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-c66-dma-memory@a9000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-c66-memory@a9100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000ac000000, size 96 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-dma-memory@ac000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b2000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-c71-dma-memory@b2000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b2100000, size 95 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-c71-memory@b2100000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: initialized node vision_apps_shared-memories, compatible id dma-heap-carveout [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000d8000000, size 192 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-lo@d8000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000e4000000, size 8 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-virtual-eth-queues@e4000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000e4800000, size 24 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-virtual-eth-buffers@e4800000, compatible id shared-dma-poo l [ 0.000000] Reserved memory: created DMA memory pool at 0x0000000880000000, size 624 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-hi@880000000, compatible id shared-dma-pool [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal [mem 0x0000000100000000-0x00000008ffffffff] [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff] [ 0.000000] node 0: [mem 0x000000009e800000-0x00000000b7ffffff] [ 0.000000] node 0: [mem 0x00000000b8000000-0x00000000d7ffffff] [ 0.000000] node 0: [mem 0x00000000d8000000-0x00000000e5ffffff] [ 0.000000] node 0: [mem 0x00000000e6000000-0x00000000ffffffff] [ 0.000000] node 0: [mem 0x0000000880000000-0x00000008a6ffffff] [ 0.000000] node 0: [mem 0x00000008a7000000-0x00000008ffffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff] [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.2 [ 0.000000] percpu: Embedded 19 pages/cpu s38376 r8192 d31256 u77824 [ 0.000000] Detected PIPT I-cache on CPU0 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] CPU features: detected: Spectre-v3a [ 0.000000] CPU features: detected: Spectre-BHB [ 0.000000] CPU features: detected: ARM erratum 1742098 [ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923 [ 0.000000] alternatives: applying boot alternatives [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1032192 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 systemd.hostname=tda4vm-sk ro ot=PARTUUID=73d5eb3e-02 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear) [ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] software IO TLB: area num 2. [ 0.000000] software IO TLB: mapped [mem 0x00000000fbfff000-0x00000000fffff000] (64MB) [ 0.000000] Memory: 1694156K/4194304K available (12480K kernel code, 1294K rwdata, 4360K rodata, 2176K init, 498K bss, 19 75860K reserved, 524288K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] Tracing variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 960 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] Root IRQ handler: gic_handle_irq [ 0.000000] GICv3: GICv3 features: 16 PPIs [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000 [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19 [ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @8a7800000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GICv3: using LPI property table @0x00000008a7030000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000008a7040000 [ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention. [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000000] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.008402] Console: colour dummy device 80x25 [ 0.012965] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.023635] pid_max: default: 32768 minimum: 301 [ 0.028374] LSM: Security Framework initializing [ 0.033159] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.040736] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.049599] cblist_init_generic: Setting adjustable number of callback queues. [ 0.057005] cblist_init_generic: Setting shift to 1 and lim to 1. [ 0.063265] cblist_init_generic: Setting adjustable number of callback queues. [ 0.070650] cblist_init_generic: Setting shift to 1 and lim to 1. [ 0.076959] rcu: Hierarchical SRCU implementation. [ 0.081855] rcu: Max phase no-delay instances is 1000. [ 0.087356] Platform MSI: msi-controller@1820000 domain created [ 0.093651] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created [ 0.103445] EFI services will not be available. [ 0.108191] smp: Bringing up secondary CPUs ... I/TC: Secondary CPU 1 initializing I/TC: Secondary CPU 1 switching to normal world boot [ 0.121475] Detected PIPT I-cache on CPU1 [ 0.121536] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000 [ 0.121548] GICv3: CPU1: using allocated LPI pending table @0x00000008a7050000 [ 0.121581] CPU1: Booted secondary processor 0x0000000001 [0x411fd080] [ 0.121633] smp: Brought up 1 node, 2 CPUs [ 0.150977] SMP: Total of 2 processors activated. [ 0.155782] CPU features: detected: 32-bit EL0 Support [ 0.161036] CPU features: detected: CRC32 instructions [ 0.166314] CPU: All CPU(s) started at EL2 [ 0.170495] alternatives: applying system-wide alternatives [ 0.177146] devtmpfs: initialized [ 0.187368] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.197359] futex hash table entries: 512 (order: 3, 32768 bytes, linear) [ 0.212828] pinctrl core: initialized pinctrl subsystem [ 0.218556] DMI not present or invalid. [ 0.222822] NET: Registered PF_NETLINK/PF_ROUTE protocol family [ 0.229531] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations [ 0.236852] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.244860] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.252985] audit: initializing netlink subsys (disabled) [ 0.258608] audit: type=2000 audit(0.168:1): state=initialized audit_enabled=0 res=1 [ 0.258854] thermal_sys: Registered thermal governor 'step_wise' [ 0.266530] thermal_sys: Registered thermal governor 'power_allocator' [ 0.272749] cpuidle: using governor menu [ 0.283509] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.290482] ASID allocator initialised with 65536 entries [ 0.304250] platform a000000.dp-bridge: Fixed dependency cycle(s) with /bus@100000/dss@4a00000 [ 0.314708] platform a000000.dp-bridge: Fixed dependency cycle(s) with /connector [ 0.322624] platform hdmi-connector: Fixed dependency cycle(s) with /dvi-bridge [ 0.330122] platform 4a00000.dss: Fixed dependency cycle(s) with /dvi-bridge [ 0.337556] KASLR disabled due to lack of seed [ 0.345162] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages [ 0.352107] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page [ 0.358510] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages [ 0.365444] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page [ 0.371845] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages [ 0.378778] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page [ 0.385180] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages [ 0.392113] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page [ 0.399445] k3-chipinfo 43000014.chipid: Family:J721E rev:SR2.0 JTAGID[0x1bb6402f] Detected [ 0.408554] iommu: Default domain type: Translated [ 0.413540] iommu: DMA domain TLB invalidation policy: strict mode [ 0.420065] SCSI subsystem initialized [ 0.424067] usbcore: registered new interface driver usbfs [ 0.429687] usbcore: registered new interface driver hub [ 0.435123] usbcore: registered new device driver usb [ 0.440547] pps_core: LinuxPPS API ver. 1 registered [ 0.445619] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.454957] PTP clock support registered [ 0.459037] EDAC MC: Ver: 3.0.0 [ 0.462776] FPGA manager framework [ 0.466289] Advanced Linux Sound Architecture Driver Initialized. [ 0.472926] clocksource: Switched to clocksource arch_sys_counter [ 0.479267] VFS: Disk quotas dquot_6.6.0 [ 0.483300] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 0.493328] Carveout Heap: Exported 512 MiB at 0x00000000b8000000 [ 0.499636] NET: Registered PF_INET protocol family [ 0.504833] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear) [ 0.513850] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear) [ 0.522624] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear) [ 0.530550] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear) [ 0.538762] TCP bind hash table entries: 32768 (order: 8, 1048576 bytes, linear) [ 0.547475] TCP: Hash tables configured (established 32768 bind 32768) [ 0.554298] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear) [ 0.561213] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear) [ 0.568675] NET: Registered PF_UNIX/PF_LOCAL protocol family [ 0.574801] RPC: Registered named UNIX socket transport module. [ 0.580861] RPC: Registered udp transport module. [ 0.585664] RPC: Registered tcp transport module. [ 0.590467] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.597058] NET: Registered PF_XDP protocol family [ 0.601959] PCI: CLS 0 bytes, default 64 [ 0.606383] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available [ 0.615547] Initialise system trusted keyrings [ 0.620215] workingset: timestamp_bits=46 max_order=20 bucket_order=0 [ 0.629451] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.635762] NFS: Registering the id_resolver key type [ 0.640956] Key type id_resolver registered [ 0.645228] Key type id_legacy registered [ 0.649359] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.656207] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 0.663861] 9p: Installing v9fs 9p2000 file system support [ 0.688800] Key type asymmetric registered [ 0.692983] Asymmetric key parser 'x509' registered [ 0.697987] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 0.705636] io scheduler mq-deadline registered [ 0.710280] io scheduler kyber registered [ 0.716431] pinctrl-single 4301c000.pinctrl: 94 pins, size 376 [ 0.722673] pinctrl-single 11c000.pinctrl: 173 pins, size 692 [ 0.732708] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled [ 0.740356] arm-smmu-v3 36600000.iommu: ias 48-bit, oas 48-bit (features 0x00001faf) [ 0.748583] arm-smmu-v3 36600000.iommu: allocated 65536 entries for cmdq [ 0.755743] arm-smmu-v3 36600000.iommu: allocated 32768 entries for evtq [ 0.763797] arm-smmu-v3 36600000.iommu: msi_domain absent - falling back to wired irqs [ 0.774919] loop: module loaded [ 0.778942] megasas: 07.719.03.00-rc1 [ 0.784772] tun: Universal TUN/TAP device driver, 1.6 [ 0.790302] thunder_xcv, ver 1.0 [ 0.793617] thunder_bgx, ver 1.0 [ 0.796925] nicpf, ver 1.0 [ 0.799920] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version [ 0.807302] hns3: Copyright (c) 2017 Huawei Corporation. [ 0.812752] hclge is initializing [ 0.816151] e1000: Intel(R) PRO/1000 Network Driver [ 0.821135] e1000: Copyright (c) 1999-2006 Intel Corporation. [ 0.827023] e1000e: Intel(R) PRO/1000 Network Driver [ 0.832093] e1000e: Copyright(c) 1999 - 2015 Intel Corporation. [ 0.838152] igb: Intel(R) Gigabit Ethernet Network Driver [ 0.843666] igb: Copyright (c) 2007-2014 Intel Corporation. [ 0.849369] igbvf: Intel(R) Gigabit Virtual Function Network Driver [ 0.855771] igbvf: Copyright (c) 2009 - 2012 Intel Corporation. [ 0.861884] sky2: driver version 1.30 [ 0.866018] VFIO - User Level meta-driver version: 0.3 [ 0.871647] usbcore: registered new interface driver usb-storage [ 0.878212] i2c_dev: i2c /dev entries driver [ 0.883532] sdhci: Secure Digital Host Controller Interface driver [ 0.889857] sdhci: Copyright(c) Pierre Ossman [ 0.894550] Synopsys Designware Multimedia Card Interface Driver [ 0.900933] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.907218] ledtrig-cpu: registered to indicate activity on CPUs [ 0.913455] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... [ 0.920177] usbcore: registered new interface driver usbhid [ 0.925871] usbhid: USB HID core driver [ 0.930517] optee: probing for conduit method. I/TC: Reserved shared memory is enabled I/TC: Dynamic shared memory is enabled I/TC: Normal World virtualization support is disabled I/TC: Asynchronous notifications are disabled [ 0.935075] optee: revision 3.20 (8e74d476) [ 0.951491] optee: dynamic shared memory is enabled [ 0.960975] optee: initialized driver [ 0.966036] Initializing XFRM netlink socket [ 0.970426] NET: Registered PF_PACKET protocol family [ 0.975652] 9pnet: Installing 9P2000 support [ 0.980073] Key type dns_resolver registered [ 0.984641] registered taskstats version 1 [ 0.988837] Loading compiled-in X.509 certificates [ 0.998777] ti-sci 44083000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)') [ 1.046140] omap_i2c 42120000.i2c: bus 0 rev0.12 at 100 kHz [ 1.073082] i2c i2c-1: Added multiplexed i2c bus 2 [ 1.078067] i2c i2c-1: Added multiplexed i2c bus 3 [ 1.082966] pca954x 1-0071: registered 2 multiplexed busses for I2C switch pca9543 [ 1.090725] omap_i2c 2000000.i2c: bus 1 rev0.12 at 400 kHz [ 1.096743] omap_i2c 2010000.i2c: bus 4 rev0.12 at 100 kHz [ 1.125130] i2c 6-0010: Fixed dependency cycle(s) with /bus@100000/ticsi2rx@4500000/csi-bridge@4504000 [ 1.134746] i2c i2c-5: Added multiplexed i2c bus 6 [ 1.139766] i2c 7-0010: Fixed dependency cycle(s) with /bus@100000/ticsi2rx@4510000/csi-bridge@4514000 [ 1.149368] i2c i2c-5: Added multiplexed i2c bus 7 [ 1.154264] pca954x 5-0070: registered 2 multiplexed busses for I2C switch pca9543 [ 1.162074] i2c i2c-5: Failed to register i2c client pca9543 at 0x70 (-16) [ 1.169102] i2c i2c-5: of_i2c: Failure registering /bus@100000/i2c@2030000/i2c-mux@70 [ 1.177107] i2c i2c-5: Failed to create I2C device for /bus@100000/i2c@2030000/i2c-mux@70 [ 1.185476] omap_i2c 2030000.i2c: bus 5 rev0.12 at 400 kHz [ 1.191560] omap_i2c 2050000.i2c: bus 8 rev0.12 at 400 kHz [ 1.197385] ti-sci-intr 42200000.interrupt-controller: Interrupt Router 137 domain created [ 1.205956] ti-sci-intr bus@100000:interrupt-controller@a00000: Interrupt Router 131 domain created [ 1.215313] ti-sci-intr 310e0000.interrupt-controller: Interrupt Router 213 domain created [ 1.223941] ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 209 created [ 1.241140] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235 [ 1.251024] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled [ 1.257787] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66346100, num_proxies:64 [ 1.266946] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[440,150] sci-dev-id:211 [ 1.277110] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled [ 1.283868] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66346100, num_proxies:64 [ 1.291860] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 193, base_baud = 6000000) is a 8250 [ 1.301394] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 194, base_baud = 3000000) is a 8250 [ 1.310254] printk: console [ttyS2] enabled [ 1.310254] printk: console [ttyS2] enabled [ 1.318699] printk: bootconsole [ns16550a0] disabled [ 1.318699] printk: bootconsole [ns16550a0] disabled [ 1.329166] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 195, base_baud = 3000000) is a 8250 [ 1.339366] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode [ 1.384930] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 1.393406] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867 [ 1.401679] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Por ts: 2 quirks:00000000 [ 1.414496] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4 [ 1.421703] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64 [ 1.428014] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010a, freq:500000000, add_val:1 pps:0 [ 1.438464] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010a, freq:200000000, add_val:4 pps:0 [ 1.550727] gpio-388 (CSI_MUX_SEL_2): hogged as output/high [ 1.559439] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100 [ 1.566307] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100 [ 1.573129] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fc7100 [ 1.579949] omap-mailbox 31f83000.mailbox: omap mailbox rev 0x66fc7100 [ 1.586738] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fc7100 [ 1.601041] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan: 13, gp-rflow: 8) [ 1.611794] ti-udma 31150000.dma-controller: Channels: 122 (tchan: 61, rchan: 61, gp-rflow: 16) [ 1.626707] spi-nor spi0.0: s28hs512t (65536 Kbytes) [ 1.631747] 8 fixed-partitions partitions found on MTD device 47040000.spi.0 [ 1.638783] Creating 8 MTD partitions on "47040000.spi.0": [ 1.644256] 0x000000000000-0x000000080000 : "ospi.tiboot3" [ 1.650324] 0x000000080000-0x000000280000 : "ospi.tispl" [ 1.656076] 0x000000280000-0x000000680000 : "ospi.u-boot" [ 1.661915] 0x000000680000-0x0000006c0000 : "ospi.env" [ 1.667478] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw" [ 1.673275] 0x0000007c0000-0x000000800000 : "ospi.env.backup" [ 1.679464] 0x000000800000-0x000003fc0000 : "ospi.rootfs" [ 1.685346] 0x000003fc0000-0x000004000000 : "ospi.phypattern" [ 1.695889] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode [ 1.740943] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 1.749401] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867 [ 1.757674] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Por ts: 2 quirks:00000000 [ 1.770483] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4 [ 1.777690] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64 [ 1.783958] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010a, freq:500000000, add_val:1 pps:0 [ 1.794575] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48 [ 1.803339] mmc1: CQHCI version 5.10 [ 1.820239] ALSA device list: [ 1.823219] No soundcards found. [ 1.847522] mmc1: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit [ 1.855121] Waiting for root device PARTUUID=73d5eb3e-02... [ 1.909350] mmc1: new ultra high speed DDR50 SDHC card at address aaaa [ 1.916317] mmcblk1: mmc1:aaaa SL32G 29.7 GiB [ 1.925344] mmcblk1: p1 p2 [ 1.959239] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Quota mode: none. [ 1.967792] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 1.977349] devtmpfs: mounted [ 1.981550] Freeing unused kernel memory: 2176K [ 1.986163] Run /sbin/init as init process [ 2.218433] systemd[1]: System time before build time, advancing clock. [ 2.265147] NET: Registered PF_INET6 protocol family [ 2.270670] Segment Routing with IPv6 [ 2.274354] In-situ OAM (IOAM) with IPv6 [ 2.305982] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYP T -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11 KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid) [ 2.337391] systemd[1]: Detected architecture arm64. Welcome to Arago 2023.04! [ 2.413050] systemd[1]: Hostname set to <tda4vm-sk>. [ 2.506542] systemd-sysv-generator[138]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. A utomatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust. [ 2.534066] systemd-sysv-generator[138]: SysV service '/etc/init.d/telnetd' lacks a native systemd unit file. Automatical ly generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make i t more safe and robust. [ 2.558150] systemd-sysv-generator[138]: SysV service '/etc/init.d/edgeai-launcher.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in orde r to make it more safe and robust. [ 2.582904] systemd-sysv-generator[138]: SysV service '/etc/init.d/netopeer2-server' lacks a native systemd unit file. Au tomatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust. [ 2.607494] systemd-sysv-generator[138]: SysV service '/etc/init.d/sysrepo' lacks a native systemd unit file. Automatical ly generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make i t more safe and robust. [ 2.766269] systemd[1]: /lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically u pdating to journal. Please update your unit file, and consider removing the setting altogether. [ 2.811564] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automaticall y updating to journal. Please update your unit file, and consider removing the setting altogether. [ 2.861698] systemd[1]: Queued start job for default target Graphical Interface. [ 2.898559] systemd[1]: Created slice Slice /system/getty. [ OK ] Created slice Slice /system/getty. [ 2.922392] systemd[1]: Created slice Slice /system/modprobe. [ OK ] Created slice Slice /system/modprobe. [ 2.946327] systemd[1]: Created slice Slice /system/serial-getty. [ OK ] Created slice Slice /system/serial-getty. [ 2.970045] systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. [ 2.993183] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Dispatch Password …ts to Console Directory Watch. [ 3.017074] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ OK ] Started Forward Password R…uests to Wall Directory Watch. [ 3.041124] systemd[1]: Reached target Path Units. [ OK ] Reached target Path Units. [ 3.060986] systemd[1]: Reached target Remote File Systems. [ OK ] Reached target Remote File Systems. [ 3.080985] systemd[1]: Reached target Slice Units. [ OK ] Reached target Slice Units. [ 3.100991] systemd[1]: Reached target Swaps. [ OK ] Reached target Swaps. [ 3.156013] systemd[1]: Listening on RPCbind Server Activation Socket. [ OK ] Listening on RPCbind Server Activation Socket. [ 3.177067] systemd[1]: Reached target RPC Port Mapper. [ OK ] Reached target RPC Port Mapper. [ 3.200218] systemd[1]: Listening on Process Core Dump Socket. [ OK ] Listening on Process Core Dump Socket. [ 3.221185] systemd[1]: Listening on initctl Compatibility Named Pipe. [ OK ] Listening on initctl Compatibility Named Pipe. [ 3.245350] systemd[1]: Listening on Journal Audit Socket. [ OK ] Listening on Journal Audit Socket. [ 3.265233] systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket (/dev/log). [ 3.285260] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Journal Socket. [ 3.305324] systemd[1]: Listening on Network Service Netlink Socket. [ OK ] Listening on Network Service Netlink Socket. [ 3.329301] systemd[1]: Listening on udev Control Socket. [ OK ] Listening on udev Control Socket. [ 3.349161] systemd[1]: Listening on udev Kernel Socket. [ OK ] Listening on udev Kernel Socket. [ 3.369209] systemd[1]: Listening on User Database Manager Socket. [ OK ] Listening on User Database Manager Socket. [ 3.409257] systemd[1]: Mounting Huge Pages File System... Mounting Huge Pages File System... [ 3.431794] systemd[1]: Mounting POSIX Message Queue File System... Mounting POSIX Message Queue File System... [ 3.473315] systemd[1]: Mounting Kernel Debug File System... Mounting Kernel Debug File System... [ 3.493204] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sy s/kernel/tracing). [ 3.511252] systemd[1]: Mounting Temporary Directory /tmp... Mounting Temporary Directory /tmp... [ 3.536290] systemd[1]: Starting Create List of Static Device Nodes... Starting Create List of Static Device Nodes... [ 3.559579] systemd[1]: Starting Load Kernel Module configfs... Starting Load Kernel Module configfs... [ 3.597398] systemd[1]: Starting Load Kernel Module drm... Starting Load Kernel Module drm... [ 3.619693] systemd[1]: Starting Load Kernel Module fuse... Starting Load Kernel Module fuse... [ 3.636765] fuse: init (API version 7.37) [ 3.652366] systemd[1]: Starting Start psplash boot splash screen... Starting Start psplash boot splash screen... [ 3.680825] systemd[1]: Starting RPC Bind... Starting RPC Bind... [ 3.697162] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIs ReadWrite=!/). [ 3.713364] systemd[1]: Starting Journal Service... Starting Journal Service... [ 3.758691] systemd[1]: Starting Load Kernel Modules... Starting Load Kernel Modules... [ 3.777314] cryptodev: loading out-of-tree module taints kernel. [ 3.787909] cryptodev: driver 1.12 loaded. [ 3.805461] systemd[1]: Starting Generate network units from Kernel command line... Starting Generate network …ts from Kernel command line... [ 3.836100] systemd[1]: Starting Remount Root and Kernel File Systems... Starting Remount Root and Kernel File Systems... [ 3.852131] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none. [ 3.861578] systemd[1]: Starting Coldplug All udev Devices... Starting Coldplug All udev Devices... [ 3.885764] systemd[1]: Started RPC Bind. [ OK ] Started RPC Bind. [ 3.909508] systemd[1]: Started Journal Service. [ OK ] Started Journal Service. [ OK ] Mounted Huge Pages File System. [ OK ] Mounted POSIX Message Queue File System. [ OK ] Mounted Kernel Debug File System. [ OK ] Mounted Temporary Directory /tmp. [ OK ] Finished Create List of Static Device Nodes. [ OK ] Finished Load Kernel Module configfs. [ OK ] Finished Load Kernel Module drm. [ OK ] Finished Load Kernel Module fuse. [FAILED] Failed to start Start psplash boot splash screen. See 'systemctl status psplash-start.service' for details. [DEPEND] Dependency failed for Star…progress communication helper. [ OK ] Finished Load Kernel Modules. [ OK ] Finished Generate network units from Kernel command line. [ OK ] Finished Remount Root and Kernel File Systems. Mounting FUSE Control File System... Mounting Kernel Configuration File System... Starting Flush Journal to Persistent Storage... Starting Apply Kernel Variables... [ 4.260084] systemd-journald[153]: Received client request to flush runtime journal. Starting Create Static Device Nodes in /dev... [ OK ] Mounted FUSE Control File System. [ OK ] Mounted Kernel Configuration File System. [ OK ] Finished Flush Journal to Persistent Storage. [ OK ] Finished Apply Kernel Variables. [ OK ] Finished Create Static Device Nodes in /dev. [ OK ] Reached target Preparation for Local File Systems. Mounting /media/ram... Mounting /var/volatile... [ 4.451392] audit: type=1334 audit(1651167747.232:2): prog-id=5 op=LOAD [ 4.458360] audit: type=1334 audit(1651167747.240:3): prog-id=6 op=LOAD Starting Rule-based Manage…for Device Events and Files... [ OK ] Finished Coldplug All udev Devices. [ OK ] Mounted /media/ram. [ OK ] Mounted /var/volatile. Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... [ OK ] Started Rule-based Manager for Device Events and Files. [ OK ] Finished Create Volatile Files and Directories. Starting Network Time Synchronization... Starting Record System Boot/Shutdown in UTMP... [ OK ] Finished Record System Boot/Shutdown in UTMP. [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Initialization. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target System Time Set. [ OK ] Started Daily rotation of log files. [ 4.997152] random: crng init done [ OK ] Reached target Timer Units. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ 5.030192] mc: Linux media interface: v0.10 [ OK ] Listening on D-Bus System Message Bus Socket. Starting Docker Socket for the API...[ 5.060595] videodev: Linux video capture interface: v2.00 [ 5.083964] j721e-pcie-host 2900000.pcie: host bridge /bus@100000/pcie@2900000 ranges: [ 5.091967] j721e-pcie-host 2900000.pcie: IO 0x0010001000..0x0010010fff -> 0x0010001000 [ 5.105163] j721e-pcie-host 2900000.pcie: MEM 0x0010011000..0x0017ffffff -> 0x0010011000 [ OK ] Listening on dropbear.socket. [ 5.118428] j721e-pcie-host 2900000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000 Starting Weston socket... [ 5.162858] imx219 6-0010: supply VANA not found, using dummy regulator Starting Console System Startup Logging...[ 5.175359] k3-dsp-rproc 4d80800000.dsp: assigned reserved memory node vision-apps-c66-dma-memory@a9000000 [ 5.191150] imx219 6-0010: supply VDIG not found, using dummy regulator Starting D-Bus System Message Bus... [ 5.210042] k3-dsp-rproc 4d80800000.dsp: configured DSP for IPC-only mode Starting Reboot and dump vmcore via kexec.[ 5.223590] PVR_K: 186: Device: 4e20000000.gpu .. [ 5.232725] img_dec 4300000.video-decoder: decoder registered as /dev/video0 [ OK ] Finished Load/Save Random Seed. [ OK ] Listening on Docker Socket for the API. [ 5.263809] imx219 6-0010: supply VDDL not found, using dummy regulator [ OK ] Listening on Weston socket.[ 5.275717] PVR_K: 186: Read BVNC 22.104.208.318 from HW device registers [ 5.277460] img_enc 4200000.video-encoder: vxe_enc_probe: using heap 1 for internal alloc [ OK ] Found device /dev/ttyS2.[ 5.300006] PVR_K: 186: RGX Device registered with BVNC 22.104.208.318 [ 5.300590] remoteproc remoteproc0: 4d80800000.dsp is available [ OK ] Reached target Socket Units.[ 5.322417] remoteproc remoteproc0: attaching to 4d80800000.dsp [ 5.332793] [drm] Initialized pvr 23.1.6404501 20170530 for 4e20000000.gpu on minor 0 [ 5.340896] img_enc 4200000.video-encoder: encoder registered as /dev/video1 [ OK ] Finished Console System Startup Log[ 5.354177] imx219 7-0010: supply VANA not found, using dummy regulator ging. [ 5.364660] k3-dsp-rproc 4d80800000.dsp: DSP initialized in IPC-only mode [ 5.365206] imx219 7-0010: supply VDIG not found, using dummy regulator [ 5.378490] imx219 7-0010: supply VDDL not found, using dummy regulator [ 5.385966] rproc-virtio rproc-virtio.0.auto: assigned reserved memory node vision-apps-c66-dma-memory@a9000000 [ 5.396279] imx219 7-0010: failed to read chip id 219 [ 5.410834] imx219: probe of 7-0010 failed with error -5 [ 5.421504] cdns-mhdp8546 a000000.dp-bridge: invalid resource [ 5.429192] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported [ OK ] Started D-Bus System Message Bus 5.441022] virtio_rpmsg_bus virtio0: rpmsg host is online m. [ 5.449884] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xd [ OK ] Finished Reboot and dump vmcore via kexec. [ 5.475592] rproc-virtio rproc-virtio.0.auto: registered virtio0 (type 7) [ OK ] Reached target Basic System.[ 5.490017] remoteproc remoteproc0: remote processor 4d80800000.dsp is now attached [ 5.515295] k3-dsp-rproc 4d81800000.dsp: assigned reserved memory node vision-apps-c66-dma-memory@a8000000 [ OK ] Started Job spooling tools. [ 5.537458] platform 41000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1) [ OK ] Started Periodic Command Scheduler. [ 5.581210] platform 41000000.r5f: configured R5F for IPC-only mode Starting Print notice about GPLv3 packages... [ 5.603907] k3-dsp-rproc 4d81800000.dsp: configured DSP for IPC-only mode Starting IPv6 Packet Filtering Framework... Starting IPv4 Packet Filtering Framework... [ 5.646719] platform 41000000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a0000000 [ 5.656342] remoteproc remoteproc1: 4d81800000.dsp is available [ OK ] Started irqbalance daemon. Starting Telephony service...[ 5.697660] remoteproc remoteproc1: attaching to 4d81800000.dsp [ 5.713567] k3-dsp-rproc 4d81800000.dsp: DSP initialized in IPC-only mode [ 5.733551] remoteproc remoteproc2: 41000000.r5f is available Starting Update pmic regis…fety feature on power rails... Starting Expand the rootfs…ll size of the boot device.... [ OK ] Started startwlanap. [ 5.790532] rproc-virtio rproc-virtio.1.auto: assigned reserved memory node vision-apps-c66-dma-memory@a8000000 [ OK ] Started startwlansta. [ 5.821080] remoteproc remoteproc2: attaching to 41000000.r5f [ 5.833196] platform 41000000.r5f: R5F core initialized in IPC-only mode [ OK ] Started strongSwan IPsec I…IKEv2 daemon using ipsec.conf. [ 5.861692] audit: type=1334 audit(1651233768.008:4): prog-id=7 op=LOAD [ 5.868428] audit: type=1334 audit(1651233768.016:5): prog-id=8 op=LOAD Starting User Login Management... [ OK ] Started TEE Supplicant. [FAILED] Failed to start Print notice abou[ 5.935635] rproc-virtio rproc-virtio.2.auto: assigned reserved memory node vis ion-apps-r5f-dma-memory@a0000000 t GPLv3 packages. [ 5.949883] virtio_rpmsg_bus virtio1: rpmsg host is online See 'systemctl status gplv3-notice.service' for details.[ 5.957347] rproc-virtio rproc-virtio.2.auto: registered virtio1 (type 7) [ 5.961954] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xd [ 5.969088] remoteproc remoteproc2: remote processor 41000000.r5f is now attached [ 5.985001] virtio_rpmsg_bus virtio2: rpmsg host is online [ OK ] Finished IPv6 Packet Filtering Fram[ 5.990730] rproc-virtio rproc-virtio.1.auto: registered virtio2 (type 7) ework. [ 5.995968] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xe [ 6.004422] remoteproc remoteproc1: remote processor 4d81800000.dsp is now attached [ OK ] Finished IPv4 Packet Filtering Framework. [ 6.035441] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xd [ 6.043129] k3-dsp-rproc 64800000.dsp: assigned reserved memory node vision-apps-c71-dma-memory@b2000000 [ 6.053215] platform 5c00000.r5f: configured R5F for IPC-only mode [ 6.059896] platform 5c00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a2000000 [ OK ] Finished Update pmic regis…safety[ 6.071871] k3-dsp-rproc 64800000.dsp: configured DSP for IPC-only mode feature on power rails. [ 6.083596] remoteproc remoteproc4: 5c00000.r5f is available [ 6.084346] Bluetooth: Core ver 2.22 [ 6.089834] remoteproc remoteproc3: 64800000.dsp is available [ 6.099044] remoteproc remoteproc4: attaching to 5c00000.r5f [ 6.105107] platform 5c00000.r5f: R5F core initialized in IPC-only mode [ 6.111774] rproc-virtio rproc-virtio.3.auto: assigned reserved memory node vision-apps-r5f-dma-memory@a2000000 [ 6.120186] NET: Registered PF_BLUETOOTH protocol family [ 6.122295] virtio_rpmsg_bus virtio3: rpmsg host is online [ 6.127624] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0xd [ 6.132673] rproc-virtio rproc-virtio.3.auto: registered virtio3 (type 7) [ 6.148603] remoteproc remoteproc4: remote processor 5c00000.r5f is now attached [ 6.151591] Bluetooth: HCI device and connection manager initialized [ 6.162603] platform 5d00000.r5f: configured R5F for IPC-only mode [ 6.176980] Bluetooth: HCI socket layer initialized [ 6.177982] platform 5d00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a4000000 [ 6.181889] Bluetooth: L2CAP socket layer initialized [ 6.181912] Bluetooth: SCO socket layer initialized [ 6.191744] remoteproc remoteproc5: 5d00000.r5f is available [ 6.197535] j721e-pcie-host 2900000.pcie: PCI host bridge to bus 0000:00 [ 6.201149] remoteproc remoteproc5: attaching to 5d00000.r5f [ OK ] Started Telephony service.[ 6.224088] platform 5d00000.r5f: R5F core initialized in IPC-only mode [ OK ] Reached target Preparation for Network. [ 6.244513] rproc-virtio rproc-virtio.4.auto: assigned reserved memory node vision-apps-r5f-dma-memory@a4000000 [ 6.257013] remoteproc remoteproc3: attaching to 64800000.dsp [ 6.261864] virtio_rpmsg_bus virtio4: rpmsg host is online [ 6.268378] virtio_rpmsg_bus virtio4: creating channel rpmsg_chrdev addr 0xd [ 6.277260] rproc-virtio rproc-virtio.4.auto: registered virtio4 (type 7) [ 6.286281] remoteproc remoteproc5: remote processor 5d00000.r5f is now attached [ 6.286658] pci_bus 0000:00: root bus resource [bus 00-ff] [ 6.300227] platform 5e00000.r5f: configured R5F for remoteproc mode [ 6.307400] remoteproc remoteproc3: unsupported resource 65538 [ 6.314269] k3-dsp-rproc 64800000.dsp: DSP initialized in IPC-only mode Starting Network Configuration... [ 6.321254] rproc-virtio rproc-virtio.5.auto: assigned reserved memory node vision-apps-c71-dma-memory@b2000000 [ 6.337164] virtio_rpmsg_bus virtio5: rpmsg host is online [ 6.342836] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0x15 [ 6.350599] virtio_rpmsg_bus virtio4: creating channel rpmsg_chrdev addr 0x15 [ OK ] Finished Expand the rootfs…full s[ 6.357969] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0x15 ize of the boot device..[ 6.370593] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xe [ 6.380460] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0x15 [ 6.382187] rproc-virtio rproc-virtio.5.auto: registered virtio5 (type 7) [ 6.388432] virtio_rpmsg_bus virtio2: creating channel ti.ipc4.ping-pong addr 0xe [ 6.402220] virtio_rpmsg_bus virtio5: creating channel rpmsg_chrdev addr 0xd [ 6.409493] virtio_rpmsg_bus virtio5: creating channel rpmsg_chrdev addr 0x15 [ 6.416944] virtio_rpmsg_bus virtio5: creating channel ti.ipc4.ping-pong addr 0xe [ 6.424714] virtio_rpmsg_bus virtio4: creating channel ti.ipc4.ping-pong addr 0xe [ 6.432495] virtio_rpmsg_bus virtio3: creating channel ti.ipc4.ping-pong addr 0xe [ 6.432633] platform 5e00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a6000000 [ 6.440132] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] (bus address [0x10001000-0x10010fff]) [ 6.458717] pci_bus 0000:00: root bus resource [mem 0x10011000-0x17ffffff] [ 6.465852] pci 0000:00:00.0: [104c:b00d] type 01 class 0x060400 [ 6.472128] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits [ 6.481936] pci 0000:00:00.0: supports D1 [ 6.486014] pci 0000:00:00.0: PME# supported from D0 D1 D3hot [ 6.494582] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring [ 6.505460] remoteproc remoteproc3: remote processor 64800000.dsp is now attached [ 6.535622] remoteproc remoteproc6: 5e00000.r5f is available [ 6.545977] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01 [ 6.554850] pci 0000:00:00.0: PCI bridge to [bus 01] [ 6.560094] platform 5f00000.r5f: configured R5F for remoteproc mode [ 6.567090] pcieport 0000:00:00.0: PME: Signaling with IRQ 695 [ 6.574883] platform 5f00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a7000000 [ 6.589018] remoteproc remoteproc7: 5f00000.r5f is available [ 6.605268] remoteproc remoteproc6: loading /lib/firmware/j7-main-r5f1_0-fw failed with error -22 [ 6.612031] pcieport 0000:00:00.0: AER: enabled with IRQ 695 [ 6.622492] remoteproc remoteproc7: loading /lib/firmware/j7-main-r5f1_1-fw failed with error -22 [ 6.632350] remoteproc remoteproc7: Direct firmware load for j7-main-r5f1_1-fw failed with error -22 [ 6.641661] remoteproc remoteproc6: Direct firmware load for j7-main-r5f1_0-fw failed with error -22 [ 6.642661] j721e-pcie-host 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges: [ 6.651370] remoteproc remoteproc7: powering up 5f00000.r5f [ 6.664522] remoteproc remoteproc6: powering up 5e00000.r5f [ 6.672981] remoteproc remoteproc6: loading /lib/firmware/j7-main-r5f1_0-fw failed with error -22 [ 6.681934] remoteproc remoteproc7: loading /lib/firmware/j7-main-r5f1_1-fw failed with error -22 [ 6.690881] remoteproc remoteproc6: Direct firmware load for j7-main-r5f1_0-fw failed with error -22 [ 6.701295] remoteproc remoteproc7: Direct firmware load for j7-main-r5f1_1-fw failed with error -22 [ 6.714400] remoteproc remoteproc6: request_firmware failed: -22 [ 6.722072] j721e-pcie-host 2910000.pcie: IO 0x0018001000..0x0018010fff -> 0x0018001000 [ 6.730607] remoteproc remoteproc7: request_firmware failed: -22 [ 6.756017] j721e-pcie-host 2910000.pcie: MEM 0x0018011000..0x001fffffff -> 0x0018011000 [ 6.765429] j721e-pcie-host 2910000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000 [ 6.779464] cfg80211: Loading compiled-in X.509 certificates for regulatory database [ 6.816172] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ 6.831519] [drm] Initialized tidss 1.0.0 20180215 for 4a00000.dss on minor 1 [ 6.856138] cdns-mhdp8546 a000000.dp-bridge: CR: max swing reached [ 6.885168] Console: switching to colour frame buffer device 240x67 [ 6.906370] tidss 4a00000.dss: [drm] fb0: tidssdrmfb frame buffer device [ OK ] Started Network Configuration. [ 6.975382] am65-cpsw-nuss 46000000.ethernet eth0: PHY [46000f00.mdio:00] driver [TI DP83867] (irq=POLL) Starting Network Name Resolution... [ 7.023064] am65-cpsw-nuss 46000000.ethernet eth0: configuring for phy/rgmii-rxid link mode [ OK ] Started Network Name Resolution. [ OK ] Reached target Network. [ OK ] Reached target Host and Network Name Lookups. Starting Avahi mDNS/DNS-SD Stack... Starting Enable and configure wl18xx bluetooth stack... Starting containerd container runtime... [ 7.332004] omap_rng 4e10000.rng: Random Number Generator ver. 241b34c [ OK ] Started Netperf Benchmark Server. [ 7.363929] remoteproc remoteproc8: b034000.pru is available [ OK ] Started NFS status monitor for NFSv2/3 locking.. [ 7.394485] remoteproc remoteproc9: b004000.rtu is available [ 7.402376] remoteproc remoteproc10: b00a000.txpru is available Starting Permit User Sessions... [ 7.411088] remoteproc remoteproc11: b038000.pru is available [ 7.423065] remoteproc remoteproc12: b006000.rtu is available [ 7.426242] remoteproc remoteproc13: b00c000.txpru is available [ 7.427200] remoteproc remoteproc14: b134000.pru is available [FAILED] Failed to start Enable and…figure wl18xx bluetooth stack. [ 7.456907] remoteproc remoteproc15: b104000.rtu is available See 'systemctl status bt-enable.service' for details. [ 7.463570] remoteproc remoteproc16: b10a000.txpru is available [ 7.475602] remoteproc remoteproc17: b138000.pru is available [ 7.481762] remoteproc remoteproc18: b106000.rtu is available [ 7.487860] remoteproc remoteproc19: b10c000.txpru is available [ OK ] Finished Permit User Sessions. [ OK ] Started Avahi mDNS/DNS-SD Stack. [ 7.569993] imx219 6-0010: Consider updating driver imx219 to match on endpoints [ OK ] Listening on Load/Save RF …itch Status /dev/rfkill Watch. [ OK ] Started Getty on tty1. [ OK ] Started Serial Getty on ttyS2. [ OK ] Reached target Login Prompts. [ 7.689219] cdns-csi2rx 4504000.csi-bridge: Probed CSI2RX with 2/4 lanes, 4 streams, external D-PHY Starting Synchronize System and HW clocks... Starting Weston, a Wayland…ositor, as a system service... [FAILED] Failed to start Synchronize Syste[ 7.774102] cdns-csi2rx 4514000.csi-bridge: Probed CSI2RX with 2/4 lanes, 4 str eams, external D-PHY m and HW clocks. [ 7.797115] j721e-pcie-host 2910000.pcie: PCI host bridge to bus 0001:00 See 'systemctl status sync-clocks.service' for details. [ 7.810256] pci_bus 0001:00: root bus resource [bus 00-ff] [ 7.823353] pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x18001000-0x18010fff]) [ 7.834718] pci_bus 0001:00: root bus resource [mem 0x18011000-0x1fffffff] [ 7.846458] pci 0001:00:00.0: [104c:b00d] type 01 class 0x060400 [ 7.855185] pci_bus 0001:00: 2-byte config write to 0001:00:00.0 offset 0x4 may corrupt adjacent RW1C bits [ 7.866986] pci 0001:00:00.0: supports D1 [ 7.871181] pci 0001:00:00.0: PME# supported from D0 D1 D3hot [ 7.881686] pci 0001:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring [ 7.890197] pci_bus 0001:01: busn_res: [bus 01-ff] end is updated to 01 [ 7.897771] pci 0001:00:00.0: PCI bridge to [bus 01] [ 7.910552] pcieport 0001:00:00.0: PME: Signaling with IRQ 720 [ 7.917308] pcieport 0001:00:00.0: AER: enabled with IRQ 720 [ 8.069181] audit: type=1334 audit(1651233770.216:6): prog-id=9 op=LOAD [ 8.076662] audit: type=1334 audit(1651233770.220:7): prog-id=10 op=LOAD Starting User Database Manager... [ 8.156517] xhci-hcd xhci-hcd.6.auto: xHCI Host Controller [ 8.162305] xhci-hcd xhci-hcd.6.auto: new USB bus registered, assigned bus number 1 [ 8.171099] xhci-hcd xhci-hcd.6.auto: hcc params 0x200073c9 hci version 0x100 quirks 0x0000002000018010 [ 8.181043] xhci-hcd xhci-hcd.6.auto: irq 721, io mem 0x06410000 [ 8.187239] xhci-hcd xhci-hcd.6.auto: xHCI Host Controller [ 8.192993] xhci-hcd xhci-hcd.6.auto: new USB bus registered, assigned bus number 2 [ OK ] Started User Database Manager.[ 8.200870] xhci-hcd xhci-hcd.6.auto: Host supports USB 3.0 SuperSpeed [ 8.213802] hub 1-0:1.0: USB hub found [ 8.217640] hub 1-0:1.0: 1 port detected [ 8.222550] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 8.232200] hub 2-0:1.0: USB hub found [ 8.236103] hub 2-0:1.0: 1 port detected [ OK ] Created slice User Slice of UID 1000. Starting User Runtime Directory /run/user/1000... [ OK ] Finished User Runtime Directory /run/user/1000. Starting User Manager for UID 1000... [ 8.415400] audit: type=1006 audit(1651233770.560:8): pid=564 uid=0 old-auid=4294967295 auid=1000 tty=(none) old-ses=4294 967295 ses=1 res=1 [ 8.428102] audit: type=1300 audit(1651233770.560:8): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffe14ddb88 a2 =4 a3=ffff952a4020 items=0 ppid=1 pid=564 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null) [ 8.454689] audit: type=1327 audit(1651233770.560:8): proctitle="(systemd)" [ 8.484957] usb 1-1: new high-speed USB device number 2 using xhci-hcd [ OK ] Created slice Slice /system/systemd-fsck. [ 8.637886] hub 1-1:1.0: USB hub found [ 8.641748] hub 1-1:1.0: 4 ports detected [ OK ] Found device /dev/mmcblk1p1. Starting File System Check on /dev/mmcblk1p1... [ 8.764979] usb 2-1: new SuperSpeed USB device number 2 using xhci-hcd [ 8.790374] hub 2-1:1.0: USB hub found [ 8.795897] hub 2-1:1.0: 4 ports detected [ OK ] Started User Manager for UID 1000. [ OK ] Started Session c1 of User weston. [ 8.839945] audit: type=1006 audit(1651233770.984:9): pid=520 uid=0 old-auid=4294967295 auid=1000 tty=tty7 old-ses=429496 7295 ses=2 res=1 [ 8.852396] audit: type=1300 audit(1651233770.984:9): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffe14ddb88 a2 =4 a3=ffff952a4020 items=0 ppid=1 pid=520 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=2 c omm="(weston)" exe="/lib/systemd/systemd" key=(null) [ 8.878931] audit: type=1327 audit(1651233770.984:9): proctitle="(weston)" [ OK ] Finished File System Check on /dev/mmcblk1p1. [ 8.956959] usb 1-1.1: new high-speed USB device number 3 using xhci-hcd Mounting /run/media/BOOT-mmcblk1p1... [ OK ] Mounted /run/media/BOOT-mmcblk1p1. [ 9.418002] usb 1-1.1: Found UVC 1.00 device <unnamed> (046d:0825) [ 9.538450] input: UVC Camera (046d:0825) as /devices/platform/bus@100000/4114000.cdns-usb/6400000.usb/xhci-hcd.6.auto/us b1/1-1/1-1.1/1-1.1:1.0/input/input0 [ 9.553432] usbcore: registered new interface driver uvcvideo [ 9.588673] PVR_K: 520: RGX Firmware image 'rgx.fw.22.104.208.318' loaded [ 9.606248] PVR_K: 520: Shader binary image 'rgx.sh.22.104.208.318' loaded [ 9.634592] usb 1-1.1: set resolution quirk: cval->res = 384 [ 9.640798] usbcore: registered new interface driver snd-usb-audio [ OK ] Started containerd container runtime. Starting Save/Restore Sound Card State... [ OK ] Finished Save/Restore Sound Card State. [ OK ] Reached target Sound Card. [ OK ] Started Weston, a Wayland …mpositor, as a system service. Starting DEMO... Starting EdgeAI OOB demos... [FAILED] Failed to start DEMO. See 'systemctl status demo.service' for details. [ 11.121804] am65-cpsw-nuss 46000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx [ 11.130532] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project tda4vm-sk -
I'm sorry I don't understand the response. You provided boot log (showing board is working). That is using which supply? If the lab bench supply is NOT working - you can power the board using USB supply and connect the lab bench supply to the power control header. Pulling Pin 1 to GND will disable the board supply.
Robert,
To make sure the board is in working condition, I asked Daiwang to post the successful boot logs using the Qualtek USB-C power supply - QADC-65-20-08CB.
That is what he did. He replied for my post saying, the board works with standard power supply....
Daiwang,
Would you please reply to Robert about the "onboard-supplies " I.e., Robert's post above --- >
Can you measure on-board supplies to see if USB controller is enabling power?Maybe measure power net VMAIN - it should have the same voltage (or near same) as the supplied VBUS. Or you can measure any of the other on-board regulators.
Regards
Shankari G
Measurement probe point is C263. When you supply 20V, do you measure 20V across the capacitor?
Reply for:
Measurement probe point is C263....
-------------------------------------------------
Hi @Robert
I measured the voltage across C263 with VDC=20 as follows:
QADC-65-20-08CB: Vc623=1.9V
Lab voltage: Vc623=1.3V
Not sure I understand the measurements, and I expected 20VDC (or close to 20V) from approved USB supply. Are you measuring correct location? I expect the USB power detection circuitry is not detecting the bench 20V power supply as a valid USB supply and is not enable power to the EVM.
Since board operates correctly from approved USB supply, can lab bench drive a voltage (say 5V) to J17 pin 1 to turn on and drive 0V to J17 pin 1 to turn off?
Sorry for my mistake, the correct measurements are as follows:
QADC-65-20-08CB: Vc623=19.1V
Lab voltage: Vc623=1.3V
Reply for:
Since board operates correctly from approved USB supply....
-----------------------------
Hi Rober
OK, according to this operation to realize "programmable power supply remote control equipment hard start" is wok.
However, if the device is not started for a long time (i.e., the USB power is on and J17 PIN1 is connected to 0V), will it affect the life of the device?
EVM Lifetime should NOT be impacted by leaving USB power enabled but EVM powered off using J17.