This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi RandyP:
I have some problems about C6455 SRIO boot.I hope you will give me some suggestion.
Now I want to make my dsp work on slave Srio boot.In my case,i use a fpga write code and data to the dsp through rapid io.But acording to the document C645x Bootloader User's Guide.It doesn't tell me how to create the image that need to burn to the mater device.
Can you tell me something about this?Thank you very much.
This needs to be a new thread since it is a new question and the other one was marked as answered.
Please follow the same instructions as listed in spruec6g section 6.1 Host/PCI.
Regards,
RandyP
If you need more help, please reply back. If this answers the question, please click Verify Answer , below.
Hi RandyP:
Thank you for answering my questions.Now I create the image that i need successfully.
And one more question.Since the rapid IO is always transfer the data in the multiple of 8 bytes.That means I need to make the data of each section multiple of 8 bytes,am I right?For example,I add data 0x00 at the end of the section.
Acording to the documents Creating a DSP Boot Image for Host Boot(sprab60).I create the image that i want.And now I have some other questions.
1.At the beginning of the srio boot,I don't have to do anything about the slave dsp.Am I right?
2.The document says the host send a doorbell interrupt and the cpu then begins executing at the base of L2.In the dsp c6455.We can send doorbell interrupt with information 0-f,20-2f,40-4f,60-6f.Which correspond to the DOORBELL_ICSR0--4.In order to interrupt the slave dsp to execute at the base of L2,which doorbell info is right?
3.In the document of C6455 BOOT UG,it says the device ID = 2 + BOOTMODE[2]:CFGGP[2:0].I configure the BOOTMODE[2]=1,CFGGP[2:0]=000.So my device ID of the slave dsp is 0x0a?
Looking forward to your answer.
Linking to http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/439/p/129376/467311.aspx#467311 where I think we have everything solved.
Regards,
Travis