Hi,Experts
GPMC is currently not working properly.
The situation is that neither writes nor reads are being done,
GPMC_CLK is not being output correctly.
It seems that 66AK2G12 is trying to output some kind of clock signal, but as far as I can see with the oscilloscope, it is not a clock signal.
GPMC_CSn0 also seems to be set to LO when accessing, but it does not seem to be working correctly.
Can you please tell me what area I should check?
The connection partner is FPGA, but GPMC is configured as follows.
・NOR Flash like, asynchronous and synchronous devices
・Non-multiplexed attached device
・Device size 16bit
・Read/Write Synchronous
・Single access
Best Regards,
Hidekazu