Other Parts Discussed in Thread: AM3352, TPS65219
Hi AM3351 Champ
A customer built a custom board designed using AM3351 and TPS6521905RHBR.
Only two boards were assembled and tested, and all output voltages of the PMIC are not checked.
They downloaded the NVM file to PMIC, and checked the Up/Down Sequence using the scope in PMIC EVK, but it didn't seem to be a problem.
And PMIC_POWER_EN pin of AM3351 is connected to EN/PB/VSENE pin of PMIC, and it is messured as LOW.
Please check if the AM3352 works normally.
Thanks.
Regards,
Jack