Hi Ti support
Out production is designed with DM3730, used two MMC channel, there are:
MMC1---EMMC
MMC3---SD-Card
And the device bootloader is u-boot-2011.06
Now, the MMC1 can be detected and could read/write EMMC device successful, use "mmcinfo" command could read the device information.
But, when try to Init the MMC3 by omap_mmc_init(2), can't read the mmc3 device information, report err"Card did not respond to voltage select!" ,see below:
philips# mmcinfo
curr_device=0
Card did not respond to voltage select!
Device: OMAP SD/MMC
Manufacturer ID: 0
OEM: 0
Name:
Tran Speed: 0
Rd Block Len: 33554432
MMC version 0.0
High Capacity: No
Capacity: 1 EiB
Bus Width: 1-bit
Could you please help this case ?