This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The same SD card with same default SDK9.1 .wic image, can boot on GPEVM, but can't boot on SK-AM64B, stop on below:
U-Boot SPL 2023.04-gb0d717b732 (Dec 06 2023 - 15:11:45 +0000) EEPROM not available at 0x50, trying to read at 0x51 Reading on-board EEPROM at 0x51 failed -19 Resetting on cold boot to workaround ErrataID:i2331 Please resend tiboot3.bin in case of UART/DFU boot resetting ... U-Boot SPL 2023.04-gb0d717b732 (Dec 06 2023 - 15:11:45 +0000) EEPROM not available at 0x50, trying to read at 0x51 Reading on-board EEPROM at 0x51 failed -19 SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)') SPL initial stack usage: 13384 bytes
Team is looking to update the release notes and images soon.
https://software-dl.ti.com/processor-sdk-linux/esd/AM64X/09_02_00_08/exports/docs/devices/AM64X/linux/Release_Specific_Release_Notes.html Contains the fix and Release notes updated . This is a early 9.2 Release to solve the SK-AM64 boot issue.