This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSICE3359: How user control GPMC address via GPIO

Part Number: TMDSICE3359

Hello,

Let me confirm meaning of GPIO2_12 and 2_13 of ICE board version 2.1.
According to following user's guide, it seems that above two are for GPMC_A18 and A19 of NOR flash.
https://www.ti.com/jp/lit/ug/spruip3/spruip3.pdf

However, it seems that these are set as GPIO not GPMC.
Then I have following questions ?

Q1. Is my above understanding that signal "gpio2_12" and "gpio2_13" are set as GPIO correct ?
Q2. If so, is there any information how you control these gpios as address function of GPMC ?

BR,